Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun 8-Pin SOIC to DIP Adapter is a small PCB that lets you adapt SOIC packages into a DIP footprint. These tiny boar…
The SparkFun Qwiic Adapter provides the perfect means to make any old I2C board into a Qwiic enabled board.
6 pin SOT-23 to DIP adaptor. Created to take SOT23 of various pin sizes breakout to DIP. This will work with 3-pin MOSFETs, B…
The Qwiic to Grove Adapter Cable allows interoperability between the SparkFun Qwiic Connect System and the I2C based Grove bo…
This Adapter allows you to run devices and cables with the classic USB Type A connector off a device or adapter with a USB Ty…
This adapter has a standard polarity Male SMA connection at both ends.
The Kingston Canvas Go! Plus 64GB MicroSD Card is a top-of-the-line memory card perfect for popular single board computers su…
It's tiny, it's handy, and it can give your normal USB-equipped device a micro-B connector! With the USB to Micro-B Adapter y…
The SparkFun Jetson Nano Basic Kit with Battery Pack provides you with all of the essential parts needed to start new project…
This is a low-cost, basic SOIC breakout boards. This custom PCB will interface a standard SOIC package IC to 0.1" headers, wh…
8, 16, 20, and 28-Pin SSOP to DIP break out boards. The footprint was rotated to accommodate different width SSOP devices and…
The SparkFun 16-Pin SSOP to DIP Adapter is a small PCB that lets you adapt SSOP packages into a DIP footprint. These small bo…
8-Pin SSOP to DIP break out board. The footprint was rotated to accommodate different width SSOP devices and can be used with…
The Edimax 2-in-1 Wi-Fi 4 & Bluetooth® 4.2 Adapter is a nano-sized USB Wi-Fi adapter that supports Wi-Fi up to 150Mbps.
This is an adapter that converts an RP-SMA board to an SMA antenna. The adapter will connect to any of our 2.4GHz wireless bo…
This is a USB Type-C Power Supply that is compatible with the Raspberry Pi 4.
This adaptor allows you to power your RPi 4 with a previous usb-micro B power supply.
This is a 3-pack of international wall adapter sockets for the UK/EU/AU.
Low-cost basic SOIC break out boards. These are custom PCB boards that interface standard SOIC devices to standard .1" header…
SparkFun Jetson Nano Intermediate Kit with Power Supply provides you with all of the essential parts needed to start new proj…
This adapter supports the mikroBUS™ Click socket with a MatesBUS interface to connect products of any TIMI model directly t…
The QC3.0 Power Supply Set (US) is a USB wall adapter with an input value of AC100-240V, and an output of 6V-6.5V/3A, 6.5V-9V…
The Teensy is an amazing development platform that allows you to get more computing power than an Arduino Uno, and in less sp…
The Mates Stand offers a simple connection for a MatesBUS compatible device, such as the TIMI-96.
SparkFun Jetson Nano Intermediate Kit with Battery Pack provides you with all of the essential parts needed to start new proj…