Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The new PureThermal Mini Pro JST-SR with Thermal by FLIR® is a hackable thermal camera for the FLIR Lepton® thermal imaging…
A first for the Raspberry Pi ecosystem: A 64MP camera module that matches the specs of smartphone cameras.
The OpenMV Cam is a small, low power, microcontroller board which allows you to easily implement applications using machine v…
The SparkFun Grid-EYE Infrared Array Breakout board is an 8x8 thermopile array, giving you a square of 64 pixels capable of i…
The OpenMV H7 Plus is a small, low power, microcontroller board which allows you to easily implement applications using machi…
The Raspberry Pi Camera Module 3 is the latest entry in our mainstream camera line-up, and the successor to the popular Came…
Add computer vision capabilities to your project, without the coding! The Person Sensor includes a camera module pre-programe…
A general purpose 5MP camera module that's SPI enabled reducing the complexity of controlling the camera for use with microco…
The Pixy2 CMUcam5 is smaller, faster and more capable than the original Pixy. The Pixy2 can learn to detect objects that you …
This is the 16mm C-mount telephoto lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module.
An ultra low power CMOS Image Sensor that enables the integration of an “Always On” camera for computer vision applicatio…
The SparkFun Edge Development Board powered by TensorFlow is perfect begin using voice recognition without relying on the ser…
The HQ Camera Module is a camera sensor designed to accept CS-mount lenses and, with the supplied adapter, C-mount lenses for…
The Raspberry Pi Zero and Zero W are both equipped with a smaller CSI (Camera Serial Interface) port than on a full-sized Ras…
The SparkFun Raspberry Pi Zero W Camera Kit provides you with a pan/tilt camera controlled via a Raspberry Pi Zero W.
Based on the 16MP Sony IMX519 sensor, this new camera module gives all Raspberry Pi hackers every bit of power they need to b…
Experience sharp, smooth video calling (720p/30FPS) in a widescreen format with the C270 HD Webcam.
The Machine Learning and AI Concept Kit is a great starting place for the basics of predictive algorithms learned from histor…
This is the 6mm CS-mount wide angle lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module.
The Tiny Code Reader from Useful Sensors is smaller than a quarter, very low cost, and connects through Qwiic.
Powered by Raspberry Pi's RP2040 microcontroller, this board has the power to run all Tensorflow Lite Micro tiny machine lear…
A 200mm MIPI Cable for interfacing the Raspberry Pi Camera Modules with the Raspberry Pi 5.
The WiFi Shield gives your OpenMV Cam the ability to connect to the Internet wirelessly and is perfect for streaming video fr…
The Raspberry Pi Global Shutter Camera is a specialized 1.6-megapixel camera from Raspberry Pi that is able to capture rapid…
The Artemis Development Kit based on the SparkFun Artemis Module and highlights software development features like Arm® Mbed…
The PureThermal OpenMV is a high-end mixed color and thermal camera for professional applications.
This Kit includes the SparkFun Artemis DK board as well as the accessories (Himax camera & USB-C cable) needed to get started…
The Leopard Imaging Camera is a 136° FOV camera module designed for use with the NVIDIA Jetson Nano Developer Kit.
A sturdy pan-tilt mechanism for most of the cameras that are used with microcontrollers.
Deploy computer vision at the edge faster than ever, with our ready-to-use, standalone intelligent camera.
Amphenol FCI FFC/FPC Flexible Circuit Connectors are a broad range of innovative connector solutions to terminate FFC/FPC.
This hardware kit consists of four each of M2 style nylon hex nuts and screws.
The EX8036 Stereo Camera is a high-end imager controller and patterned IR illuminator with a global shutter capable of both c…
This 8MP IR (Infrared) camera module is capable of 1080p video and still images and connects directly to your Raspberry Pi.
The Raspberry Pi High Quality Camera M12 Mount is the same high quality camera as the previous model but with an M-12 lens mo…
This 8mp camera module is capable of 1080p video and still images that connect directly to your Raspberry Pi.