Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
This is a portable, slim, lightweight solar panel charger with 10 watts of power and a standard USB connection port.
The gator:log is the perfect data logging tool for your next experiment.
The Argon POLY+ Raspberry Pi 4 Case uses a three piece snap-fit plastic design to protect your Pi 4 in a cost-effective way.
When you're working with e-textiles, you have a tendency to collect a lot of small parts: LilyPad boards, bobbins, needles, t…
The Qwiic MultiStar adds five additional ports to boards that have only one Qwiic port on the I2C bus and can also be added t…
This is a black plastic bezel, custom made to mate with the silicon rubber pads. Black 1/8" ABS plastic. Using two of these b…
These are Philips-head M3 screws. They are 12mm long and come in packs of three. This is the screw size that the MiP robotic …
**Description**: These are standard nuts with 2-56 thread. For use with 2-56 machine screws and five button pad set listed be…
These are standard screws with 2-56 thread and 3/8" long, recommended for the small button pad sets. Can be used with a 2-56 …
This sleek, red 16GB thumb drive has been emblazoned with our SparkFun Electronics logo and our moniker to Start Something!