Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun Qwiic Pulsed Coherent Radar Sensor - Acconeer XM125 brings powerful 60 GHz radar technology to your projects.
This SparkFun Distance Sensor Breakout utilizes the VL53L1X next generation ToF sensor module to give you the highly accurate…
The SparkFun Qwiic Mini ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), mu…
This SparkFun Distance Sensor Breakout utilizes the VL53L4CD next generation ToF sensor module to give you the highly accurat…
This economical sensor provides 2cm to 4m of non-contact measurement functionality with a ranging accuracy that can reach up …
The TCT40 distance sensor is great for non-contact distance readings from 2cm to 400cm. This unit adds a pair of Qwiic connec…
The LIDAR-Lite v3 LED is a small, lightweight, low-power optical ranging sensor with incorporated ANT profile wireless networ…
The SparkFun Qwiic ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), multizo…
The LIDAR-Lite v4 Qwiic from GARMIN is a high-performance, wireless optical distance measurement sensor that doesn't require …
The SparkFun Pulsed Radar Breakout provide you with a high-precision distance measurement unit with reliable speed, motion, o…
This is the SparkFun "Time-of-Flight" Range Finder equipped with the VL6180 distance sensor and acts as a near drop-in replac…
This is the SparkFun RGB and Gesture Sensor, a small breakout board with a built in APDS-9960 sensor that offers ambient ligh…
This economical sensor provides 2cm to 400cm of non-contact measurement functionality with a ranging accuracy that can reach …
The SparkFun Proximity Sensor Breakout is a simple IR presence and ambient light sensor utilizing the VCNL4040.
The HC-SR04 distance sensor is great for non-contact distance readings from 2cm to 400cm. This unit adds a pair of Qwiic conn…
The SparkFun Qwiic Mini dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an …
The SparkFun Qwiic Mini dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an …
This is the SparkFun "Time-of-Flight" Range Finder, a breakout for the VL6180 distance sensor.
The SparkFun Qwiic dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
Embrace the World of Precision Distance Measurement with the SparkFun DataLogger IoT Distance Sensing Kit.
The ZX Distance and Gesture Sensor is a touchless sensor that is capable of looking for simple gestures. Developed in conjunc…
The SparkFun Qwiic dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
RCWL-0516 is a technology that uses radar Doppler, microwave induction special module for detecting moving objects.
The Kitronik Autonomous Robotics Platform for Raspberry Pi Pico is a fun and hands-on introduction to buggy robotics.
Deploy computer vision at the edge faster than ever, with our ready-to-use, standalone intelligent camera.
Passive Infrared (PIR) sensors are great for detecting motion in a small area around the sensor.
The SparkFun Proximity Sensing Kit is intended to provide you with everything you need to start making proximity related proj…