Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The new PureThermal Mini Pro JST-SR with Thermal by FLIR® is a hackable thermal camera for the FLIR Lepton® thermal imaging…
The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWI…
The SparkFun Qwiic Mini ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), mu…
The SparkFun AS7331 Qwiic Spectral UV Sensor measures UV radiation on three channels, UVA, UVB, and UVC, with high sensitivit…
The SparkFun Mini AS7331 Qwiic Spectral UV Sensor measures UV radiation on three channels: UVA, UVB, and UVC, with high sensi…
The SparkFun Qwiic ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), multizo…
The OpenMV Cam is a small, low power, microcontroller board which allows you to easily implement applications using machine v…
A first for the Raspberry Pi ecosystem: A 64MP camera module that matches the specs of smartphone cameras.
With the FLIR Radiometric Lepton Dev Kit you will be able to bring FLIR's thermal imaging reliability and power to your desir…
Add computer vision capabilities to your project, without the coding! The Person Sensor includes a camera module pre-programe…
Based on the 16MP Sony IMX519 sensor, this new camera module gives all Raspberry Pi hackers every bit of power they need to b…
The HQ Camera Module is a camera sensor designed to accept CS-mount lenses and, with the supplied adapter, C-mount lenses for…
The Raspberry Pi Camera Module 3 is the latest entry in our mainstream camera line-up, and the successor to the popular Came…
The radiometric Lepton has 80x60 active pixels to capture accurate, calibrated, and non-contact temperature data in every pi…
The smaller and more affordable Oak-D LITE can still be considered the swiss army knife of computer vision.
The SparkFun Qwiic Mini dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an …
An ultra low power CMOS Image Sensor that enables the integration of an “Always On” camera for computer vision applicatio…
The Oak-1 is an all-in-one machine vision solution. It’s a 4-trillion-operations-per-second AI powerhouse that performs you…
This is the 16mm C-mount telephoto lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module.
The SparkFun Qwiic dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
The Raspberry Pi Global Shutter Camera is a specialized 1.6-megapixel camera from Raspberry Pi that is able to capture rapid…
This is the 6mm CS-mount wide angle lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module.
The Tiny Code Reader from Useful Sensors is smaller than a quarter, very low cost, and connects through Qwiic.
The SparkFun Qwiic Mini dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an …
The Raspberry Pi High Quality Camera M12 Mount is the same high quality camera as the previous model but with an M-12 lens mo…
The SparkFun Qwiic dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
The Leopard Imaging Camera is a 136° FOV camera module designed for use with the NVIDIA Jetson Nano Developer Kit.
The OAK-D-IoT-40 is an Embedded/IoT version of the OAK-D imaginf platform from Luxonis.
The FLIR Lepton Thermal Camera Breakout Board is an easy-to-interface evaluation board to quickly connect the Lepton camera m…
The EX8036 Stereo Camera is a high-end imager controller and patterned IR illuminator with a global shutter capable of both c…
This Oak-D DepthAI variant interfaces over USB3C to the host, allowing use with your embedded host platform of choice, includ…
The PureThermal OpenMV is a high-end mixed color and thermal camera for professional applications.