Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun AS7331 Qwiic Spectral UV Sensor measures UV radiation on three channels, UVA, UVB, and UVC, with high sensitivit…
The SparkFun Mini AS7331 Qwiic Spectral UV Sensor measures UV radiation on three channels: UVA, UVB, and UVC, with high sensi…
The OpenMV H7 Plus is a small, low power, microcontroller board which allows you to easily implement applications using machi…
Add computer vision capabilities to your project, without the coding! The Person Sensor includes a camera module pre-programe…
If you’ve had ideas for a project that depends on the ability to sense different spectrums of visible light and react based…
The Pixy2 CMUcam5 is smaller, faster and more capable than the original Pixy. The Pixy2 can learn to detect objects that you …
This is the SparkFun RGB and Gesture Sensor, a small breakout board with a built in APDS-9960 sensor that offers ambient ligh…
Basic breakout board for the TEMT6000 Ambient Light Sensor. Only what you need, nothing you don't. Sensor acts like a transis…
The VEML6030 is a high accuracy ambient light sensor with 16-bit resolution. Even more impressive is that it can detect ligh…
The LilyPad Light Sensor is a sewable breakout board with an ALS-PT19 light sensor built in and ready to use right away.
The SparkFun Qwiic Mini dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an …
The SparkFun Qwiic Mini dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an …
Get ready to monitor your environment with this limited-edition kit that includes everything you need to get started with the…
Looking for a Qwiic sensor that can measure the ambient light level directly in lux? This is it! The VEML7700 is a high ac…
Based on the 16MP Sony IMX519 sensor, this new camera module gives all Raspberry Pi hackers every bit of power they need to b…
The SparkFun Qwiic dToF TMF8820 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
The SparkFun Qwiic dToF TMF8821 Imager is a direct time-of-flight sensor that includes a single modular package with an assoc…
The Raspberry Pi Global Shutter Camera is a specialized 1.6-megapixel camera from Raspberry Pi that is able to capture rapid…
This tiny little guy is the ALS-PT19, an SMD ambient light sensor that is much smaller than the standard TEMT6000. The ALS-PT…
This is a small ambient light sensor that acts as an NPN transistor. The more the sensor is exposed to light, the stronger th…
This 8mp camera module is capable of 1080p video and still images that connect directly to your Raspberry Pi.
This 8MP IR (Infrared) camera module is capable of 1080p video and still images and connects directly to your Raspberry Pi.