Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
4-digit 7-segment displays are really neat little devices, it's a shame that they can be so cumbersome to control. Well we've…
It's the end of the world, and you need a button to press. This is it. A 100mm diameter (outside diameter) dome illuminated p…
The motor requires a voltage between 4.5-9V, has a gearbox ratio of 1:48 and a speed of 140RPM at 4.5V.
The SparkFun Qwiic Button with red LED simplifies all of those nasty worries away into an easy to use I2C device, no solderin…
With improved thermal features to support the higher peak power consumption of Raspberry Pi 5, it integrates a variable-speed…
This is a simple pack of five Red LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at you…
The red SparkFun Qwiic Alphanumeric Display allows you to display all sorts of numbers, characters, and symbols. With Qwiic, …
This is a handy selection of popular LED's in a handy carrying case.
This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect fo…
You don’t have to worry about adding a resistor to an LED if you get an LED with a built in resistor! This pack contains 20…
This pack of 25 red 5mm LEDs will help alleviate any frustrations you've had with accidentally burning them out by having a r…
The SparkFun Qwiic Alphanumeric Display Kit comes with six different colored, 14-segment Qwiic displays. This is your all-in-…
This red Mini Breadboard is a great way to prototype your small projects! With 170 tie points there's just enough room to bui…
**Description**: How could anyone improve on the clear plastic breadboard. I mean, that's pretty sweet right? What if it wa…
The SparkFun Qwiic Alphanumeric Starter Kit comes with two displays, one red and one white, standoffs and screws for mounting…
This metal enclosure finished in SparkFun Red will help protect your electronics from harmful contact from outside sources.
This Red 14-Segment Alphanumeric Display allows you to display all sorts of numbers, characters, and symbols.