Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The WS2812B (or "NeoPixel") may look like a common 5050-sized SMD LED, but there’s actually an integrated control circuit e…
The SparkFun Qwiic SerLCD is a serial enabled LCD that provides a simple and cost effective solution for adding a 20x4 Black …
The SparkFun Qwiic SerLCD is a serial enabled LCD that provides a simple and cost effective solution for adding a 16x2 Black …
This APA102C is the regular, 5050-sized SMD LED version. With a control circuit embedded, the APA102C-5050 is incredibly brig…
We know these look like a lot of our other LEDs, but they're not! These are PTH Addressable RGB LEDs with a WS2812 (or "NeoPi…
The WS2812B (or "NeoPixel") may look like a common 5050-sized (5x5mm) SMD LED, but there’s actually an integrated control c…
The SparkFun Qwiic SerLCD is a serial enabled LCD that provides a simple and cost effective solution for adding a 16x2 RGB on…
The SparkFun Qwiic Twist is a digital RGB rotary encoder breakout that is also able to connect to our Qwiic Connect System.
Ever hear of a thing called RGB? Red, Green, Blue? How about an RGB LED? These 5mm units have four pins - Cathode is the long…
This is not your basic 7-segment display. The Dual 7-Segment Display features two digits with an RGB LED in every single segm…
If you’ve had ideas for a project that depends on the ability to sense different spectrums of visible light and react based…
This is the SparkFun RGB and Gesture Sensor, a small breakout board with a built in APDS-9960 sensor that offers ambient ligh…
Rotary encoders are used similarly to potentiometers. They're different from potentiometers in that an encoder has full rotat…
This is a breakout board for the WS2812B RGB LED. The WS2812B (or "NeoPixel") is actually an RGB LED with a WS2811 built righ…
We know this looks like a lot of our other LEDs, but it's not! This is a PTH Addressable RGB LED with a WS2812 (or "NeoPixel"…
These are addressable 5-meter-long 5V RGB LED strips that come packed with 300 APA102Cs. APA102 LEDs are very similar to WS28…
The WS2812B may look like a common 5050-sized (5x5mm) SMD LED, but there’s actually an integrated control circuit embedded …
These 32x32 RGB LED panels are an awesome place to start to add color to a project! You can create animations, games, or usef…
This is a clever little breakout board for both the RGB and R/G illuminated rotary encoders. On one side, it breaks out all o…
Blink any color you need!
This is a right angle 5mm addressable LED. It sounds boring, but at the time of writing, *this is the first one in the world*…
These are addressable 1-meter-long 5V RGB LED strips that come packed with 60 APA102Cs. APA102 LEDs are very similar to WS281…
Affectionately dubbed "Fairy Lights" for their similar appearance, these addressable RGB LED string lights are a great way to…
The SparkFun Lumenati 8-stick is a small board equipped with eight APA102C LEDs in a row and two mounting positions.
These color-changing LEDs take the work out of creating crazy, flashy, blinky... ness. Simply apply power and the LED will cy…
Check out these big 10mm common cathode through-hole LEDs! The opaque epoxy package causes these LEDs to have a soft, diffuse…
These are sealed addressable 1 meter long 5V RGB LED strips that come packed with 60 APA104s per meter.
These 5mm units have four pins - one for each color and a common cathode (the longest pin).
Ever hear of a thing called RGB? Red, Green, Blue? How about an RGB LED? These 5mm units have four pins: one for each color a…
This version of the APA102 (or “DotStar”) is an astoundingly tiny, 8-pin, 2020-sized (2x2mm) SMD LED. With an integrated …