Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The LilyPad Sewable Electronics Kit lets you explore the wonderful world of electronic sewing (e-sewing) and e-textiles throu…
This is the E-textile Basics Lab Pack, a basic wearables learning kit that can easily get you and a group of peers or student…
Sure, your flashing, chip-tune playing T-shirt is really cool at the party... but at some point you need to turn it off. And …
We designed this board to give the user a low profile button without any sharp edges. Button closes when you push it and open…
This is the LilyPad Rainbow LED strip, with seven LilyPad LEDs that are still attached to one another, letting you snap LEDs …
This is a simple pack of five White LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at y…
The LilyTwinkle is a tiny little LilyPad board designed to add some twinkle to your project. Even though it's as small as som…
The LilyPad E-Sewing ProtoSnap Kit is a great way to incorporate buttons and switches into an e-textile project without any p…
The LilyTiny is a tiny little LilyPad board designed to add flashy functionality to your project without taking up a lot of r…
LilyPad is a wearable e-textile technology designed to have large connecting pads to allow them to be sewn into clothing & co…
The LilyPad Arduino 328 Main Board is an Arduino-programmed microcontroller designed to be easily integrated into e-textiles …
The LilyPad MP3 Player is your all-in-one audio solution, containing an Arduino-compatible microcontroller, MP3 (and many oth…
This is a simple pack of five Blue LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at yo…
This is a three axis accelerometer for the LilyPad system. Based on the ADXL335 MEMS accelerometer from Analog Devices, the L…
This is a simple pack of five Yellow LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at …
This is a simple pack of five Pink LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at yo…
This is a simple pack of five Red LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at you…
The LilyPad E-Sewing ProtoSnap is a great way to explore how buttons and switches behave in simple e-sewing circuits before c…
The LilyPad Light Sensor is a sewable breakout board with an ALS-PT19 light sensor built in and ready to use right away.
This is a simple slide switch for the LilyPad. Use it as a simple ON/OFF switch, or to control LEDs, buzzers, sensors, etc. T…
This is a simple pack of five Green LilyPad LEDs that are still attached to one another, letting you snap the LEDs apart at y…
Apply 5V and be shaken by this small, but powerful vibration motor. Works great as an physical indicator without notifying an…
The MCP9700 is a small thermistor type temperature sensor. LilyPad is a wearable e-textile technology developed cooperatively…
Blink any color you need!
This is a small buzzer for the LilyPad system. Use 2 I/O pins on the LilyPad main board and create different noises based on …
The LilyMini ProtoSnap is a great way to get started learning about creating interactive e-textile circuits before you start …
The LilyPad Simple Power is a simple e-textile board with a 500mA charge rate that lets you connect and charge a lipo battery…
The LilyPad Reed Switch is a simple breakout for a reed switch that will make it easy to use in e-textiles circuits in exactl…
This set of sewing needles is a must-have when stitching together your next e-textile project. Each envelope contains three 4…
The full-color LilyPad Sewable Electronics Kit Guidebook contains step-by-step instructions for creating four interactive pro…