Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The BBC micro:bit v2 is a pocket-sized computer that has been updated with additional features that let you get creative with…
The micro:bit v2 is a pocket-sized computer and the Go Bundle provides you with everything you need to get hooked up and powe…
The Logitech K400 Plus Wireless Touch Keyboard is a compact keyboard with an integrated touchpad that puts all your controls …
If you need to add user input without using a button, then a capacitive touch interface might be the answer. The AT42QT1011 S…
If you need to add user input without using a button, then a capacitive touch interface might be the answer. The AT42QT1010 S…
Add capacitive touch to your next project with Qwiic so you can start playing with the touch capabilities as three unique tou…
This is a 1024 x 600 resolution IPS display touchscreen for the Raspberry Pi.