Hey and welcome back, everyone! First thing's first: CAPTION CONTEST. You've been waiting so patiently, and the results are in! Congratulations Hardware.Panda, you're the winner of the "Hacker on the Go" wishlist! Let the wave of glory wash over you like a lead-free tide.
Now, at SparkFun, we have always prided ourselves on our ability to pull ourselves up by our bootstraps, discover solutions that resolve issues we face while staying within our means, and as a consequence, learn and grow through the experience...even if we stumble and fall a few times along the way. Well, this collectively shared value of ours still holds true today. And here is a story about a recent and ongoing educational experience in our Production operations that has pushed us to learn more about how to scale up our manufacturing capabilities while staying true to ourselves...
At the first of this year (not too long after Free Day v3.0), we began to see that our current dual-machine, two-shift pick-and-place operations were reaching, or were already at, max capacity. If you’ve only begun just recently following along with what we do here at SparkFun, we have been running two Manncorp MC38x pick-and-place machines for a little over 3 years now. These two assembly robots have been great investments for us and have no doubt done an excellent job meeting our PCB population needs. They have also been a great model to learn pick-and-place operations on at a pretty decent entry level price.
However, given the lower production capacity of these machines and our building’s space limitations, we had to make a decision between finding new equipment to help us beef up our output or adding a third shift of operation on our two machines. And because of the cultural impacts that we believe would inevitably accompany the addition of a third shift, we decided that new equipment was the direction that should be taken. It also didn’t hurt that we love exploring the use of new tools and equipment - challenges that excite us a good bit more than solving complex organizational and behavioral ones.
So our hunt for the next generation of SparkFun PCB assembly equipment began in earnest last March. Though we knew that component population speed was a critical factor we needed to get better at, we also recognized that the ability to more quickly change over from one production run setup to the next would likely give us the greatest boost in our pick-and-place operational output. After years of running lower-volume PCB assemblies of almost 400 different designs, we learned that rapid changeovers from one production run setup to the next were key to staying on top of a dynamic and ever-changing production schedule. After doing some of our own research and exploring the latest offerings at last spring’s IPC Expo in San Diego, it became quite clear which machine would deliver the results we were looking for...
ReplaceMeOpen
ReplaceMeClose
We were first introduced to the MYDATA machines a couple of years ago and were blown away by the intelligence built into the design of their PCB assembling bots. For starters, their Agilis feeder system made so much sense to us the moment we saw it in action for the first time. It was a sort of “duh” moment for us. As in, "how have we lived without this all these years?!" The Agilis feeders use a small blade to peel back the clear tape on a component reel from the side, instead of requiring a machine operator to manually peel back the tape and tie it off to the feeder, a process which not only takes more time but also results in the unfortunate discarding of quite a few components which must either be populated by hand or discarded.
But what about that improved component placement speed that we were looking for? Well, you may have seen or heard about machines out there with multiple mountheads that work simultaneously together to pick up parts and place them on a stenciled PCB, or panel of PCBs. If you have two pick-and-place heads, you’ll double your speed, right? Yes, most likely...or at least you’ll get close to populating boards twice as fast. Even MYDATA builds & sells machines with dual mountheads. But stepping up to that amount of throughput capacity comes at a cost, one that is likely very easy to justify for extremely high volume contract manufacturers. Lucky for us, MYDATA also designed a version of their high volume machines for lighter volume PCB assemblers. Our MY100LXe has only one mounthead, but is still able to populate a board eight times faster than either of our current Manncorp machines. This is partially a result of the eight-nozzled HYDRA system on the machine that is able to pick up eight components in a single trip to the component feeder section of the machine, and then populate those eight parts in the blink of an eye on its return trip to where the PCBs are. (Check out the video below to see this lightning fast speed in action!) Granted, this system is typically used for the placement of passive parts (though there are many non-passives that it can handle); however, the majority of the parts on most of SparkFun’s board designs are passives.
ReplaceMeOpen
ReplaceMeClose
Fun fact: the mounthead on our MYDATA machine has already traveled 291km (180.8mi) since we began using the machine back in August -- about the same distance as a roundtrip drive from Denver to Vail and back!
We’ve made it this far and I haven’t even mentioned the downtime reduction savings that can be realized on this machine, if it is managed well. During a production run, if a component feeder runs out of parts, the machine will automatically either begin to pull from that component’s secondary location on the machine or move on to other parts that it can place if there is no secondary location. While it has moved on to picking and placing other parts, a fresh and fully loaded feeder of that expired part can be placed onto the machine at any time and the software will recognize instantly that the part it had previously skipped is now “restocked” and available to be pulled from again. This on-the-fly feeder loading feature is what allows for such quick turnaround times between the completion of one assembly run and the start of the next.
A few more fun specs on our new MY100LXe:
It probably goes without saying that we are extremely pumped to be working with such a beautiful piece of highly-tuned machinery these days, and are enjoying the challenges that come with integrating any new piece of equipment into our assembly process. All in all, this is a significant upgrade for us. Although this post may sound a bit more like a review of MYDATA machinery and, perhaps even a promo for them, the ultimate takeaway that I hope to have conveyed is that there is a time and a place for bootstrapped solutions, but that once a particular scale has been reached, the logistical challenges associated with that scale often have very good solutions already developed, and a great deal of support behind those solutions. Allowing ourselves to invest in a costlier but very efficient pick-and-place machine was a difficult decision for us because of our still scrappy mentality. But we’re still learning about how to meet the still growing demand for open-source electronic hardware, and this new machine allows us to grow and develop into a better version of ourselves. We may be a little older and a little wiser, but not to worry, we still keep the old “reflow oven” around so that we never forget our roots!
Man, this has given me bitter envy. You know, when you're envious of something but also realize that there is no way in a million years you will ever get to play with it. Sigh, I guess I'll just keep pretending that I have access to a PnP machine by making "bwzzt" noises when I use tweezers to place components (at the breakneck speed of up to 80 an hour!)
MYDATA, made in Sweden - actually by a good friend of mine. :)
Will this reduction in wasted parts mean that the PnP grab bag product is going to be discontinued?
I keep hearing the term 'hipster' but I don't know what it means. I better learn or I'll continue to lose these caption contests.
Oh I see... yet another group of "non-conformist" conformists. Wow that's new and unique
¯_(ツ)_/¯
Great post, a good read and happy for you guys getting an upgrade. We used to use some older MyData machines before we converted over to all Juki lines. I don't know much about them though, it was really before my time.
How much is the MYDATA MY100LXe? $250,000?
(Places "Free Day 2013" sticky note on Emcee's monitor next to the "Monthly Caption Contest" sticky)
Wow, it's almost January again!
LOL Why is there a dog in the background at 0:40 on the last video?
because we don't allow cats at work.
XD You guys are awesome!!!
There are always dogs at SFE! Get with it!! :-)
It's normal to bring loved ones to the office. Dogs are no exception in this town. :)
How do you hear about these contests? Are they on the home page, or what?
Hi, we try to run a caption contest once a month on the homepage - just keep an eye out for posts titled "[Insert month here] Caption Contest"!
FYI, your RSS feed is translating special characters (') into a horrible mess. It looks as though someone is writing the posts on a Mac, expecting someone on a PC to read it. This post is by far the worst I've seen so far. Special characters turn out looking like a typewriter barfed on the page ;-)
Thank you for the heads-up. Our IT department is working on getting it sorted out as soon as possible - thanks for your patience!
Noooo! How did I lose? I had "Forever Owl-lone" it was a gimme, a shoe-in.
And I'd already cleared a place on the mantle for the nano-oscilloscope.
Next time Hardware Panda -- the day will be mine.
Yes....Yours was good... but it was inspired by my "Programs in OWL. Forever Alone." which admittedly would have bested yours. The day may be yours soon...but next time will be mine! :)
Inspired? Bwah! Goldman's "The Princess Bride" was inspired. Your entry was rubbish, Rubbish I say!
J/K -- I totally stole from you. The contests are great fun.
The only real loser here is the owl with the penny in his eye -- they couldn't even spring for prosthetic presidential dollars? It's that sort of cheapness that keeps a great company like SparkFun from achieving greatness. It's likely the same reason they haven't yet awarded me a nano-oscilloscope TOL-10244 ($99) for use in my high-school physics classroom for a strong second entry. And that same cheapness is keeping you Gizmoguy, from getting a refurbished version of the diagonal Cutters ($1.95) TOL-08794 in an honorable mention.
That is awesome! Glad to hear how y'all are growing and expanding! That is definitely an upgrade! Can't wait to read about the stencil printer tomorrow!
It burns! The tide burns!!!!
Random curiosity on this: "the cultural impacts that we believe would inevitably accompany the addition of a third shift" You didn't mention what you thought those inevitabilities might be?