New Product Friday: On the Go

We've got two new videos this week as well as some exciting new products.

Favorited Favorite 0

It's once again Friday, and you know what that means! It's time for new products. We've got a few big products this week. Many people have been eagerly awaiting the release of the new version of the IOIO (as well as the Netduino). We even decided to take a little extra time and do a stand-alone instruction video on the Shift-In Breakout.

ReplaceMeOpen

ReplaceMeClose

Shift registers are pretty useful if you need more inputs or outputs. Connect up a few pins from your microcontroller, and you can have access to as many (almost) inputs or outputs as you want! We have two breakouts that make it easy.

ReplaceMeOpen

ReplaceMeClose

So now you don't have to be limited by the number of digital IOs on your microcontroller! Hopefully that helped simply explain how they work.

alt text

The new version of the IOIO is finally here! With the IOIO-OTG, it's now possible to use the board as an 'on-the-go' device, as well as a USB host. It even comes with an OTG USB cable. If you're a Java developer looking to add advanced hardware I/O capabilities to your Android or PC application, this is the board for you!

alt text

We now have a new supplier and stock for our Piranha 5mm LEDs. These square common cathode RGB LEDs have 4 legs and can fit into a breadboard for testing. These new versions are much brighter than our old ones, and we now sell them as singles.

alt text

The SN74HC165N is a neat little IC that will take an input of up to 8 parallel lines and produce a single, serial output. We now have a breakout that uses this IC and allows you to increase the number of digital inputs on your microcontroller. Each board can be daisy-chained for epic digital-inputness.

alt text

We have a new version of the popular Netduino development board this week. The Netduino 2 runs faster, has more code space, and even sports 2 additional GPIOs. It even works with Arduino R3 shields! If you need a bit more horsepower, check out the Netduino 2.

alt text

And lastly, we have a revision on a 4D Systems OLED. The μOLED-128-G1 is now the μOLED-128-G2 and gets some hardware and software updates. The 1.5" OLED module can act as a standalone module or work with another microcontroller for powerful embedded applications.


Comments 41 comments

  • Member #288566 / about 12 years ago / 3

    Thanks guys for keeping our hobby alive with new stuff every week and for letting everyone know whats out there with these updates. When I need to get anything for my Arduinos or robot,I come here first. You guys are top shelf.

  • Vampist / about 12 years ago / 3

    How fast can one pump out data to a shift register before it would become noticeable?

    For example, a LED cube. If you wired together a few registers how many pins or LEDs could you control before you could see the animation time of said cube diminishing? If you take into account we are not using any charlieplexing.

    EDIT: Forgot to add, with an Arduino.

    • Shift registers are quite fast. The 595, for instance, has a guaranteed shift frequency of 30MHz. You may find that an Arduino running at 16 or 20MHz will be the limiting factor in a large cube.

      One way to speed things up might be to write your own shiftOut function instead of using Arduino's standard shiftOut. By using low-level commands to write directly to the Arduino registers for the clock and data pins, you may be able slim down and save precious clock cycles.

      • MikeGrusin / about 12 years ago / 2

        Arduino's SPI library takes advantage of on-chip hardware, so it's pretty fast (up to 8MHz on a 16MHz Arduino!)

        • sgrace / about 12 years ago / 2

          Either way, writing pure C and not using any of the framework would still yield a faster speed. Very little overhead when you do it yourself. ;)

          • ajnorster / about 12 years ago / 2

            Or even assembly, especially if you need to count clock cycles to coordinate things.

    • TECH GEEK / about 12 years ago / 2

      I've seen an 888 RGB LED cube done with them. It even used the shift registers to make a pwm signal for each led

  • TECH GEEK / about 12 years ago / 3

    They are called Piranha LEDs for the feeling you feel when you walk onto a pile of them bear-footed. :0

  • Highlight of my week! ...I need a girlfriend

    • It's my highlight as well!! Luckily for me, I was able to get my girlfriend into micro-controllers and programming!! :-D

      • CF / about 12 years ago / 3

        NEVER let her go!

        • I won't!!!! We're starting to build some Xbee computer to computer (more like serial to serial) communication devices. Maybe make some kind of texting device that (for now) will only be transmitted and received by these two Xbees. Next revision will probably use series 2 Xbees to create multiple (more than two) device communication. We'll see :-)

  • Chandhooguy / about 12 years ago / 2

    Netduino description shouldn't it be even supports 2 additional GPIO's?

  • CF / about 12 years ago / 2

    Nick, is it possible to eliminate the uc with a clock and some divide by 8 counters?

    • The nice thing about shift registers is that they use synchronous serial, thus the clock line, and they're not really picky about the speed or consistency of the clock. You could hook up a couple of pushbuttons and clock in bits by hand if you wanted to!

      There's no reason you couldn't get rid of the uC in my example.

  • SoSpartan / about 12 years ago / 1

    Robert points to a 74HC165 and says "input", Nick points to a 74HC165 and says "output"... I'm so confuzzled!

    • JoeH / about 12 years ago / 1

      Both the 165 and 595 take some input and provide some output. The 165 is a parallel in, serial out chip. It's reads 8 input lines and serially shifts them out. The 595 is a serial in, parallel out chips. It shifts in 8 'states' and sets 8 output lines accordingly.

      From the perspective of creating more IO lines, the 165 is useful for creating more input lines, thus it's an 'input' device. The 595 is useful for creating more output lines, thus it's an 'output' device.

  • Also Robert, it's ALWAYS good news!!!

  • Dave_RI / about 12 years ago / 1

    Awesome demo! Thanks Nick!

  • ajnorster / about 12 years ago / 1

    Great presentation! It's not always easy to find accessible explanations for these kinds of devices.

  • Joel_Q / about 12 years ago / 1

    I finally understand shift registers! I just assumed before that they used some form of dark magic. =P Joel Q

  • Wow shift registers really are going to be helpful for me in the future.......So instead of buying an Arduino Mega 2560, I could buy an uno and a shift register(or multiple) and control just as many inputs/outputs?

  • WiKi / about 12 years ago / 1

    The link for Piranha 5mm LEDs goes to 'Product not found'

Related Posts

Recent Posts

Tags


All Tags