SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
Hello everyone! I'm finally back from my trip and ready to start talking about new products again. Special thanks to Nick for filling in for me in my absence. In the next couple of weeks, I'll be compiling data from the Leiger and post my findings here. Right now, I just need to go over all the logs and wrap my head what all the numbers really mean.
[UPDATE: You can see Robert's Chernobyl wrap-up here!]
But for now, let's check out the new products for this week.
ReplaceMeOpen
ReplaceMeClose
We were a bit strapped for time this week, so I wasn't able to properly demo the products. But rest assured, in the next week or two, I'll get some demos together.
You've probably seen us play around with electrodes back when we made Mr. Twitchy. This week, we have the Muscle Sensor V3 Kit which allows you to read input from muscles instead. The Muscle Sensor Kit comes with 6 electrodes, breakout cable and breakout board. With this kit you can read muscle input into your microcontroller.
Want (or need) to detect seismic activity or ground movement? The Geophone SM-24 will let you do just that! It's a simple device; it translates ground motion into voltage that can easily be read by a microcontoller.
Do you need a case for your new pcDuino? This week we have a new enclosure made specifically for the pcDuino. It can also be used with an Arduino as well. It even has a mounting spot for a 16x2 LCD! If the case isn't quite big enough, this extension plate will give you a bit more room.
If you've picked up one of the new 4D Systems LCDs (or are thinking of doing so), chances are you might need a USB-to-Serial Bridge like the new μUSB-PA5. This allows you to communicate with the 4D Systems' screens and controllers. It's based on the FTDI FT232RQ and replaces the μUSB-MB5 and μUSB-CE5.
And lastly, we have a new version of the RN-41 Bluetooth module. The version of the module does away with the pads on the underneath side which were used for connecting an external antenna. Please note that the new module only allows you to use the on-board chip antenna.
Well, that's all for this week. It's good to be back home and at work. Thanks for reading and we'll have more demos, products, and videos coming soon! Check back next week. Thanks for reading and see you then!
If I could mutate and have extra hands, I think I would take a trip to Chernobyl too. That would come in quite handing putting boards together. ;)
Rob's new hands look pretty good, he should be a hand model or something.
Tee hee, Goro is from Pripyat.
Incidentally, I have a couple of the old RN modules that I'm not doing anything yet. I'm learning Arduino, however, and I might be able to build a custom BT joystick or something, what do ya think?
Are you going to be getting any BeagleBone Blacks in?
yes, I believe so.
I have no idea what the first product was, I was too busy laughing! Excellent humor!
If ever there is a lite week for product posts again, you must compensate with more cinematography. More angles, more cuts, panning, zooming, focusing, wide shots, narrow shots, close-ups, far-downs, explosions, celebrity cameos, fish-eye lenses, solar flare, explosions, green screen landscapes, negative strobe effects, orchestral score, and credits. THAT is how you get an Oscar.
Rob, Did I see a green glow all around you during this video, did you stay too long in the danger zone?
Link is incorrect where it says "Serial Bridge like the new μUSB-PA5." Someone added a 0 onto the end of the link resulting in no product being found. Also, is it me, or does that link's tab name say "No such produkt"? Product mispelling intentional? lol
Fixed. Thanks!
Hope you make a video talking about the Chernobyl trip.
I will. It will take time though.
Check out Wiki's featured picture: http://en.wikipedia.org/wiki/File:Chernobyl_radiation_map_1996.svg
took me a sec, but i love the extra arms!
Welcome home Robert!
thanks!