SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
A couple months ago, I left for Chernobyl to do some photography and take some readings with my DIY geiger counter/logger. If you missed the original post about the trip, you can check it out here. I'm back now, and not only do I have some pictures, I've got some stories and of course some data. I'd like to say the Leiger worked perfectly, but that would be a lie. I ended up getting good data, but there were also some problems.
As I talked about in the video a couple months ago, I had a simple message that showed up on the screen to let me know if there was a GPS lock or not. Unfortunately, it always showed 'no lock' even if there was valid GPS information. I still haven't fully gone through the code to figure out what happened, but I suspect it's the way I was determining if the GPS sentences were valid or not. At first, I thought the GPS module had decided to kick the bucket. Thankfully, Dave brought his laptop and we were able to verify that the data was good and there was a GPS lock. But that wasn't the only problem I encountered.
By my estimates (and real-world testing), I determined the Leiger could last around 26 hours on a single charge. However, about 6 hours into our first flight, I went to check on the Leiger, and it was dead! There's an old saying, 'if it ain't broke, don't fix it'. I should have remembered that. The day before the trip, I noticed there was a VERY faint sound coming from the buzzer. It was most likely some feedback from the high voltage side of the board. It was only audible in a very quiet room, with the enclosure off. But, it bothered me enough that I decided I'd try and 'fix' it. I ended up grounding the other side of the slide switch, which made it silent, unless it was enabled. So now the buzzer could be truly silenced.
At the time, I didn't realize that when the buzzer was turned 'off', it was actually just shorting out the power supply. So that 26 hour run-time went down to just a few hours, and also made the whole unit get pretty warm inside. Thankfully I figured it out while I should have been sleeping on the plane. As soon as we landed in Kiev, I used my trusty Leatherman to open the case, dissemble the PCB, and cut the ground wire. It was still telling me it didn't have a GPS lock when it actually did, but at least the power supply was good and it was logging data. It seems no matter how much you test something, or plan your design, there's always going to be a problem. Thankfully, mine were relatively minor. I did end up getting some good numbers from the trip. Before we get into the actual data, I'd like to explain a bit more about the hardware inside the Leiger.
The main portion of the Leiger is based on the fantastic DIYGeigerCounter project. I bought it as a kit and made a few tweaks and adjustments. I wanted a simple interface for turning on and off the LED, buzzer, and screen. So, I moved a lot of the LEDs and buttons to a separate PCB. The PCB started as a standard protoboard, but I cut and hand-filed it down to the size I needed. I added some switches, a button, LED, and various connectors and mounting holes. I also needed a way to mount the GPS (a D2523T), as well as the geiger tube (SBM-20) itself. The case was from OKW Enclosures and faceplate was designed in SolidWorks and machined by Front Panel Express. As you can see, not much space is wasted here. I wanted it to be as small as possible.
The control PCB as well as the LCD 'shield' sit on top of everything else, and cover the rest of the electronics. Once they are removed, you can see the actual Geiger counter board, the ATmega328, an OpenLog, and a PowerCell. The PowerCell worked wonders for this project and provides 5V to everything (except for the GPS, which has its own 3.3v voltage regulator), and charges the 18650 battery. Programming and testing was a bit tricky as the OpenLog sat on the FTDI header and needed to be removed for programming. Since most of the unit needed to be disassembled to get down there, I estimate I've completely disassembled the Leiger a few dozen times. If you look closely, you can see a lot of grey foam tape, which worked well for keeping everything in place, as well as added a bit of shock-proofing for travel.
Here is the code for the Leiger. I'm not a great programmer, so excuse the mess. It mostly works though. Ultimately, it just used an interrupt to count particles, and then displayed it on the screen in various fashions. It also stored these values at regular intervals (along with the GPS data) on an microSD, courtesy of the OpenLog. For keeping track of dosage (overall radiation exposure), I wrote this value to the EEPROM. I chose to write it to the EEPROM instead of the microSD because the RX (receive) was already being used by the GPS, so there was no elegant way to read in the dosage information when the unit was turned on. I didn't want to rely on the softserial library (which is awesome) because I didn't want to mess with the interrupts, which proved to be a good decision). In the end, all the information I wanted got logged. So, how radioactive was Chernobyl?
There's not a really easy answer for this. Generally speaking, it's not very radioactive. The vast majority of the zone has been decontaminated and is roughly the same level of radiation as the rest of the world. However, in a few instances, Chernobyl lives up to the hype. Normal background radiation (as measured by the Leiger), is around 20-30 CPM (counts per minute, or about 0.14 uSv/hour). In the picture above, you can see a reading of over 622 uSv/hour, or about 4500 times background. Also, if you're doing the math, 10922 CPM doesn't actually convert out to 622 uSv/hour. At first I thought it was an error. Actually, I didn't anticipate measuring over 100k CPM, so the screen just isn't formatted to display numbers that high. But as you can see in the data (posted below), it did peak at over 100k CPM (keep in mind that's nearly 1500 counts every second).
What you're seeing in the picture is a boot worn by one of the firefighters that responded immediately after the explosion. After 25+ years, it's still extremely radioactive (I didn't stay long). It was sitting in a hallway in the basement of the hospital. It amazes me that after all this time, artifacts like this still exist. We even saw a claw that was used to remove radioactive material from the roof of reactor 4. Overall though, with the exception of a few radioactive places and objects, the radiation is well controlled. So how much radiation did I end up getting?
After looking over the data, I came up with a good number. I took the total dosage (as recorded from the Leiger) over the course of the full 4 days I was in the exclusion zone. For all hours not accounted for with the Leiger (sleeping, when it was charging, etc), I took the background averages and filled in the missing gaps in the logs. Based on my readings for background levels here at home, and the total dosage I got from Chernobyl, I concluded that my 4 days in the exclusion zone was equal to just under 3 years of normal background radiation. It's a lot in a short period of time, but it's still well below the yearly limit for radiation workers, and just a fraction of the levels known to cause health problems.
Originally, I had planned to do a map of the radiation for the zone, but after getting the data back, I saw that the huge variances made graphing or mapping anything problematic. Because the hot spots were generally several thousand times higher than the surrounding area (and often-times inside a building), setting a scale was nearly impossible. I do encourage you to download the data and sort by the uSv rate. You will find some interesting places. See if you can find the cooling towers, Jupiter factory, hospital, cemetery (the only place in Pryp'yat that wasn't decontaminated) and of course outside reactor 4.
For those of you that skipped down to the bottom, or missed the links in the text, here is the data, the Leiger code, and my pictures from the trip. Thanks for reading (or at least scrolling this far down). It was an amazing trip, and I'm very glad I went. For a photographer, just having access to these amazing locations was an experience of a lifetime. This was all a lot to cover and I'm sure I've left out some important details, so feel free to ask questions in the comments. Thanks again for reading.
Do you still need a lamp to read at night?
You entrusted your future health and ability to have children on a home-made Geiger counter, to deliver us the epic story of the year.. .. .. You sir have cojones the size of Europa. Thank you.
haha. the geiger counter wasn't the only thing I relied on. it was 6 months of planning and research, and we had other geiger counters too. but yeah, size of europe...
Compliments on your choice of glassware, the 14-24 f2.8 is a wonderful lens. Oh yes, some nice images in there too. Certainly looks like an interesting trip. Did you see any other parts of the country?
Dave was rocking his 14-24mm. I was using my trust Zeiss 21mm.
We stayed in Kiev, and then went down to Odesa. Then we flew on to Istanbul for a week.
I put together a quick and dirty heatmap of day 1: https://copy.com/uZ6kG7YnBjct
I like how it says GTFO when the radiation count is above a certain count.
hehe. "alarm" and "warning" just seems too passive....
Unless you picked up 1.2 Rem you were no where near 3x what you get from natural sources. I haven't looked at your data but that would be well in excess what you are allowed to get as a non-rad worker. Be careful when you start measuring your dose as to what you put out there. Just FYI....do a search, an average person in the US gets ~300 mrem per year from naturally occurring sources,(radon, cosmic, food, other people, medical, dental, fallout, etc...)
Cool project.
Keep in mind the unit is strictly geared towards gamma only. the case blocks most beta, and it really can't measure alpha. I'm basing my figures mostly on what it measured here, versus what it measured in Chernobyl. I've logged several days consistently here and have averaged about 0.15uSv/hour with it. In Chernobyl, it gave me ~3891 usV over the course of 4 days, which equates to 3 years. Does that make sense? The device isn't calibrated, I'm mostly using the relative numbers as a comparison.
Awesome photos. Glad you had a good trip.
In that third last picture - are they gas masks on the ground? It's quite a chilling image.
Yes. This was in the elementary school. It's largely a tourist setup. They kinda dumped them all there so they can bring people and give them a photo opportunity. But if you look at my other pictures, you can see a gas mask in almost every shot. They are everywhere in town. the child-size masks are especially creepy.
In USSR times, schools had to arrange civil defense trainings for pupils. Using gas masks and anti-gas medical kits were a part of it, so every school had large amount of these masks in storage. Some legacy of Cold War.
Where's the Caption Contest?
I'd submit, "Are you my mommy?" and, "The Leiger is pretty much my favorite project."
I love that shot of the baby doll wearing a gas mask in the nursery. It’s my desktop background now! I might have it printed and framed. (Hee hee, “Are you my mummy?” was the first thing I thought of.) Now, was that made for a child, or specifically for the doll?
Very good - but it should be "mummy".
awesome trip! I want to do it one day. Im actually wondering one thing.. why does that white land rover have a polish license plate?
Our guide was Polish. We had 2 people with us at all times, our Polish guide, and a Ukranian government official. I recommend going :-)
Where did you get the big red button cover like the one that is on the "set" button?
Never mind, I found them!
I would love to build my own Geiger counter.
There's nothing stopping you!
You see a lot of wolves? They're taking that place over.
We didn't see many wolves, but we saw a lot of stray dogs. They're running all over the place.
These look like real life pictures of the game Fallout 3. Have you considered making the Leiger into a Pip-boy form?
I did, but with all the other photo gear and flashlights and such, it would have been pretty cumbersome.
Hi Robert, I like your overall design, etc. I have been working on a Geiger Shield for the Arduino which makes designing a custom Geiger counter very easy to implement. The shield takes care of generating a variable high voltage to work with just about any Geiger tube and has buffer circuitry to interface to the Arduino for pulse detection. The is also an onboard LED and speaker which the speaker can be fully controlled by the Arduino.
I also have a 4 part Youtube video demonstrating the shield starting at part 1 here
I can also make the PCB available for those interested in building it.
Thanks, Tony
I'm not sure if glowing in the dark is worthy enough to take the risk for such a travel. In any case, nice article!
You did a terrific job with this article and the pictures are amazing as well. This entire story is publication-worthy. Thanks for the great read.
Thank you! There's so much more to say (in regards to the actual time spent wandering around the area), but I tried to stay on topic with the Leiger.
This is extremely cool. I love the pictures, especially the gas mask one. I love the fact that you documented the counter's problems, some may have glossed over it but you went step by step over everything, "Here's what I did right, here's what went wrong" laid out plainly. That's awesome. Thank you for sharing this and welcome back!
Thanks! I couldn't honestly say "it worked awesome" because it had some quirks. And after being there, I would have changed the design a bit. But overall, I'm still pretty happy with the results.
Thanks Robert! Great story. Great project. Great pictures.
But if you start getting a hunger for brains, it's too late, you are turning into a zombie. ;)
Wow! Robert that was an amazing trip and no doubt about it. So can you claim to be an official stalker now?
Very cool. Were there any decontamination procedures in place for tourists? Or were you on your own?
Lots of guts climbing that cooling tower.
re: Guts: That's what I was thinking.. Wouldn't catch me climbing on a modern US tower that tall, let alone one built 30+ years ago in the cold war era soviet union potentially having no maintenance in 25 years or so.
There weren't any decontamination procedures, but we had to pass through stand-up detectors when passing through check-points. The car was also checked at various times. There are several security checkpoints throughout the zone.
Yes, Dave loves climbing stuff, not me. He climbed everything he could. I watched.
Thanks for the notes and pix of your trip! Very jealous! I was getting my B.S. in Nuc. Eng. when this tragedy happened and still find it fascinating. I was able to 3D plot your path and dose rate data (after some minor cleaning up) using Log[100,DoseRate]. It looks good, but I need more time to generate an overlay on a map or Google Earth.
cool! let me know what you find out.
What is the itinerary like to get there? I assume you have to fly into Kiev, and then train/bus/drive to the Pripyat?
We flew in to Kiev via Montreal then Frankfurt - I couldn't find any flights direct from the US to Kiev. From Kiev, it's a couple hours by car to get to Pripyat.
Robert, neat story, cool adventure. I'm glancing at the data, (Day 1). Why are some timepoints (e.g. 4/3/2013, 11:48:30) replicated numerous times, but with different observation data? Also, It appears that it was planned to have a every 6 second sampling rate (?)...what is the mathematical connection between counts and cpm?
good questions. for replicated entries, the GPS did not have a lock. so, it just used the last value. I did this instead of verifying valid data. the 6 second sampling rate was really 5 seconds, but with all the interrupts and everything else running, it turned out to be 6 seconds. counts is just the total number of counts that are seen by the unit. CPM is a per minute calculation. if you take two entries, subtract the counts from one reading to the next, and multiply by 10, you should see the CPM. The CPM is calculated, whereas the counts are the actual counts being recorded.
Where you not wearing a radiation dosing tag?
nope. from what I understand, they stopped doing that a few years ago.
Excellent article and project. I been following this since the last time you wrote about it. One thing. The links to the data seems to point to the same file as the code link. I really want to see the data can you help me? Thanks and super job!!!!
Wayne Hilliard
nice catch, should be fixed now.
Thats a sweet enclosure! You wouldnt happen to carry those would you?
Honestly, after seeing it, I contacted the company, but they aren't responding :-(