New Product Friday: Get Under Control

A new motor, camera, and remote! What's not to like about this week's new products?

Favorited Favorite 0

Welcome back everyone! Exactly seven planetary rotations have occurred, and we have new products. We have a little something for everyone this week, so check it out.

ReplaceMeOpen

ReplaceMeClose

The new camera module for the Raspberry Pi was pretty interesting to play with. We're still working on a few demos, but we've already hooked it up to a telescope and a microscope. It's a versatile module and the price is right.

alt text

It seems that almost everything has Bluetooth connectivity these days. Why create your own remote control from scratch when all you need is a simple handheld remote with a few buttons? The iMedia Remote is a simple Bluetooth remote with 5 buttons. Turn it on, pair it with a device, and you have a handy remote control. It even has a built in battery charger for the internal lithium polymer battery.

alt text

People are using their Raspberry Pis for just about everything - the possibilities are nearly endless. With the introduction of the Raspberry Pi Camera Module, now you can easily use your Pi for imaging. The 5MP camera is capable of full 1080P video as well as still images. There's even a good amount of image processing/adjustment commands that you can play around with.

alt text

I'm not sure why, but electricity and water aren't the best of friends. Get them together and watch the sparks fly! But what if you need to move something when water is present? Don't worry, we got you covered. Check out the new HS-646WP from Hi-Tec. It's a standard sized servo that carries an IP67 rating, which means it can handle immersion up to 1m. Maybe next year we'll do a water course for AVC.

alt text

People seem to like LEDs. People seem to REALLY like addressable LEDs. So what's not to like about the new WS21812 breakout? The WS2812 combines a surface-mount RGB LED with a WS2811 addressable LED driver IC that's INSIDE the LED. Check out the picture below. These can be daisy-chained together for some pretty cool applications.

alt text

Want just the bare LED? We got that. Put this on your own board, flexible PCB strip, or whatever. These LEDs allow you individual control without any extra circuitry.

alt text

And lastly, we have a new version of the UAV Development Board. We've made a few changes with the UDB5, we've removed the MMA7361 three axis accelerometer, the dual axis IDG500 gyro, and the single axis ISZ500 gyro and moved to an MPU-6000. The PCB form factor hasn't changed. If you like, you can add a reset button and/or a 0.2F super cap.

That's all I've got for this week. As I'm typing this, more stuff is coming in. As always, be sure to check back next week for more new stuff. Thanks for reading!


Comments 16 comments

  • an iPhone in an open-source engineering building!? BLASPHEMY!!! CALAMITY!

    • diz / about 11 years ago / 2

      I love OSS, but Android sucks for us developers: http://opensignal.com/reports/fragmentation-2013/

      iOS development is enjoyable. I love my iPhone.

    • I use it only as a phone to augment my Google Voice service which I have at home. I have a 100 minute per month pay as you go plan, and bought it refurbished.

  • CHaskins / about 11 years ago / 2

    Nobody happened to notice that the Raspberry Pi Video was mirrored? I thought I was going blind cause I couldn't read Sparkfun on the boxes! It was backwards! lol

  • Iron man / about 11 years ago / 2

    you guys haven't mentioned that you transferred a bunch of items from your eagle library to fritzing for people to use in their designs. which is so helpful as i enjoy using fritzing. it has a more friendly user interface than eagle.

    • Yup! Pamela from our marketing team has been working closely with the Fritzing folks to get more parts transferred over. Glad to hear it's helping you out!

  • North Alabama PC / about 11 years ago / 2

    Rob, it looks like the circuit board in the servo has conformal coating over it, this also helps to protect it from water/moisture.

    • yes, it did have a coating over it. I will say that it was a bit sloppily applied, but it was on there. I think the gasket will do you the most good. there were some parts of the inside that didn't appear to be covered.

  • andy4us / about 11 years ago / 2

    The datasheet link for the WS2812 RGB LED Breakout gives a 404 error

  • andy4us / about 11 years ago / 2

    In the product description for the servo, it says "Voltage: 4.8-6.0 Volts" , but in the video you say 6.0->7.4V

  • HP / about 11 years ago / 2

    sooo.. why does it say WS2811 on the board if it is a WS2812? isn't it the WS2811 which is the combination of a RGB LED and a WS2801? oh, the similatities..

    • KirAsh4 / about 11 years ago / 2

      The IC is a WS2811, not 2801. The combining of a 5050 LED plus the WS2811 is what manufacturers are calling a WS2812. As a comparison, the WS2801 can do both constant current as well as constant voltage. The WS2811 is only constant current.

  • Vinnie / about 11 years ago / 1

    This is a really good product post. I'll get one of those camera mods when I can.

  • supersat / about 11 years ago / 1

    YES!!!! I've been waiting forever for those WS2812s! MOAR!!!

Related Posts

micro:bit Resolutions

Recent Posts

Tags


All Tags