New Product Friday: Dumpster Dive

This week we have a bunch of new buttons, cases and the first ever SparkFun Dumpster Dive!

Favorited Favorite 0

This is a special week for new products at SparkFun. Not only do we have bunch of new products this week, but we also have the first ever "Dumpster Dive." Check the video below for more details.

ReplaceMeOpen

ReplaceMeClose

As we said in the video, the Dumpster Dive will not be available until noon Mountain Time. Check back then for the link below to work. We don't expect them to last long, get them while they last, we only have 50!

alt text

Over the years we've accumulated a lot of excess parts. Between prototyping, engineering samples, customer returns, and just old stuff that's been sitting on the shelves for way too long, we've amassed over 75 pounds worth of electronic excess. Some of it's one-off, some of it's a little broken or ugly, and the rest of it's just not worth individually listing and selling. We didn't like the idea of just tossing it. Sure, we would have responsibly recycled it, but it's all still useful and worth getting into people's hands. Introducing the SparkFun Dumpster Dive.

So what we've done is filled up 50 boxes with 1.5 pounds of stuff each. We're selling it for $10 a box, limit one per customer. Each Dumpster Dive is different and contains a lot of different goodies (1.5 pounds actually adds up to quite a bit). Some of it might be broken, missing parts, or otherwise undesirable in some way. Some of it might just be overstock. It's a gamble. Check the video above for some footage of us actually putting products in the boxes to get a better idea. The link will be active at noon, Mountain Time.

alt text

Who doesn't like buttons? That's what I thought. We have a bunch of new buttons for you this week. First up are these great metal pushbuttons. We have them in 5 different colors, and 2 varieties (momentary and latching). The buttons are SPDT, and have separate pins for controlling the LED ring.

alt text

If you're looking for a basic pushbutton, check out these simple panel mount buttons. They are momentary, which means they are only 'on' when you are pressing them. We have them in green, black, yellow, blue, white, and of course red. They have simple solder connections at the base and include a nut and washer.

alt text

If you have an Arduino Mega, you've probably learned that there aren't many enclosures made for it. We found a neat mega enclosure from the same makers of the Pi Tin. Like the Pi Tin, you don't need any tools and you still have access to all your pins, headers, and connections. If you're using shields, we do recommend getting some stackable headers though. We have them in black, blue and clear. These are some pretty cool cases.

alt text

A few weeks back we received an incorrect shipment of Pi Tins and ended up with some green ones. You guys (and gals) liked them so much we decided to carry even more colors. In addition to the clear and green, we now have black, pink, yellow, blue, and white. As I said above, these cases are cool because they don't require tools, give you access to everything, and are inexpensive. They make a great addition to the Raspberry Pi (model A or B).

alt text

Have some big LEDs you need to drive? The PicoBuck LED Driver is an economical and easy to use driver that will allow you to control and blend three different LEDs on three different channels. At roughly 2x3cm, it's a great way to drive higher-powered LEDs.

alt text

The TMP006 is a pretty cool little IC. The TMP006 breakout can measure the temperature of an object without making contact with it. By using a thermopile to detect and absorb the infrared energy an object is emitting, the TMP006 breakout can determine how hot or cold the object is. The IC is mounted on a board with 0.1" spaced header and some mounting holes. Check out the product page for a quickstart guide, library and example code.

alt text

If you're an educator looking to get into the world of technology, check out the new book, Invent to Learn. This book explores how you can join the exciting maker movement and turn any K-12 classroom into a center of innovation.

ReplaceMeOpen

ReplaceMeClose

Speaking of learning, we created a new video to showcase our new and improved SparkFun Inventor's Kit. It has new circuits, a new much-improved case and updated instructions. Check it out!

Phew, that's all I have for this week. If it's before noon, be sure to check back at noon (mountain time zone) for a chance to grab one of the Dumpster Dives. Thanks for reading, watching, and see you next week!


Comments 21 comments

  • andy4us / about 11 years ago * / 9

    Monday Morning meeting, Head of Production ( HoP), Robert, and Nate in high backed armchair, stroking a white cat.
    HoP: "I have 75lbs of crap in the corner I need to get rid of"
    Robert: "I'll bet you $20 I can get rid of it for $500 in less than 2 minutes"
    Nate: "Exceeelent"

    • you know, it went down like this, almost exactly... except, I'm allergic to cats.

      • Mr. Bigglesworth was hairless... edit: your BB format breaks my link!

        • andy4us / about 11 years ago / 1

          James Bond can be streamed on Netflix right now, so I was more going for a Blofeld feel , http://en.wikipedia.org/wiki/Ernst_Stavro_Blofeld . Although the "Exceeelent", was more Monty Burns from the Simpsons !

  • Member #317608 / about 11 years ago / 4

    In the future, could you do these sorts of quick-sell promos in the evening or on weekends. I was at my High School at noon, and our firewall blocks your website (e-commerce, and the fact that our firewall is completely ridiculous). Also, was there a cushion in that dumpster, or does Dave have indestructible bones?

    • He's probably just broken them so many times that they have all been exchanged for titanium implants.

  • Truth is, if I lived near boulder I would make late night trips to sparkfun HQ on a regular basis.

  • Dumpster Dive? I'm surprised those weren't already under Dings and Dents. Those tamper-free buttons sure are pretty! I got a couple of those from somewhere, but without the LED ring. I think the red one would be perfect for an Antimov kill switch.

  • The metal buttons are super slick.

  • TECH GEEK / about 11 years ago / 1

    Is it possible (if) I get one of the 50 packs, to request for it to be shipped out on monday/tuesday when I'll be placing a second order?

    • you can immediately email customer service after your order. OR, you can select another shipment or payment method.

  • Is this available to international customers? (I'm in the UK).

    • Yes, you just have to pay for shipping (and the $10 for the actual box). It's roughly 2 pounds boxed up.

  • ransomhall / about 11 years ago / 1

    Dumpster Dive Dave rocks the mount and enter move. For sure he's done that a few times before...

    • the best part is that I jokingly suggested he do a front-flip into the dumpster. I really didn't expect him to take me seriously. The Friday New Product Videos is just an elaborate way to see if Dave will ever question what I tell him to do...

      • Erik-Sparkfun / about 11 years ago / 3

        Dave doesn't know the word 'fear.'

        Lightning edit: He probably DOES know the word 'pain,' though.

        • Lightning edit: He probably DOES know the word ‘pain,’ though.

          I can confirm this. So far I've only had to force him to seek medical treatment once, but I doubt it'll be the last time.

        • I don't think he knows the word 'no'.

  • ME heat o nator / about 11 years ago / 1

    Electronics and Dumpster-diving! Two childhood loves morph into one box of greatness :)

Related Posts

Recent Posts

Tags


All Tags