A Cornucopia of New Products - RP2350, Quadband GNSS, Compute Modules, and More!

It's a special Wednesday Product Post here at SparkFun and we have many new products to be thankful for!

Favorited Favorite 0

No, your eyes aren't lying to you, it's a Special Wednesday Product Post here at SparkFun Electronics! Since it's Thanksgiving tomorrow here in the US, we decided to push up our normal weekly product post a few days. That way, if there's anything released today that you think might make the perfect gift, you could potentially factor that into your gift shopping before Black Friday and Cyber Monday.

But first, some house keeping: SparkFun will be closed Nov. 28th and Nov. 29th in observance of Thanksgiving. Any orders qualifying for same day shipping placed after 2:00 p.m. MST on Wednesday, Nov 27th will be processed on Monday, Dec 1st. Wishing you a safe and happy holiday weekend from all of us at SparkFun! In case you need a little help in order to know when exactly you can place your orders and get them by December 24th, we’ve updated our handy guide for absolute last minute shipping deadlines.

FINAL NOVEMBER DEALS WEEK!

We have SO MANY new products for you today including a new RP2350 Thing+, a new Qwiic five-way directional pad, pre-orders on new quadband GNSS products, and Raspberry Pi released 20+ new products today annoucning their new Compute Module 5 board. We, of course, can't forget about the new Pico 2 W released on Monday, either! So let's jump in and take a closer look at all of this week's new products!

Utilize the new RP2350 module from Raspberry Pi in a familiar Thing+ format!

SparkFun Thing Plus - RP2350

SparkFun Thing Plus - RP2350

WRL-25134
$29.95

The SparkFun RP2350 Thing Plus is a dynamic and powerful wireless development platform in the Thing Plus form factor. Built around the RP2350 microcontroller from the Raspberry Pi Foundation, this board includes their radio module for single-band 2.4 GHz WiFi 4 (802.11n) and Bluetooth® 5.2 along with standard hardware components found on all Thing Plus Boards. This includes on-board Lithium Ion (LiPo) battery charging and fuel gauge circuits, µSD card socket, Qwiic connector, and the Thing Plus pinout (Feather-footprint), allowing use of the RP2350 Thing Plus in a wide variety of both local and remote applications.


SparkFun RTK Postcard

SparkFun RTK Postcard

GPS-26916
$174.95
1

Designed and manufactured in Boulder, CO USA, the SparkFun RTK Postcard is a compact development board for your high-precision positioning and navigation needs. This board combines the Quectel LG290P GNSS RTK receiver with an Espressif ESP32-PICO-MINI-02 MCU module, running our latest RTK Everywhere firmware. The ESP32 provides the SparkFun Postcard with WiFi and Bluetooth® connectivity to operate as an NTRIP caster or client. Meanwhile, the 4-pin locking JST-GH connector allows users to transmit or receive RTCMv3 messages for RTK corrections from a local base station.

This board is now available for pre-order.


SparkFun Portability Shield

SparkFun Portability Shield

DEV-27510
$34.95

The SparkFun Portability Shield adds all the user interface bits needed to take a SparkFun development board into the field. A LiPo battery connector, charger, fuel gauge, and an on/off switch address your power needs. A friction-fit microSD connector allows for data logging. The 1.3in. OLED and a five-way navigation switch provide an excellent user interface. Locking 0.1in. headers along the shield's edge make it easier to solder male pins in place.

This board is now available for pre-order.


SparkFun Qwiic Directional Pad

SparkFun Qwiic Directional Pad

PRT-26851
$5.95

The SparkFun Qwiic Directional Pad adds a five-way directional pad to your I2C bus! When connected to a microcontroller, press down on the directional pad (up, down, left, right, or center) to provide additional input for your application. The built-in RGB status LED provides visual feedback indicating which button is pressed.


Raspberry Pi Pico 2 W

Raspberry Pi Pico 2 W

DEV-27345
$7.00

The Raspberry Pi Pico 2 series of microcontroller boards is built on RP2350and the Pico 2 W adds wireless functionality with a 2.4GHz 802.11n wireless LAN and Bluetooth 5.2 wireless radio and on-board antenna.. With a higher core clock speed, double the on-chip SRAM, double the on-board flash memory, more powerful Arm cores, optional RISC-V cores, new security features, and upgraded interfacing capabilities than the previous version. The Raspberry Pi Pico 2 series delivers a significant performance and feature boost while retaining hardware and software compatibility with earlier members of the Raspberry Pi Pico family.

This board is now available for pre-order.


Raspberry Pi Compute Module 5 Development Kit

Raspberry Pi Compute Module 5 Development Kit

KIT-27252
$130.00
1

A complete development kit for the Raspberry Pi Compute Module 5, providing all products required to allow an engineer to start a design “out of the box”. This includes a Raspberry Pi Compute Module 5 32GB Wireless with 4GB RAM, Metal Case, IO Board, Passive Cooler, Power Supply (NA plug), Antenna, and HDMI and USB A to C Cables.

If you're looking to use a different Compute Module 5, we have 16 different options to choose from!

This kit is now available for pre-order.


Raspberry Pi Compute Module 5 IO Board

Raspberry Pi Compute Module 5 IO Board

DEV-27251
$20.00

The Raspberry Pi Compute Module 5 IO Board breaks out every interface from a Compute Module 5. It provides a development platform and reference baseboard, reducing the time to market for Compute Module 5 based designs.


Raspberry Pi Compute Module 5 IO Case

Raspberry Pi Compute Module 5 IO Case

PRT-27411
$15.00

This is a metal case designed to fit the Compute Module 5 IO Board. The case includes an integrated fan, which can be connected to the 4-pin fan connector on the IO Board to improve thermal performance of the Compute Module 5.

This case is now available for pre-order.


Raspberry Pi Compute Module 5 Passive Cooler

Raspberry Pi Compute Module 5 Passive Cooler

PRT-27412
$5.00

This is an aluminum heat sink designed to fit on a Compute Module 5. It includes thermal pads for maximum heat transfer from the CPU, memory, wireless module (if fitted) and eMMC (if fitted) components to the heatsink itself. We highly recommend using one with the new Compute Module 5 line.

This accessory is now available for pre-order.


Raspberry Pi Compute Module 5 Lite - 2GB RAM

Raspberry Pi Compute Module 5 Lite - 2GB RAM

DEV-27481
$45.00

The Raspberry Pi Compute Module 5 is a system on module that delivers the power of Raspberry Pi 5 in a form factor ideal for embedded applications. Featuring a quad-core Arm Cortex-A76 processor, dual 4Kp60 HDMI output, Gigabit Ethernet, optional fully-certified wireless module providing Wi-Fi® and Bluetooth connectivity, and a variety of RAM and eMMC flash options. Compute Module 5 enables you to leverage Raspberry Pi 5’s powerful hardware and optimized software stack in your own custom systems and form factors.

As we mentioned before, if you're looking to use a different Compute Module 5, we have 16 different options to choose from!

These boards are all available for pre-order.


That's it for this week. As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another! As a reminder, SparkFUn will be closed tomorrow and Friday in observance of the Thanksgiving holiday. Happy hacking!

Never miss a new product!


Comments 0 comments

Related Posts

Recent Posts

Tags


All Tags