SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
This was a pretty big week SparkFun. Not only did we have the big Intel Edison announcement earlier this week, but this was the first week we started occupying our new building. We still managed to throw together a New Product Post Video, even though we don't have a studio setup yet. If you want a sneak peak at the new digs, check out the video below.
ReplaceMeOpen
ReplaceMeClose
In the next few (several?) weeks when we get more settled, I'm sure we'll have a formal walkthrough video of the new building. It's still a bit of a work in progress and it's only about half-occupied, we still need to move stock and production over. Plus, we need to setup the new studio, what will it look like?
Earlier this week we did a mid-week product post, announcing not only the new Intel Edison, but also the 'Blocks' that we are making to accompany the module. Blocks are a lot like shields are for Arduino. They connect to the Edison module to not only expand functionality, but also to gain access to the hardware contained in the tiny module. Want to know more? Check out the video below.
ReplaceMeOpen
ReplaceMeClose
This is the HackRF One, a Software Defined Radio (SDR) peripheral capable of transmission or reception of radio signals from 10MHz to 6GHz. Designed to enable test and development of modern and next generation radio technologies, HackRF One is an open source hardware platform that can be used as a USB peripheral or programmed for stand-alone operation. Be sure to check out the wiki for more information!
If you're going to get a HackRF One, you're going to need an antenna. The ANT500 is a telescoping antenna made specifically for the HackRF. It has an SMA connector, telescopes from 20cm to 88cm and is designed for operation between 75 MHz to 1 GHz. You can also act like Zorro with one if you're bored.
We have another MOSS robotics kit this week. The Exofabulatronixx 5200 is not only hard to type, it's got a LOT of pieces. Whereas the Zombonitron is 1600, the Exofabulatronixx is a whopping 5200! But seriously, it has a lot more MOSS blocks and spheres to build more stuff. It also includes a 'double brain' block which uses Bluetooth to link your robot to your mobile device or computer. If you're not familiar with MOSS, it's a system of interconnecting robotic blocks, held together by metal spheres. The spheres not only act as a means to transmit power, but also signals between blocks.
You’ve always wanted to output analog voltages from a microcontroller, the MCP4725 is the DAC that will let you do it! The MCP4725 is an I2C controlled Digital-to-Analog converter (DAC). A DAC allows you to send analog signal, such as a sine wave, from a digital source, such as the I2C interface on the Arduino microcontroller. We have a new version this week that fixes some minor silk issues and gets a basic update.
We also cleaned up the Touch Shield a bit, fixing some minor layout issues. The Touch Shield uses an MPR121 touch IC and has 9 touch pads along with 3 extra external connections for additional pads. The shield makes touch input nice and easy for your Arduino.
Lastly, we have some panel mount nuts. You know those really thin nuts that come with panel mount buttons and switches that you end up losing and can't find replacements for at the hardware store? We now have the most common size (M12 0.75) in packs of 25.
That's all for this week. If you didn't get enough new stuff between the Intel Edison products and the ones we have for today, I don't know what to tell you. I guess you'll just have to come back next week and see what else we have then. Thanks for reading and we'll see you again next week.
I had high hopes that this week's NPV would be filmed in the back of a U-haul truck driving up the Diagonal Highway.
As always, more great stuff that I didn't even know I needed until Sparkfun showed it to me. I'll have to do a local pick up so I can see the new digs!
Ok, the awesome of Sparkfun is showing in that walkthru.
Suddenly we see.... A Princess Dress, a Dombek, and an office being painted in a Elven candles and forest motif....
Incidentally, have we seen the last of the "RedBox wall"? I mean, will that part of the classic Friday New Product Vid live on in the next set?
To speak to the Red Box Wall, I'm not sure what's in store, but our photo / video studio in this building is HUGE. Like 16' wide and 35' long. It's probably about 4x the size of the old studio and hasn't gotten any serious work done on it yet, so as time goes on you'll probably see it develop into something entirely new.
How about a wall made of all the different widgets and stuff you sell. It would still be mostly red too!
When the guys tear down the old set, I wonder if they will find the box that had the 6Ahr LiPo, Arduino, and Sparkfun adhesive bandages....
looks like a nice halloween costume in the works?
Anyone know why Intel decided to name their product after a businessman instead of a scientist this time? runs
Well, Edison "invented" a lot of things, just like Intel "invented" the Arduino.
*Edison ... damn you autocorrect ...
Hey there since a lot of you build drones or have interest in drones, here is a fun fact I just learned about them. By using drones, biologists have proven the often scoffed theory that animals know when you are watching them and behave differently then when they dont know you are watching. It's been proven with certain birds and cats.
I'm not sure about "Blocks are a lot like shields are for Arduino." - maybe "Blocks are a lot like shields for Arduino."
Feel free to make the change, or not :) Cheers!
This is probably weird, but your shelves at 1:32 bring back memories. I spent a week assembling those exact shelves for my previous employer. You have to get past any fear of heights when you are lifting heavy pieces of plywood up 12 feet and then hammering on the platform you are sitting on to set the beams. Then again, maybe you had a better way of assembling them...
Ok the Edison looks fairly cool but WOW does that thing get expensive really fast O.o
Great job replicating the stairwell from the old building! Anytime I felt like a good leg workout, I'd order something from Sparkfun just to use the stairs. You guys are like Crossfit for the geek crowd.
Sadly, the reception area is downstairs now, so there's no need to climb the stairs if you're picking something up. Then again, if you're taking classes at SparkFun, you do need to get to the second floor somehow!
No rock climbing equipment or elevator?
Very true, but feel free to stop by one day and just walk up and down the stairs! :)
That last picture is oddly satisfying...
Very nice video guys. And that last guy, great pronunciations of lots of techno babble.