New Product Friday: Slip and Slide

Tons of new stuff this week including some Actobotics kits, robot parts, and more.

Favorited Favorite 0

You want new products? That's good, because we have quite a few this week! We even have some new robotics stuff, and everyone loves robots, right? Check out the video, and then brace yourself for the new stuff below.

Wasn't that fun? Slip rings are really cool and definitely solve a difficult problem in robotics.

alt text

Want to start messing around with Actobotics but have no idea where to even begin? Why not check out the Actobitty? It's a small an simple robotic platform that uses two motors for motion and a central channel for attaching sensors and other goodies. It even comes with these clever little clips that allow you to attach an Arduino to the top. It comes as a kit and assembles easily and can interface with all other Actobotics products.

alt text

Need something a bit bigger and off-roadier? Check out the 4WD off-road chassis. Like the Actobitty, it has all Actobotics products, but is quite a bit more substantial. It has a pivoting suspension, plenty of room for batteries, controllers, and other electronics and uses 4 heavy duty planetary gearhead motors. Check the video and watch Casey try to break them. Casey approves, and Casey knows motors.

alt text

OK, so maybe robots aren't your thing, that's cool. We don't judge (well, maybe Casey will). What about cameras? This week we have a camera slider kit from Actobotics. It uses a 24" channel, a timing belt, and some pulleys to create a simple motorized slider (motor not included). You can use any of the Actobotics motors or even attach a NEMA 17 stepper with an adapter plate.

alt text

So. Now you have all this really cool Actobotics stuff, but you want to make this crazy robotic arm thing. But how do you make the arm rotate 360 degrees while still maintaining an electrical connection? Two words: slip rings. Slip rings are simple electromechanical devices that have a set of wires on each side, and allow you to spin assemblies while maintaining electrical connections. Check out the video above for a demonstration. We have them in 3 flavors. We have a 12 wire and 6 wire (both capable of 2A), and a 3 wire capable of 15A.

alt text

Remember those little clips on the ActoBitty for connecting your Arduino? We have those as separate products. They don't require tools, you just snap them on the channel, and snap in your board. We have a pair of them for both Arduino boards and for the Raspberry Pi.

alt text

Last, but definitely not least, we have some new hookup wire. This isn't just any ordinary hookup wire, this is super flexible silicone jacketed wire. It's great at abrasion resistance, heat resistance and is extremely flexible. We have it in both black and red, 30 awg, 24 awg, and 12 awg, in lengths of 1, 5, and 10 meters. Check here for all the lengths, colors, and sizes.

That's it for this week folks. Thanks for reading, watching, and just coming to the site to hang out. Of course, we'll be back again next week with more new products, see you then.


Comments 21 comments

  • PalmTreesandPICs / about 10 years ago / 7

    Man I love the awkward guy at 4:00 walking into the shot, panicking, and leaving the shot.

    • Byron J. / about 10 years ago / 11

      It became suddenly apparent that I wasn't going to be able to talk to Rob just then.

      • Imaxinar DM / about 10 years ago / 3

        Next time, just do a little dance and steal the shot LOL.

  • Curtie44 / about 10 years ago / 2

    Strangely, I miss the wall of red Sparkfun boxes that lined the old "New product Friday" video room...

  • Imaxinar DM / about 10 years ago / 2

    Would be WAY cool if you could find a source for Slip Rings that had 3 large gauge and 4 or 6 small gauge in one package. Power to the Articulated and Data at the same time... PS.. screw the cost.. it would be worth it (just kidding.. yeah.. inexpensive LOW rev speed units please)

  • Ogre / about 10 years ago * / 1

    Is there a possibility of getting the new, insanely exciting ESP8266 WIFI module in one of these new product friday bits soon?? Please?

  • erco / about 10 years ago / 1

    Please clarify. The fellow says he is using the slip rings to make the USB camera connections. I can believe that it's a wireless webcam transmitting an image and he is just sending power through the slip rings. Or are you saying that you are sending the a noise-free video image through the slip rings?

    • Yup! I'm simply passing the USB connection through the slip ring. Noise isn't a problem (at least not in the sense that it would leave video artifacts) because of USB's (shockingly robust) comm protocol. If data packets fail CRC check, the host won't ACK and they get re-sent by the sender.

      In short, if you measured the practical transfer speed across the moving slip ring, it would be lower than in an uninterrupted USB cable (due to packets getting lost/corrupted and re-sent) but there's still more than enough capability left to pass webcam video!

  • Imaxinar DM / about 10 years ago / 1

    GREATLY appreciate that you are carrying the silicone wire in long lengths ! ! ! I'm not fond of having to splice 3 meter lengths of it to get to what I needed. I'll be ripping out the old wire (from Another vendor) and going with yours. I tend to build big....

    Now if we could just see long lengths of the smaller gauge in more than just Red & Black.. those of us with articulated assemblies would be thankful.

  • Member #50317 / about 10 years ago / 1

    Do you have strand counts on the silicone wire?

  • CrowDojo / about 10 years ago / 1

    OK those Slip Rings are seriously awesome :D Will admit that my heart sank a bit when I clicked on the pic and saw the price for the 3ring as I was expecting the 6ring to end up being more expensive. Fair disclosure I am a legendary tightwad. I'm glad I did a search because at half the price for double the connectors (tho admittedly not as beefy in the amperage department) the 6 ring is freaking sweet :D

    Definitely going to be picking one up to set up a usb camera It is literally the perfect part at the perfect time for the platform I'm working on. :D

  • Member #403458 / about 10 years ago / 1

    Genuine Panther RC Rock Crawling tires...impressive!

  • tiagofumo / about 10 years ago / 1

    when robert is talking about the wires there is a kid talking to a woman while she is carrying a box that is like half her size and the kid didn't help her. They talked till the end of the video and not only the kid didn't help her but also she could have just put the box on the ground while they were talking.

    • Member #151148 / about 10 years ago / 3

      Don't worry, I am ok. The box was big but not heavy at all. It was just a card reader with a lot of padding for shipping.

  • How low in temperature can the silicone wire can go to? In cold weather? At what temperature it start to lose that flexibility.

  • n1taz / about 10 years ago / 1

    Do you guys sell those parts boxes with the red latches I see in Nick's work area? If not do you have a part number and manufacturer?

    • Hey man, Aren't they great??

      We don't actually sell those, but they're available from GlobalIndustrial. I'll do a blog post before too long about the way my new shop is organized. Those parts bins with the red latches are inexpensive Homak Brand Organizers which happen to fit beautifully, side-by-side, in this particular size of Nexelate wire shelving

      This was my (sort-of) thrifty response to Adam Savage's incredible Sortimo boxes and it's working out fantastically so far.

      If anyone from GlobalIndustrial is reading, can I get a piece of the action $$$ from these web-referrals? :P

      • SuperCrackMunkey / about 10 years ago / 1

        That's almost identical to the ones I use which can be picked up on the cheap at Harbor Freight usually.

      • ME heat o nator / about 10 years ago / 1

        I would love to get community feed back on optimal bench set up. I know the twitter contest is going on now, but I didn't see an entry for bench set-up. I am looking to rework mine and am short on input.

      • n1taz / about 10 years ago / 1

        Nick thanks for the info. I saw them in last weeks new products post and meant to ask. I liked the Adam Savage's setup too, but the price was a little prohibitive. Looking forward to the post about your shop I am thinking of setting up an extra monitor for standing work like yours as well.

Related Posts

Sense & Transmit

Recent Posts

Tags


All Tags