SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
Hello again. This week we have a few products and a couple product-specific videos. Don't worry, the Friday New Product Post Video didn't go away, we just did individual videos again this week. Let's get right to it, here are the products for this week.
Wouldn't it be cool if you could integrate LEDs into your Danish-made interchangeable plastic building block system? The Build Upons let you do exactly that! They snap directly into your favorite name-brand building bricks and work like a normal LED. Each 10 pack comes with 2 of each of 5 colors. Want to see them in action? Check out this video:
The Teensy LC is a breadboard-friendly development board with loads of features in a, well, teensy package. The LC is a low cost version of the popular Teensy that has a lot of the same features, but at a lower price. The processor on the Teensy also has access to the USB and can emulate any kind of USB device you need it to be, making it great for USB-MIDI and other HID projects. The 32 bit processor brings a few other features to the table as well, such as multiple channels of Direct Memory Access and an I2S digital audio interface! There are also 4 separate interval timers plus a delay timer! It's a cool little board.
The FEZ Spider Tinker Kit is a 100% open-source (hardware and software) .NET Gadgeteer compatible mainboard running .NET Micro Framework. This tinker kit enables users to program the FEZ Spider and its add-on modules from Microsoft’s Visual Studio using C# or Visual Basic, allowing developers to take advantage of the extensive built-in libraries for networking, file systems, graphical interfaces, and peripherals. Nick put together a little demo and explains what's included in the kit. Let's watch.
Classic Nick. That's it for this week. We'll be back again next week with more new stuff, so be sure to check back then. Thanks for reading and watching.
Uh, can you imply compatibility with Danish-made interchangeable plastic building blocks if only half of it is there and the other half is blocked by wires?? Also I found it odd that 2 of your three demos did not utilize the interlocking feature at all and would have been just as easy to do with standard LEDs. Hope there is an improved version in the future.
I was thinking the same. Perhaps a version that is compatible with the electrical connector bricks? http://www.brickowl.com/catalog/lego-electric-wire-with-plates-16cm-long-75938
hyw
Could you make some BuildUpons that have the leads coming out of the side of the block and allowing the bottom to be a normal ... Danish-made interchangeable plastic building block system bottom?