The Field Guide to Arduino

Just in time for Arduino Day, we're bringing you the magic of infographics.

Favorited Favorite 3

With Arduino Day fast approaching, we're doing a lot of thinking on everyone's favorite development board. We're practically up to our knees in Arduino here at SparkFun, so it can be easy to forget that not everyone is familiar with it, especially in all of its varied forms. So, in an effort to help you identify these species, we've decided to step back and take a 30,000-foot view at the world of Arduino. What follows is a handy field guide to help you navigate the woods and plains of Arduinostan... Arduinoland? The People's Republic of North Arduino. We can workshop the name later. For now? You'd best familiarize yourself with its wild inhabitants:

SparkFun Field Guide

PDF


Comments 12 comments

  • saccade / about 9 years ago / 3

    A PDF might be a more convenient reading format than a big, tall JPEG.

  • joelspark / about 9 years ago / 1

    Is that a typo or an easter egg? "What is a Michaelcontroller?" :D

  • Professor Paulsen / about 9 years ago / 1

    I would like very much to have a downloadable PDF of your booklet Field Guide to Arduino. It must be printer friendly.

    Professor Chuck Paulsen 203-270-0103 wcpaulsen@earthlink.net

  • Member #460847 / about 9 years ago / 1

    Thanks for the PDF, But would make a version that was easy to print.

  • ameyring / about 9 years ago / 1

    A nice summary since I don't usually keep up with the developments unless I need to find a board for a project. BTW, "Duemilanove" is misspelled on the first page. On the Lilypad page, "Wear it Out!" is misleading in a funny way - how about just "Wear it!"? :)

  • Member #141281 / about 9 years ago / 1

    Curious why the Teensie's weren't included.

  • Robert / about 9 years ago / 1

    Wait, an ATMega168 is more powerful than an Amiga 4000? Sacrilege! I demand a recount!

    • Yea, that comparison chart isn't even wrong. It is so obviously fraudulent that they probably should update that part of it. Any AVR would be totally smoked by a 286 and demolished by a MC68000 series chip beyond a couple of carefully staged tests where the AVR has advantages like hardware multiply and DES/AES support. 640KB of ram might not be enough for anyone but it certainly beats the pants off of 8K, which is the most any AVR has in it. Even when you add in the flash, the most a normal AT MEGA can have is 512KB and you are doing PC style segmentation as soon as you go beyond 64K and it really gets annoying beyond 128K.

      Where the AVR wins is both performance per dollar and watt. Those are plenty good enough reasons to use it, no need to embellish the truth.

      • Hey guys, this comparison is in instruction speed only (as indicated by the graph labels in MIPS)

        We understand that MIPS is not a measurement of computing "power" and that the richness of the instruction set, branching, etc. play a key role in determining the speed and performance of a CPU. That being said, MIPS is still a really good measure of task performance speed and we don't feel that it's disingenuous to compare the 168 to legacy hardware on those grounds.

        Sorry if it bummed you out, frankly, I think it's a pretty cool comparison. No one here is trying to say that an ATmega would be better than any of those computers at their given application.

        • scharkalvin / about 9 years ago / 1

          I figured that you might be only looking a MIPS. I don't remember what the clock speed was on the old VAX11-780 was, but it was considered a supermini computer at the time. With the ability to address megabytes of 32 bit wide memory comparing it to an ATmega328 is a bit lame. The atmega might be able to sprint by the VAX in a few well placed subroutines, but it would lose the race in total work done. OTOH a $35 RPI might give the old VAX some cause for embarrassment, especially if you hooked up a "small" disk drive to it via a USB-SATA adapter!

  • ME heat o nator / about 9 years ago / 1

    I love it. Long live the long since dead Arduin!!!

Related Posts

Recent Posts

Tags


All Tags