×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

T³: Making Things Move with the Edison

Let's dissect another section of EdiBot 2.0 and learn how to spin DC motors with Python.

Favorited Favorite 1

The Intel® Edison offers a few interfaces for working with hardware peripherals, and we have four Pulse Width Modulation (PWM) pins at our disposal. However, the PWM functions are fairly limited when compared with microcontrollers. For example, the I/O voltage is 1.8V, and you can only select a frequency between 4.6Hz and 4.688kHz in discrete steps (see Section 4.8 of the Edison Hardware Guide for more information).

That being said, the PWM, with some amplification, is enough to drive some gearmotors for a simple robot.

EdiBot 2.0 with motors

Slightly less of a wiring mess than the original EdiBot

On the original EdiBot, I had trouble driving the four gearmotors on the Rover 5 chassis from just the Edison, so I took the long way around: Edison sends UART commands to an Arduino running Firmata, which then sends out the necessary PWM and DC voltage signals to the now-retired Rover 5 Driver Board.

alt text

Original EdiBot electronics: Yup, it was as bad as it looks.

To control the motors on the revised EdiBot 2.0, I used:

Even though the micro gearmotors are rated for 6--12V, we can get them spinning with a measly 4.2V (from the Edison's Vsys), and they have enough torque to move a little bit of weight (say, a lightweight acrylic chassis and some electronics). I also wasn't worried about drawing too much current, as the TPS62065 on the Edison Base Block could provide up to 2A, and the stall current on each of the motors was listed as 360mA (at 6V).

By connecting the motors to the A1, A2, B1 and B2 pins on the H-Bridge Block and soldering the "VSYS->VIN" jumper closed, we could construct a basic differential drive for the robot.

EdiBot 2.0 differential drive motors

EdiBot 2.0 drive system

All we need to do is put a caster on the back of the chassis and we're good to go – now driving the motors at different speeds causes the whole robot to turn. One thing to note, however, is that the low voltage being supplied to the motors means that we really can't supply any less than about 50 percent PWM.

Full EdiBot drive system

If you look closely, you can see the caster under the battery wires.

Upload the following Python code to the Edison to try out the differential drive:

import time
import mraa

# False: A is right, True: A is left
swapMotors = True

# Motor parameters. Set to 1 or -1 to change default direction
leftDir = 1
rightDir = 1

# PWM A (pin 12) is on pin 20 in MRAA
pwmA = mraa.Pwm(20)
pwmA.period_us(1000)
pwmA.enable(True)

# PWM B (pin 13) is on pin 14 in MRAA
pwmB = mraa.Pwm(14)
pwmB.period_us(1000)
pwmB.enable(True)

# Direction pins A1 and A2 are on GPIO 48 and 47 (33 and 46 in MRAA)
a1 = mraa.Gpio(33)
a1.dir(mraa.DIR_OUT)
a1.write(1)
a2 = mraa.Gpio(46)
a2.dir(mraa.DIR_OUT)
a2.write(1)

# Direction pins B1 and B2 are on GPIO 15 and 14 (48 and 36 in MRAA)
b1 = mraa.Gpio(48)
b1.dir(mraa.DIR_OUT)
b1.write(1)
b2 = mraa.Gpio(36)
b2.dir(mraa.DIR_OUT)
b2.write(1)

# Assign left and right motors
if swapMotors:
    leftPwm = pwmB
    left1 = b1
    left2 = b2
    rightPwm = pwmA
    right1 = a1
    right2 = a2
else:
    leftPwm = pwmA
    left1 = a1
    left2 = a2
    rightPwm = pwmB
    right1 = b1
    right2 = b2

# Standby pin is GPIO 49 (47 in MRAA)
standby = mraa.Gpio(47)
standby.dir(mraa.DIR_OUT)
standby.write(1)

# Differential drive. A and B can be -1 to 1.
def diffDrive(leftSpeed, rightSpeed):

    # Make sure the speeds are within the bounds
    if leftSpeed < -1.0:
        leftSpeed = -1.0
    if leftSpeed > 1.0:
        leftSpeed = 1.0
    if rightSpeed < -1.0:
        rightSpeed = -1.0
    if rightSpeed > 1.0:
        rightSpeed = 1.0

    # Set motor speeds
    leftSpeed = leftDir * leftSpeed
    rightSpeed = rightDir * rightSpeed
    if leftSpeed < 0:
        left1.write(0)
        left2.write(1)
        leftPwm.write(abs(leftSpeed))
    else:
        left1.write(1)
        left2.write(0)
        leftPwm.write(leftSpeed)
    if rightSpeed < 0:
        right1.write(0)
        right2.write(1)
        rightPwm.write(abs(rightSpeed))
    else:
        right1.write(1)
        right2.write(0)
        rightPwm.write(rightSpeed)

# Test the differential drive
diffDrive(0.8, 0.8)
time.sleep(1)
diffDrive(1.0, 0.6)
time.sleep(1)
diffDrive(-1.0, 1.0)
time.sleep(1)
diffDrive(-0.7, -0.7)
time.sleep(1)
diffDrive(0.0, 0.0)

That code should cause the robot to do a little dance: move forward, turn one way, spin another, back up, and stop. This differential drive code was used as the basis for EdiBot 2.0. The robot can locate a yellow object in its field of view, drive to face it, and back up if the yellow object takes up too much of the frame.

Demonstration of EdiBot 2.0 chasing a ball

Want to make your own EdiBot 2.0? A full step-by-step tutorial can be found here.


Comments 4 comments

  • Member #394180 / about 8 years ago / 1

    I ended up doing something like this with my old Magician Chassis. I also used the Edison and dual H-bridge block, but I soldered male pins onto the board and just slipped jumper wires onto them.

    The other Edison feature I used was the access point mode. I wrote a javascript server that runs on the Edison and interfaces with the H-bridge so I'm able to steer the robot with a web interface GUI (usually on a mobile device). It's fun to have the robot attempt to "socialize" with our cat herd. The herd, BTW, can easily hear the ultrasonic rangefinder used by the robot. Spooky.

Related Posts

Recent Posts

Tags


All Tags