Pi Day is upon us again and to celebrate we've put some of our most popular Raspberry Pi items on sale. From the excellent Pi-Top lineup to the SparkFun PiRetrocade, today is the day to slice yourself off a great Pi product. And if you haven't gotten your fill of Pi, check out this handy Pi facts infographic we put together.
Rules: Sale prices end 3/14/2017 at 11:59pm. Sale prices apply to customer and guest accounts only. No backorders allowed on sale items.
Happy 3.14!
Once again we get to celebrate by eating round objects and increasing our circumference! Happy Pi day:)
But rember, you can only eat half a pie on pi day
So the Model B+ and Model 2 are two-dimensional objects, and the rest are 3-dimensional?
Also, 1k mA? Seriously? 1A or 1000mA, not 1k mA… preferably 1A.
That "Model 2", that's what is commonly referred to as B+, right? Also, why is the vertical dimension missing from Models B and 2?
I chuckled to "weight in average tarantulas".
The graphic indicates that Pi Zero has two USB ports... That is nonsense. It's like saying the model A+ has two USB ports. The second one isn't USB, it's just a power connector.
That is correct. All Pi boards have a microUSB port for power including the Zero. The Zero also has a OTG port to connect your peripherals. We'll see about getting that updated.
I think @tetsujin was complaining about calling a power input a "USB port".
He has a point here. A "USB port" should also have the USB signal lines. Without the USB signalling, it is just a power input that happens to use a USB connector.