SparkFun's module shows up in an FCC study on body sensor networks. We've also got a new speedometer tutorial and some new products.
by
Nate
March 6, 2009 7:00 am UTC
8
Favorited
Favorite
0
Our friends at Nordic VLSI gave us a heads up that our nRF2401 breakout is being used in an FCC study. Near as I can figure, General Electric Healthcare (GEH) wants the FCC to open up the band from 2360MHz to 2390MHz for something called a 'Body Sensor Network' (BSN). GEH wants to snag a rather large slice of the spectrum pie and have it for themselves and their BSNs. Unfortunately this band overlaps with flight test telemetry systems and the Navy is a bit concerned.
Johns Hopkins Applied Physics Labs ran the tests. They had to come up with a way to tell if a new BSN device operating in this 236-2390MHz band would interfere with flight test operations. Checkout the hack they did to push the 2.4GHz Nordics into the 2.3GHz band:
"To permit the Nordic chips to operate in the AMT band, the 16.00 MHz surface mount crystal was replaced by a 15.36 MHz crystal. This shifts the operational frequency range of the Nordic transceiver from 2400 – 2525 MHz to approximately 2300 – 2425 MHz. With no further hardware changes whatsoever, the prototypes can operate at any frequency within this 125 MHz band."
"The Figures also illustrate the manner in which two devices, one in transmit mode and one in receive mode, can communicate at a distance of two miles by connecting the receiver to a 15 foot diameter parabolic dish AMT receive antenna and low noise amplifier combination at Patuxent River..."
Where's that 15-ft parabolic when I need one?
Checkout Ryan's new tutorial on a
Digital Speedometer. Turns out his car was indicating 5mph over what his actual speed was!
Onto new products!
Product Update! The Arduino USB Board is now being shipped with ATMega328. The new Arduino USB board is still fully compatible with the Arduino IDE, contains twice as much memory, and uses a faster baud rate to upload sketches.
The
Powerline Communication Modem is a transceiver module designed to send and receive data transparently over power lines. Includes headers that are compatible with
XBee modules, as well as the two next items below. Wirelessly monitor your power hungry devices and decrease your carbon footprint!
I do my research work in this space, and I'm a big proponent of Bluetooth at 2.4Ghz. Bluetooth has a number of advantages :
- prevelance in existing electronics
- multiple protocol stacks implemented
- lower current consumption per bit than most other protocols
- higher data throughput
- high power & high data rate options available
- built-in DUN (dialup networking) allows for simplified telemetry over the cellualar network
etc..
I find the range of the 900-series Xbee's very interesting. Sad thing is, we in Europe can't use them as the frequencies these use are used for mobile phones. Are there any Xbee's that operatie in the 868MHz (or 433-434 MHz band)?
There is an amazing XBeePro for the European 868 MHz frequency.
To wet your apetite:
- 40 km RF LOS w/ dipole antennas
- 80 km RF LOS w/ high gain antennas (TX Power reduced)
- 128-bit AES encryption
Devkit containing two 868s, USB- and RS232-adapters: 99$!
Link: http://www.digi.com/products/wireless/point-multipoint/xbee-pro-868.jsp
Indeed. I got all excited only to be shot down by silly regulations. I'm trying to use the Xbees inside a warehouse and it seems not even the power of the Pro 50mW is enough to punch through the weirdness of that building.
One would expect any real Body Area Network (there's an IEEE draft for this) would use two-way data communications.
A test with a the narrow beamwidth of a 15dBi gain dish on one end is curious: such antenna gain would be irrelevant to a real system. So the range achieved is moot.
Moreover, it would seem that a standards-based MAC and PHY would be assessed for this need.
Aren't they testing to see whether their big flight testing-related antennae will pick up stray transmissions from the BSN-sized antenna?
The inline pics are swapped for the RS232 and RS485 interfaces, other than that sounds great!!! Any thing new about XBee is exciting!
Thanks Michael - the text placed below each image is a bit confusing, but the images and links are correct.