Friday Product Post: Raspberry Pi Zero W

The new Pi Zero W has made its way to SparkFun, along with everything you need to connect it up!

Favorited Favorite 0

Hello and happy Friday! We are very pleased to announce that we are now carrying the Raspberry Pi Zero W, as well as a whole slew of add-on parts to get you set up and started! On top of an enclosure and cables, we've also made a simple kit with every part you need in one box. Alright, let's take a closer look at what we have available this week.

Plenty of features at a ridiculously low price!

SparkFun Raspberry Pi Zero W Basic Kit

KIT-14298
5 Retired

The Raspberry Pi Zero W can be a bit tricky to set up with its unique power and cable requirements --- that's where this kit comes in. The SparkFun Raspberry Pi Zero W Basic Kit provides you with everything you need to get started with the newest Pi, all without breaking the bank or causing great difficulty. Inside each kit you will find a Raspberry Pi Zero W with a fully programmed NOOBS card, Mini HDMI and USB OTG cables, and a high-quality wall adapter.

Raspberry Pi Zero W

Raspberry Pi Zero W

DEV-14277
$15.00
48

Is all you need just the board? The Raspberry Pi Zero W is still the Pi you know and love, but at a largely reduced size of only 65mm long by 30mm wide and at a very economical price. With the addition of wireless LAN and Bluetooth(R), the Raspberry Pi Zero W is ideal for making embedded Internet of Things (IoT) projects. The Pi Zero W has been designed to be as flexible and compact as possible with mini connectors and an unpopulated 40-pin GPIO, allowing you to use only what your project requires.

Raspberry Pi Zero Case

Raspberry Pi Zero Case

PRT-14273
$5.95

The Raspberry Pi Zero Case has been designed to fit both the Pi Zero and the Pi Zero W. These official cases consist of several parts and protect the Raspberry Pi Zero from things like rogue wires that might short it out while still allowing full access to the board. Simply snap the RPi into the bottom half of the enclosure, then snap on a desired top. No tools required!

Raspberry Pi Zero Camera Cable

Raspberry Pi Zero Camera Cable

PRT-14272
$5.95
1

The Raspberry Pi Zero and Zero W are both equipped with a smaller CSI (Camera Serial Interface) port than on a full-sized Raspberry Pi board --- luckily, that's where this cable can help! The Raspberry Pi Zero Camera Cable replaces the pre-existing camera module cable, allowing your Zero or Zero W light and imaging capabilities.

Mini HDMI Cable - 3ft

Mini HDMI Cable - 3ft

CAB-14274
$5.50
2

This is an inexpensive 3-foot-long HDMI to Mini HDMI Cable that you can use to hook up your Raspberry Pi Zero W to a suitable monitor or TV.

Pi Zero Micro-B to USB A socket - 5in

Pi Zero Micro-B to USB A socket - 5in

CAB-14276
$3.50
1

USB On-The-Go (OTG) is a really useful USB specification! This 5-inch-long Female A to Micro-B cable allows some small devices that would usually be unable to act as a host to have limited hosting capabilities! USB OTG is common for things like tablet computers and smartphones in order to allow for USB peripherals like flash drives, keyboards, etc. to be hooked up.

Raspberry Pi GPIO Male Header - 2x20

Raspberry Pi GPIO Male Header - 2x20

PRT-14275
$1.05

This 2x20 male header has the same number and spacing of pins as a Raspberry Pi but is best served when used in conjunction with the Pi Zero since they come with a space of unpopulated headers.

And that's it! We hope you enjoyed all our new products this week and are able to get set up with the Raspberry Pi Zero W easily. As always, we can't wait to see what you make with these parts! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

Thanks for stopping by. We'll see you next week with even more new products!


Comments 8 comments

  • Great! Raspberry Pi is so increadible! Good Joob!

  • Member #394180 / about 7 years ago / 1

    Why is everybody limiting it (Pi 0 W) to 1 per customer? I had to go to Microcenter twice with 2 different friends to to get the 4 I needed. What's so wrong with giving the customer what they want without making them jump through silly hoops? You (retailers in general) know we'll get it anyway, it's just how much goodwill we'll have left for you at the end that's different.

    For that matter, why are the Raspberry Pi folks so brainless? Every version they've ever come out with has been an instant hit. Why don't they plan their production runs based on previously demonstrated demand?

    Just wondering. The world is weird enough today without artificial weirdness being added.

    • M-Short / about 7 years ago / 1

      Raspberry Pis are hard for most retailers. The demand is high, and the profits low (or in some cases non existent) and the distributor agreement limits what we can do. But everyone is limiting these to 1 because the Raspberry Pi Foundation requires us to do so. Unfortunately this means either we give you a limit of 1 or a limit of 0 (we don't carry it). Having gone to Microcenter with my dad and brother to buy Pi Zeros I understand your frustration, we'd love to be able to sell you 10 and make a profit, unfortunately that's not an option at the moment.

      • Member #394180 / about 7 years ago / 1

        OK, I'll save my disgruntlement for the foundation

  • Sembazuru / about 7 years ago / 1

    By using a hyphen as a bullet point in the video, it looks like that the RPi0W is running at negative 1 GHz... lol

  • Elimegrover / about 7 years ago * / 1

    Out of curiosity, was Sparkfun not licensed to Carry the RPi0? You guys are generally my go-to for this kinda stuff. It was a bit of a bummer I couldn't get any from you previously. Glad I can now though!

  • Applekid / about 7 years ago / 1

    Any chance you'll start carrying the original Pi Zero?

Related Posts

Recent Posts

Tags


All Tags