×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

Enginursday: Prototyping 3D Parts

A look at the design considerations of rebuilding the fiber optic mounts for my light suit to accommodate new fiber optics and LEDs

Favorited Favorite 1

So we just got this neat little 3D mouse up here in Engineering, and I'm finding just about every excuse to use it. I've been needing to perform some serious redesigns on a few components of my fiber optic light suit, mainly the fiber optic mounts.

alt text

They're a tad too large for my liking, and I'm also changing the fiber optic and LED that I'm using, so I'll need to devise a new way to get that light into the fiber. These original mounts also ended up failing on the printer quite a few times, and when they didn't fail, they didn't perform how I had originally envisioned them to perform, so we go back to the drawing board until our vision comes to fruition!

Version 2.0

So let's go over the issues with the original part that I'd like to remedy (Version 2.0, pictured below).

alt text

First of all, sometimes the scaffolding that holds up the left and right sides of the part ends up sagging under the heat of the printer, resulting in a part that won't hold an LED or fiber. To fix this, I'm going to change the design to get rid of scaffolding altogether; this way, there will be nothing to warp. This will also partially fix the second issue with the part --- it requires too much finishing after I take it off of the printer. Without any scaffolding, I'll have nothing that needs to be peeled off of the part. In the end this also makes for a much smoother and better-looking part. The final issue I was having was that the part would sometimes crack under the stress of being clamped down in the fiber optic. This can be fixed with a simple change of infill, so more of the inside of the part is full of plastic.

Print, Fix, Repeat

Getting a part just right often takes a few iterations, as the printer (or at least the Taz 6 I print on) has a little under a millimeter of error, which doesn't sound like a lot until you start printing parts with itty-bitty details. What I will usually do is adjust multiple features of the part at once, but for the purposes of this post, I'll only change one thing at a time from one version to the next.

alt text

Shown from left to right above are versions 2.01, 2.02 and 2.03. In these versions, I shortened the tube that holds the fiber and adjusted its size to fit my new fiber optic. In 2.01, the hole was too small. I overadjusted in 2.02, and the hole was too large. In 2.03, I found the Goldilocks zone, and the part grips perfectly. It's a little tough to notice in the photo, but each half of 2.03 is nearly perfectly flush with each other. This is because I used a rasp to smooth this face of the part to allow a tighter fit.

Now, I'd like to change the screw holes in order to allow for countersunk screws to keep the profile of the part free of bumps from hardware. In versions 2.04--2.06, shown below from left to right, I was adjusting hole sizes and countersink depth in order to get the screw holes perfect.

alt text

I ran into an issue here of a lack of support structure in my countersinks. Since the countersinks are on the bottom face of the part, the printer occasionally makes little beads of plastic around the edge of the hole due to a lack of support structure. This makes my countersink a bit of an imperfect hole, and the nut doesn't sit perfectly without a careful drilling out of the countersink. However, I fixed the problem of a serious amount of hardware hanging off of the part. I'm going to go ahead and call it a success, as I've reduced the finishing of the part to only two steps: the rasp on the faces that are in contact with each other, and milling out the countersink.

I'll have to do a few more iterations once I receive the LEDs and boards to ensure they attach and fit correctly, but PCB manufacturers do occasionally take a little bit of time to make boards, so that update will come in time. The final version that I'm currently happy with is shown below.

alt text


Comments 4 comments

  • Sembazuru / about 7 years ago / 2

    Technically, you aren't using countersinks for relief for your machine screws, you are using counterbores.

    Other than that, great write up on the importance of small incremental steps when iterating designs. Yes, it takes longer, but easier to track changes and in some cases more clarity on what change caused what effect.

    • Woops! This is what I get for attempting to sound like a Mechanical Engineer. You're absolutely right though, small changes are the key to knowing what may be going wrong in a part. When I do make multiple changes in a single iteration, I try to keep them in different areas of the part so they are unaffected by each other.

      • Sembazuru / about 7 years ago / 1

        To be fair, I was nearly positive that countersinks are always conical but wasn't sure enough to post until I did my own research. ;-)

  • Member #1212220 / about 7 years ago * / 1

    thank you for the information about prototyping using 3d printing. it also helps me to learn about 3d printers and also for my online shop. https:// printyoursolution.com

Related Posts

Recent Posts

Tags


All Tags