Enginursday: "I've got a really good feeling about this"

Let's add some electricity to your favorite things. I take a LEGO® speeder from Star Wars® and use Arduino to give it a little something extra.

Favorited Favorite 3

I have countless fond memories of building and creating LEGO® sets as a kid. Those simple bricks gave me creative freedom to make what I wanted and not be afraid to fail. Now as an engineering student, I've grown apart from the toys that played such a major part in my development as both an academic and a person. Through years of exams and school projects, I've developed a fear of failure, and a hesitation to pursue my craziest ideas.

When building with bricks, I didn't stop myself before trying something that may have seemed absurd, I just went for it. Interning at SparkFun has made me realize how important that freedom is and how much I've missed it. If I've learned anything from my time here, it is that you shouldn't be afraid to embrace who you are and to try something different, no matter how crazy it may sound. It is this philosophy that inspired me to make something I was passionate about using some SparkFun components, a drill and some LEGO® bricks.

First of all, I'm a huge Star Wars® fan so you can probably guess what kind of set I picked out as the base of my project – a speeder belonging to a certain scruffy-looking nerf herder by the name of Han Solo caught my eye.

The completed set prior to modifications

LEGO® Han Solo's Landspeeder™

This is what the completed set looks like. Seem familiar? Han Solo used this same vehicle to escape Lady Proxima before leaving Corellia in Solo: A Star Wars Story™. The opening scene shows Han hot-wiring this speeder and the boosters flickering to life. The suspense and the imperfection in the speeder struggling to ignite was an effect I wanted to replicate as I set out to modify this vehicle.

But before I got too far, I needed to understand the infrastructure of the set. While assembling the speeder I focused on understanding the methodology behind the design. I wanted to know what parts were vital and if any bricks could be removed to make room for some electronics. The next step was determining how I could give the final design more life. I wanted to transform the speeder into something more dynamic and realistic.

Finding the best place for the LEDs

Two blue booster LEDs and one white headlight LED

The rear of the landspeeder includes two wheels in place of the boosters. I also noticed there was a wheel in the front, ideal for a headlight. That's when the idea for LEDs popped into my head. Lights could be used to add to both the aesthetics and functionality of the speeder. Each wheel has room for an LED and, using a drill, I was able to make small holes for the leads. Getting the leads into these holes took some patience, but the LEDs fit well in the end.

Before putting the boosters back on the speeder, I needed to make room for wires, sensors and a microcontroller. For the brain of the speeder I wanted something small and easy to program. The blue and white LEDs I utilized operate at around three volts; this made the 3.3V Arduino Pro Mini perfect for this project. I also wanted a sensor to actuate the LEDs.

Seeing as this is a landspeeder, I thought it would be fitting if the LEDs turned on when you set the speeder down and turned off when you picked it up. To do this I used a time-of-flight range finder sensor, which detected the distance between the speeder bed and any object below it.

Arduino Pro Mini 328 - 3.3V/8MHz

Arduino Pro Mini 328 - 3.3V/8MHz

DEV-11114
$10.95
54
SparkFun ToF Range Finder Sensor - VL6180

SparkFun ToF Range Finder Sensor - VL6180

SEN-12785
$29.50
11

E-Textiles Battery - 110mAh (2C Discharge)

PRT-13112
6 Retired

Once I had my hardware, I needed to find a place to store it. I wanted the electronics to be as hidden as possible, so I took what I learned from the initial build and hollowed out the front end of the speeder, which was not vital to the overall structure of the set.

Filled speeder hood Empty speeder hood
The speeder hood as designed by LEGO®. These bricks add to the aesthetics of the set, but are not required. The speeder hood emptied to allow room for the Pro Mini, battery and various wires.

This front compartment will have room to fit both the Pro Mini and a battery to power the whole circuit. There was still no room in this space for the range finder sensor, so I had to make space on the bottom of the speeder.

Original undercarriage Empty undercarriage New undercarriage
The speeder undercarriage as designed by LEGO®. More room needs to be made for the range finder and for the wires attached to the LEDs. The emptied undercarriage. The redesigned undercarriage with additional open space.

After redesigning the base of the set, I topped it off by drilling a large hole to bridge the undercarriage and the front compartment. This allows for wires from the LEDs and range finder to reach the Pro Mini without needing to wrap completely around the speeder.

The next step was to make sure I got the circuit working. I grabbed a breadboard, some jumper wires, a switch, LEDs, the range finder and the Pro Mini, and got to work. The two blue LEDs, connected to the boosters, share one digital pin, as they will be lit at the same time. The white LED, acting as the headlight, will be connected to a separate digital pin. The range finder will communicate using I2C, meaning the sensor will require four connections: ground, power, SDA and SCL.

Complete circuit diagram for the solo speeder

The landspeeder circuit

After completing the circuit and checking connections, I uploaded some simple code to insure the LEDs were all working.

As I continued developing more detailed code, I thought back to my original inspiration. Simply turning the LEDs on didn't seem exciting enough. There is a risk involved, an uncertainty in the movie. I decided to program the booster lights to flicker at start-up a random number of times for a random duration, then fade from darkness to full brightness as the speeder comes to life. I then added the headlight sparking to full brightness, as to illuminate the darkened streets of Corellia.

To bring the risk to the next level, I programmed the ignition to, at random, fail at start-up. In this case the boosters will still flicker but they will instead fade to darkness and the headlight will brighten for less than a second before also shutting off. In the end, my code looked like this:

//Solo Speeder
//Author: Jackson Hootman
//SparkFun Electronics
//July 20, 2018

//Arduino 1.8.5
//Arduino Pro Mini 3.3V 8 MHz

//required libraries to use range finder
#include <Wire.h>
#include <SparkFun_VL6180X.h>

//pin definitions
#define blue 10
#define white 11

//distance triggers (in mm)
#define distLlim 20
#define distUlim 35

//I2C address of range finder
#define VL6180X_ADDRESS 0x29

//Initialize range finder
VL6180xIdentification identification;
VL6180x sensor(VL6180X_ADDRESS);

//variable for storing distance from speeder bed to ground
int dist;
//values for which startup will fail
int loser[6];
//value of startup
int event;
//is the speeder grounded?
boolean grounded = false;

void setup() {

  //Start Serial at 115200bps
  Serial.begin(115200);
  //Start I2C library
  Wire.begin();
  //LEDs to output
  pinMode(blue, OUTPUT);
  pinMode(white, OUTPUT);
  delay(100);

  //Initialize device and check for errors
  if (sensor.VL6180xInit() != 0) {
    Serial.println("FAILED TO INITALIZE");
  };

  //Load default settings to get started
  sensor.VL6180xDefautSettings();
  delay(1000);
}

void loop() {

  //find distance to ground
  dist = sensor.getDistance();
  //print distance
  Serial.print("Distance measured (mm) = ");
  Serial.println( dist );
  Serial.println();

  //if put on the ground
  if (dist < distLlim && grounded == false) {
    Serial.println("Attempting ignition...");
    //attempt ignition with a number of flickers between 1 and 20
    ignition(random(1, 20));

    //if successful
    if (caseGen()) {
      Serial.println("Engines stable");
      //Boosters fade to bright
      for (int m = 0; m <= 255; m += 5) {
        analogWrite(blue, m);
        delay(50);
      }
      //all lights on
      digitalWrite(blue, HIGH);
      headlight();
      digitalWrite(white, HIGH);
      //speeder grounded
      grounded = true;
      Serial.println();
    } else {
      //if not successful, turn lights off
      Serial.println("Engines failure");
      for (int n = 255; n >= 0; n -= 5) {
        analogWrite(blue, n);
        delay(50);
      }
      digitalWrite(blue, LOW);
      headlight();
      digitalWrite(white, LOW);
      grounded = true;
      Serial.println();
    }
  }

  // if lifted off the ground, turn LEDs off
  if (dist > distUlim && grounded == true) {
    Serial.println("Deactivated");
    powerDown();
    //grounded now false
    grounded = false;
    Serial.println();
  }
  delay(500);
}

void ignition(int delays) {     //Ignite booster engines

  //array holdeing 3 different delay lengths
  int delaylen[3];

  //assigning random delay lengths
  for (int j = 0; j <= 2; j++) {
    delaylen[j] = random(10, 50 * j + 25);
  }

  //boosters flickering
  for (int i = 1; i <= delays; i++) {
    digitalWrite(blue, HIGH);
    delay(delaylen[random(0, 2)]);
    digitalWrite(blue, LOW);
    delay(delaylen[random(0, 2)]);
  }
}

boolean caseGen() {     //Generate random result

  //is ignition successful
  boolean result;

  //assigning values of startup failure
  for (int k = 0; k <= 5; k++) {
    loser[k] = random(1, 10);
  }

  //event will be randomized at an integer between 1 and 10
  event = random(1, 10);

  // if event integer is equal to 1 of the integers in the loser array, ignition will fail
  if (event == loser[0] || event == loser[1] || event == loser[2] || event == loser[3] || event == loser[4] ||         event == loser[5]) {
    Serial.println("Ignition failed... Lady Proxima is on your tail!");
    result = false;
  } else {
    Serial.println("Ignition success... I've got a really good feeling about this");
    result = true;
  }
  return result;
}

void headlight() {      //Flicker headlight

  digitalWrite(white, HIGH);
  delay(100);
  digitalWrite(white, LOW);
  delay(100);
}

void powerDown() {      //Turn lights off

  for (int p = 255; p >= 0; p -= 5) {
    analogWrite(blue, p);
    analogWrite(white, p);
    digitalWrite(blue, LOW);
    digitalWrite(white, LOW);
  }
}

With the code completed, the next step was to mount the sensor, microcontroller, switch, boosters and headlight to the speeder. I used hot glue to attach the switch, range finder and the Pro Mini to detachable bricks. This way, the components won't be permanently fixed to the base plate of the set. I used 22-gauge wire to make all the electrical connections in this project. In cases where I needed to solder wire to an LED lead, I covered the solder joint with heat shrink wrapping.

Blue 22 gauge wire soldered to a blue LED

Twist the stripped, 22-gauge wire around the LED lead then add solder

I chose wire colors that complimented the color scheme of the landspeeder, which largely added to the overall look of the set. The key here is to be subtle with your wiring. You don't want it to overpower everything else. At the same time though, you want the wires to be evident. They give the speeder a futuristic look authentic to the Star Wars universe. Adjusting everything to fit was a bit of a puzzle, but like the entirety of this project, I enjoyed the creative problem solving it took to get the job done.

When the speeder is set down the booster lights flicker, then power on. After the boosters are on then the headlights will power up

The final product in action

The most difficult process during the speeder's construction was taking the working circuit and transferring the wiring and components to a less user-friendly environment. The soldering was slow and the placement of parts was delicate but above all, it was exciting seeing an idea of mine come to life. Taking a thought and making it real, in the end, was the whole purpose of this project: to try something, to have an idea and pursue it.

The landspeeder's electronic components

So for anyone reading, I challenge you to embrace your nerdiness, to pursue the absurd, and to try something new. Take something you're passionate about and make it better. Take an idea and make something completely new. Don't let a fear of failure slow you down, let curiousity guide you, and learn about something that's fascinating to you.

I already have countless ideas to build on this project, and even more ideas for new and bigger projects. It seems as though, at least in my case, the biggest step was getting started. Once I took that fist step, I was able to step away from the style of learning I had adopted in school. I experimented because I was curious, I took the time because I was invested and I tried because I had an idea and I wanted to see it become reality.

Landspeeder functionality in darkness

So good luck out there, makers! I hope you find a project that makes you as excited as Han Solo is about making the Kessel Run in 12 parsecs. And if you want to give this project a go, check out these helpful links to get you started:

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

VL6180 Hookup Guide

Get started with your VL6180 based sensor or the VL6180 breakout board.

How to Use a Multimeter

Learn the basics of using a multimeter to measure continuity, voltage, resistance and current.


Comments 5 comments

  • Member #134773 / about 6 years ago / 2

    Great project! Thanks for sharing!

    I do have one question: I assume that the LEDs you used have built-in limiting resistors? You don't show the resistors in the schematic. (LEDs without resistors will quickly let the "magic smoke" out of things...)

    I'm a tad bit envious, as 50+ years ago when I was a kid I didn't get to have any LEDO® sets -- my mother claimed they were too expensive. (She also accused me of taking my allowance money down to "Radio Shack and throwing it at them" -- I heard the last of that when in the mid-70s I was making more per hour as a factory electronics technician than my father was as a heavy equipment operator working for the state highway department.)

    One other comment about LEGO® sets: they used to have sets that included gears and such -- every year I'd buy one or two of these and donate them to one of the local toy drives in the hope of inspiring an unknown child to reaching higher. I was really irked when they dropped those lines.

    • Are you referring to the LEGO® Technic line? I remember those as a kid, as well. Lots of fun building working contraptions with motors, gears, pneumatics, etc. That line still exists, but it seems to focus a lot on form over function. It still seems like all the gears and functionality is there but just hidden under custom plates.

    • Action Jackson / about 6 years ago / 1

      Thanks for reading! As for the limiting resistors, the white LED requires an input voltage of 3.2-3.4V and has a maximum current of 20mA. The blue LEDs require an input voltage of 3.0-3.4V and also shouldn't exceed 20mA of current. The board I used runs at 3.3V logic and with the small lithium ion battery I used, the current draw was well below the maximum values. I didn't include limiting resistors in mine so I could get a nice brightness out of the blue LEDs but for longevity sake I completely agree that adding limiting resistors is a great idea.

      And I remember building sets that included gears too. They definitely add a functionality to the set that I always really appreciated.

  • Member #1414076 / about 6 years ago / 1

    Absolutely crushed it. I loved how there was a story behind the project. I felt it was very relatable for older generations and reemphasizing how important it is to go back to your roots and allow yourself to explore and be creative again. In a sense taking a child’s toy to the big kids level. Excellent writing skills and instructions. 10/10. Job well done.

Related Posts

Makers You Should Know

Recent Posts

Tags


All Tags