SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
Hello, everyone! This week we have two new Artemis boards available, one in our Feather-compatible Thing Plus footprint, and the other as our new Edge 2 iteration. In addition, we are also releasing a new Qwiic-enabled Motor Driver to make your next robotics project as easy to set up as possible! Rounding out the week we have a USB 2.0 microphone used in our TJBot Kit that we hope can get some good use outside of the kit, as well. Now, let's jump in and take a closer look at all of our new products for the week!
If you are looking for a board that (almost) does it all, look no further! The SparkFun Artemis Thing Plus takes our popular Thing Plus footprint and adds in the powerful Artemis module for ultimate functionality. Fully compatible with SparkFun's Arduino core, the modern USB-C connector makes it easy to program under the Arduino IDE, but for more advanced users who prefer to use the power and speed of professional tools, we've also exposed the JTAG connector. To make the Thing Plus even easier to use, we've moved a few pins around to make the board Feather-compatible, and it utilizes our handy Qwiic Connect System, which means no soldering or shields are required to connect it to the rest of your system!
The SparkFun Qwiic Motor Driver takes all the great features of the Serial Controlled Motor Driver (SCMD) and miniaturizes them, adding Qwiic ports for plug-and-play functionality. Boasting the same 4245 PSOC and 2-channel motor ports as the SCMD, the SparkFun Qwiic Motor Driver is designed to communicate over I2C to make setting up your next robotic project as fast and easy as possible! Utilizing our handy Qwiic system and screw terminals for motor and power hook-up, no soldering is required to connect it to the rest of your system.
This is a tiny USB Microphone from Kinobo that plugs into your laptop, desktop, Raspberry Pi, Jetson Nano Dev kit or anything with a USB port you may be using as a computer. There is no need to install any extra software as your OS should detect the device and automatically install it. Simply launch a program that requires microphone input, and away we go!
That's it for this week! As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!
very helpful, i was hesitating to buy coz i need to look for better specs of this and this one sure helps a lot.