Alternate Vision Through Distance Sensing Glasses

Distance sensing combined with haptic feedback create a way to "see" the world around you.

Favorited Favorite 0

When one of Thomas Sullivan's friends lost sight in one eye, Sullivan decided to design a device to help with peripheral vision. The feedback he received was so overwhelmingly positive, he decided to design a pair of glasses that combined distance sensing and haptic feedback to allow the wearer to form a mental image of the three-dimensional space in front of them.

alt text

While Sullivan continues to share his design with friends and family, he ultimately hopes that someone will take the design even further to allow for more widespread testing and access.



Comments 1 comment

  • Member #134773 / about 4 years ago / 1

    Three comments (hopefully "constructive") for Mr. Sullivan:

    Since the sensor has Qwiic connectors by default, I would have been inclined to do the electrical connections by taking a Qwiic cable, and clipping it in two, stripping the ends of the wires, and soldering them to holes close to the Trinket. This would greatly simplify experimenting with other (hopefully Qwiic enabled) sensors, rather than having to unsolder/resolder them.

    A second thought is that rather than 3-D printing the "frames", get a pair of "reading glasses" (they're cheap -- Walmart, Target, Costco, etc. for sources) and remove the lenses. You'd have to do some "tinkering" to connect the breadboard, but they'd have the advantages of having hiinges built in as well as having (relatively) comfortable nose pieces. Also, the side pieces, being metal, could be bent if necessary, to provide a better fit.

    The third thought is that with the slightly-lamented demise of Radio Shack, nibblers can be hard to find. FWIW, I've gotten them from Digi-Key.

Related Posts

Recent Posts

Halloween Hacking

SparkFun Spooktacular

Tags


All Tags