Announcing the new micro:bit v2

The second iteration of micro:bit is now available, with new SparkFun kits to go along with it!

Favorited Favorite 0

Over the past few years, we have seen the micro:bit grow into one of the most useful programming tools available. Here at SparkFun, we even developed and released a whole ecosystem of carrier boards and kits for it. The micro:bit became our top selling educational platform within a year of its release. Since then, it has been a steady rock for STEAM education in a time of uncertainty while most students participate in school at home. The micro:bit is easy to program, easy to administer and affordable enough to send home with students.

All of that being said, this week marks an exciting moment for the micro:bit: the announcement of micro:bit v2! Here is a sneak peek on what's new on the micro:bit v2 to look forward to.

micro:bit v2 Front

micro:bit v2 Back

Before jumping into the new additions, here's a quick comparison for you table nerds out there.

micro:bit v2 Features Table

New Brain

Not that the older version of the micro:bit was a scarecrow by any means - it was pretty hefty in terms of computing power - but there were some users, specifically those looking to get the most out of Bluetooth, who were pushing the micro:bit to the limits.

New micro:bit v2 Back

The micro:bit v2 sports a new Nordic nRF52833 and doubles the amount of flash memory on the board. This updates a number of features, speed and power consumption on the micro:bit. One thing we are looking forward to is its potential to open the doors to Artificial Intelligence (AI) and machine learning (ML) for your micro:bit projects (this is just us speculating - there is nothing to point at in terms of the micro:bit Foundation and its partners rolling out AI/ML out of the gates, but it does have potential in the future). We will keep an eye on this prospect.

Audio Upgrade

Since the release of the original micro:bit, students have always been able to have fun programming the micro:bit to play music and sounds, sometimes through an external speaker. This was always a bit of a letdown for those getting into micro:bit, as it was something they had to add on to the hardware.

Close up of the micro:bit v2 Back

We’re glad to see that the micro:bit v2 has a built-in speaker. The speaker is on the back of the micro:bit v2, and I can tell you from experience it is as loud and annoying as the external speakers that we include in our kits. Now your students can make a noise machine, set up a burglar alarm or build a musical instrument using just the micro:bit itself. Oh, joy!

The powered up micro:bit v2

Along the lines of sound, the micro:bit v2 also has a microphone. This was a wonderful addition to the on-board sensor suite of the board. At first I was skeptical about the quality of the microphone and how clean its inputs would be - would it be too sensitive, or not sensitive enough? However, I was wonderfully surprised by how responsive the microphone was and, at least when combined with the bar graph functionality on the LED array as a graphical output, how consistent and clean the signal was. Between the microphone and the speaker this opens up a whole possibility of new projects with just the micro:bit alone!

Touch Sensor

The micro:bit Foundation added one more sensor to the board: a capacitive touch sensor. If you have used the micro:bit before, you may have used the touch functionality on the pins of its edge connector. This was great, but at times was a little tough to use with the pins being jammed together. The micro:bit v2 has moved the touch functionality and connected it to the micro:bit logo at the top of the board.

Metal micro:bit v2 Logo

Comparing it to a previous version, you can see that the logo is no longer part of the silk screen, but actually metal. Another wonderfully simple input for this little board.

Bluetooth

While not the most flashy collection of updates to the board for most people, for those looking to push the limits of the micro:bit, v2 features BLE 5.0. This change opens up a number of potential avenues in terms of communication with other devices such as phones, laptops, etc.

At SparkFun, we also like the change to a dedicated I2C port, as many of our accessories such as the moto:bit and weather:bit communicate with the micro:bit via I2C. This means a more stable and consistent user experience.

Improved Connections

Another update to the micro:bit v2 that you may have noticed are the small “bites” taken out of the edge connector.

The newest micro:bit

These are there to make it easier to connect external components to the micro:bit with alligator clips without them sliding around, falling off or shorting on other pins. I can tell you from personal experience, this small and seemingly simple modification is a big deal and improves prototyping greatly.

Power

Last but not least, the additions of a few updates around powering the micro:bit and its output. The micro:bit v2 includes a way to turn it on/off from the board. Those of you that have burned through batteries when students leave the battery packs plugged in will understand the value of this!

Another great update for those who do a lot of tinkering with external components and the micro:bit is that the total output current through the micro:bit v2 has been bumped from 90mA to 200mA. This is great for driving more than one or two LEDs before things start to go dim. There are also a few improvements for the power inputs as well, but I will wait to test those in more depth until I have more than one on my desk.

Looking Forward

After reviewing the board and being hands on with it, I can tell you that the Foundation put a lot of thought into the updates. They listened to feedback - both from teachers and students, but also from partners.

micro:bit v2 Board

micro:bit v2 Board

DEV-17287
$16.50
7
micro:bit v2 Go Bundle

micro:bit v2 Go Bundle

DEV-17288
$19.95
2
micro:bit v2 Club Kit - Go Bundle 10-Pack

micro:bit v2 Club Kit - Go Bundle 10-Pack

KIT-17290
$175.00
6

The micro:bit v2 will start shipping sometime around mid to late November, with limited availability. Until then, we are offering the micro:bit v2 Board, the micro:bit v2 Go Bundle, and the micro:bit v2 Club Kit for pre-order today. Placing your order will reserve stock in the order that it is received, so the sooner you place your order, the sooner you'll get your micro:bit v2 product!

SparkFun Inventor's Kit for micro:bit v2

SparkFun Inventor's Kit for micro:bit v2

KIT-17362
$53.50
SparkFun Inventor's Kit for micro:bit v2 Lab Pack

SparkFun Inventor's Kit for micro:bit v2 Lab Pack

LAB-17363
$460.00
SparkFun Educator Lab Pack for micro:bit v2

SparkFun Educator Lab Pack for micro:bit v2

LAB-17361
$320.95

Between now and when we expect micro:bit v2 to start shipping, we are updating our current ecosystem to support the v2 release with the SIK for micro:bit v2, SIK Labpack for micro:bit v2, and the micro:bit v2 Educator Lab Pack. All three of these kits are available for pre-order and the photos may not be final and are subject to change. Don't worry, all of our previous micro:bit Kits will remain available until the beginning of next year.

We will be testing out our existing micro:bit ecosystem of carrier boards to make sure that everything works and is as compatible as we can make it. We may even sneak some new content in there for those of you that are early adopters of the v2. Keep an eye out for updates from us on our social media channels, newsletter and video releases.


Comments 4 comments

  • ppelleti / about 4 years ago / 3

    Could you add the comparison chart at a legible size? Thanks!

  • MikeJones / about 4 years ago * / 1

    I own one of these micro:bit's and I love them.

  • Member #332207 / about 4 years ago / 1

    You'll be happy to hear that AI/ML is already possible using Espruino on the micro:bit V2. It uses a very similar MCU to the Bangle.js and we (NearForm) worked with Gordon in Espruino last November to get TensorFlow Lite Micro running on the Bangle along with a sample gesture recognition model.

    Latest Espruino release announcement with micro:bit V2 support is here

    More on TF and Bangle.js is here

    HTH

Related Posts

Recent Posts

Tags


All Tags