×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

A Kit of Alphanumeric Proportions

Our new Qwiic Alphanumeric Displays get their own kit, a new robotics development board from Holybro, and a different version of the OpenMV Cam!

Favorited Favorite 0

This is the last week before Black Friday and Cyber Monday, so all the new products this week are expected to be a great hit for the holidays! We start the week off with a new and simple kit for our Qwiic Alphanumeric Displays. Following that, we have FOC ESC robotics driver and a new OpenMV H7 camera. Let's jump in and take a closer look at all of our new products!

14-segments in a single kit!

SparkFun Qwiic Alphanumeric Starter Kit - Red and White

SparkFun Qwiic Alphanumeric Starter Kit - Red and White

KIT-18624
$22.95

The SparkFun Qwiic Alphanumeric Kit comes with two displays, one red and one white. Also included in this kit are 10 standoffs and screws for mounting as well as two Qwiic cables to get up and running as fast as possible. These fourteen-segment digits allow you to display all sorts of numbers, characters, and symbols. With Qwiic, simply plug it in and go. No soldering, no figuring out which is SDA or SCL and no voltage regulation or translation required!


SparkFun IOTA - Satellite Communication Module (ARTIC R2)

SPX-17984
Retired

Is your project linked to environmental protection, awareness or study, or to protecting human life? Perhaps you are developing a wildlife tracker, ocean buoy, environmental monitoring system or need to transfer emergency medical information? Do you need to be able to transmit and receive data anywhere? If so, this is the product for you! IOTA (Integrated Open-Source Transceiver for ARGOS) allows you to send and receive short bursts of data via the ARGOS satellite network, anywhere on Earth including the Polar regions.


Mini FOC ESC Based on VESC®6

ROB-18715
Retired

The Mini FOC ESC Based on VESC®6 is a field-oriented control (FOC), electronic speed controller (ESC) board developed by Holybro using the Variable Electronic Speed Controller (VESC) format. No matter what your project is or what scale it has - as long as it incorporates electric motors or actuators, you can use this board to control and regulate the power. You will be able to set parameters that ensure that the motor operates safely.


OpenMV Cam H7 R2

SEN-18982
Retired

The OpenMV H7 R2 Camera is a small, low power, microcontroller board which allows you to easily implement applications using machine vision in the real-world. The Plus variation adds 32 MB of external 32-bit SDRAM and 32 MB of external quad SPI flash. You program the OpenMV Cam in high level Python scripts (courtesy of the MicroPython Operating System) instead of C/C++. This makes it easier to deal with the complex outputs of machine vision algorithms and working with high level data structures.


JST Right-Angle Connector - SMD 2-Pin (Black)

JST Right-Angle Connector - SMD 2-Pin (Black)

PRT-11641
$0.95

This is a two pin, compact surface mount JST connector. We really like the solid locking feeling and high current rating on these small connectors.


That's it for this week. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. We won't be have any new products to showcase next Friday in observance of the Thanksgiving holiday here in the United States, but be sure to check in to find out more about the exciting sales we have planned. Please be safe out there and be kind to one another!

Never miss a new product!


Comments 0 comments

Related Posts

Super LoRaSerial

Recent Posts

Tags


All Tags