×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

Precision Meets Customization Meets...You! Meet the MicroMod GNSS Carrier Board!

A look into the MicroMod GNSS Carrier Board and how to utilize it with u-center.

Favorited Favorite 0

As you can probably tell with the last few product releases, we're really excited about all things geospatial. One of our larger recent product releases, the new SparkFun MicroMod GNSS Carrier Board, exemplifies everything that is so revolutionary in that space right now. This board, equipped with the ZED-F9P chip from u-blox, sits at the convergence of highly-precise and highly-configurable. Plus, being a MicroMod board, it is part of a highly-customizable ecosystem that makes it easy to utilize different processors depending on your specific project needs.

SparkFun MicroMod GNSS Carrier Board (ZED-F9P)

SparkFun MicroMod GNSS Carrier Board (ZED-F9P)

GPS-17722
$269.95

Overview of the board

The ZED-F9P chip on the SparkFun MicroMod GNSS Carrier Board is a top-of-the-line module for high accuracy GNSS and GPS location solutions, including RTK, capable of 10mm, three-dimensional accuracy. With this board you will be able to know where your (or any object's) X, Y, and Z location is, roughly within the width of your fingernail! The ZED-F9P is unique in that it is capable of both rover and base station operations. Utilizing the M.2 and Qwiic connectors, no soldering is required to connect it to the rest of your system. However, we still broke out 0.1"-spaced pins in case you prefer to use a breadboard to attach additional peripherals.

To properly utilize this kind of module, you'll want to use an antenna that can get a clear view of the sky. It will need to be one that is robust enough to be outside, has long cable, and has an SMA connector.

The Taoglas AA.200 MagmaX2 Multiband GNSS Magnetic Mount Antenna is a good choice for the job. It can access most major constellations including GPS (L1/L2/L5), GLONASS (G1/G2/G5), Galileo(E1/E5a/E5b) and BeiDou(B1/B2). The AA.200 antenna is an active multiband GNSS magnetic mount antenna that exhibits excellent gain and good radiation pattern stability. The combination of these elements help ensure the best possible positional accuracy for systems where RTK is enabled and disabled.

MagmaX2 Active Multiband GNSS Magnetic Mount Antenna - AA.200

MagmaX2 Active Multiband GNSS Magnetic Mount Antenna - AA.200

GPS-17108
$83.50

Lastly, you'll need to pick up a processor board of your choosing; you can use our comparison chart to decide, or try a few out!

SparkFun MicroMod Teensy Processor

SparkFun MicroMod Teensy Processor

DEV-16402
$21.50
8
SparkFun MicroMod ESP32 Processor

SparkFun MicroMod ESP32 Processor

WRL-16781
$16.95
1
SparkFun MicroMod RP2040 Processor

SparkFun MicroMod RP2040 Processor

DEV-17720
$12.95
1
SparkFun MicroMod nRF52840 Processor

SparkFun MicroMod nRF52840 Processor

WRL-16984
$21.50
SparkFun MicroMod Artemis Processor

SparkFun MicroMod Artemis Processor

DEV-16401
$14.95
1

SparkFun MicroMod STM32 Processor

DEV-17713
SparkFun MicroMod SAMD51 Processor

SparkFun MicroMod SAMD51 Processor

DEV-16791
$18.95
1

As usual, we produced a product showcase that goes through the board specs and capabilities in depth. We also included a more complete understanding of the many different GNSS technologies that the ZED-F9P chip utilizes, as well as different software platforms to make full use of the module.

The showcase highlights all the satellite constellations the ZED-F9P can communicate with!

How to configure using u-center

For any board based on u-blox chip, using u-center, a Windows free software tool, is an easy way to configure your receiver. We have a robust beginner tutorial on connecting your receiver with u-center through configuring your COM port and baudrates. Make sure that your antenna has a clear view of the sky, and once you're connected you'll see a breadth of data appear.

Start by configuring your hardware:

u-center dashboard
The u-center main dashboard

Seeing your satellite connections

There are two things to note in the next screenshot - firstly, that the receiver is acquiring data from multinational satellite constellations, meaning it is a proper GNSS tool. You can see on the right hand side that is communicating with GPS, GLONASS, Galileo, and BeiDou satellites. You can also see, in the second screenshot, that the module sis communicating with 25 satellite units at the moment, so it is gathering a lot of information. The other thing to note, is that without any correction data, the module is within 2 meters of accuracy. We have a tutorial on using NTRIP to stream correction data to your device using both u-center and other platforms.

accuracy without NTRIP
Without any correction data, the ZED-F9P module is still within 2 meters of accuracy!

SVs
Not only is the module receiving data from 25 SVs, but they are from each of the international satellite constellations.


Google Maps Static API

There are multiple menus to utilize within u-center, one of which is the maps menu. By using Google Maps Static API, you can visualize the module spatially, as well as add speed vectors and scales. You'll need to add billing information to your Google Developer profile for the API to work properly.

google map
Go to Tools -> Preferences -> Access Tokens to add your Static Google API key.

There's also preferences for creating a Google Earth Server that will track in real time where your module is.


Setting up a Geofence

A key use case for a receiver as precise as this one is the ability to geofence, or create a boundary for the module's location. If the module leaves that boundary, then the user is notified that it has left that radius. U-center makes it easy to set this tool up. Within the configuration menu, you can set the latitude and longitude of the location, as well as radius that will serve as the boundary. Then, in the messages menu, under NAV, you'll be able to track whether the module is inside or outside of that radius you set up.

setup geofence
Within u-center, it's easy to set a boundary for geofencing.

test geofence
You can watch if your module is inside or outside of your designated geofence!


Learn more about u-center

U-center is a dense but extremely useful program for utilizing your GNSS receiver to it's full potential. There's tons more information not included in this blog, like logging data into a database, utilizing camera view, and so much more. If you're interested in these features, check out the in-depth user guide, or comment below on what parts of the software you'd like us to dig into to help you with your projects. In the meantime, put that brand new MicroMod GNSS Carrier Board to good use, and track where it is (and isn't) at all times. Happy Hacking!

 



Comments 0 comments

Related Posts

Recent Posts

Tags


All Tags