SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!
Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.
Hello and welcome, everyone! We are back again with more new products for this week's Friday Product Post. We are taking another look at the new MyoWare® 2.0 products that were released a few weeks ago, but this time, we've made two new kits that take advantage of the first two examples in the MyoWare 2.0 Guide. Following that, and based on your feedback, we assembled 10 MyoWare 2.0 Reference Cable in a single kit in order for you to easily hook these EMG sensors to your body. SparkX released a new Qwiic triple axis magnetometer utilizing the MMC5983MA from Memsic, as well! We are going to wrap up the week taking a look at new Carbide 3D CNC products and for extra cables. Enough of the intro, let's jump in and take a closer look at this week's new products!
The MyoWare® 2.0 Muscle Sensor Development Kit is an Arduino-compatible, all-in-one electromyography (EMG) sensor kit that provides you with all the boards from the MyoWare 2.0 ecosystem to test out different configurations for your application. Depending on your configuration, you can visualize the muscles in action with the MyoWare 2.0 LED Shield or read the analog output using an Arduino-compatible microcontroller! Simply snap on a MyoWare 2.0 Shield, add some EMG sensor pads, attach the sensor to a muscle group, and flex!
The MyoWare 2.0 Muscle Sensor Basic Kit, is another Arduino-compatible, all-in-one electromyography (EMG) sensor kit that provides you with the bare minimum from the MyoWare 2.0 ecosystem to get started measuring and visualizing muscle activity. Simply snap on the MyoWare 2.0 LED Shield, add some EMG sensor pads, attach the sensor to a muscle group, and flex! The kit also includes a mini screwdriver to easily remove shields, USB A to C cable to recharge the 40mAh LiPo battery, and MyoWare 2.0 Reference Cable to connect to large muscle groups.
This is a 10 pack of the MyoWare Reference 2.0 Cables. The MyoWare 2.0 Reference Cable is meant as an extension for the MyoWare 2.0 Muscle Sensor's reference pin. You will just need to insert the pin into its housing and place a biomedical sensor pad into the electrode snap. When ready, stick the reference cable's snap pin to a separate section of the body such as a bony portion of the elbow or a nonadjacent muscle near a targeted muscle where the MyoWare 2.0 Muscle Sensor's built-in reference pin is unable to reach.
The Qwiic MMC5983MA Board from SparkX is a highly sensitive triple axis magnetometer by MEMSIC. It is capable of sensing down to 0.4mG enabling a heading accuracy of ±0.5°. Output rates of 1000Hz, ±8G FSR, and 18-bit resolution make the MMC5983MA a phenomenal magnetic sensor for electronic compass applications.
Carbide 3D is available at SparkFun Electronics again and you can light up your (or someone else's) life with this amazing project kit! You'll be glowing with joy from all the things you can make. Illuminate your home, office, nursery, even living room with your new Edge Light Kit.
The Carbide Compact Router is a trim router packaged for use with CNC machines. The Compact Router includes a 12 foot power cord to make wiring easier for everything from our Shapeoko 3 to the larger Shapeoko XXL.
We have even more new Carbide 3D products available starting today, so make sure to check out our complete offering.
This is a servo adapter cable that allows you to hookup your servo directly to alligator clip connections. On one end you have a shrouded male servo connector, and on the other end three 30mm shrouded alligator clips.
This servo cable has a shrouded male servo connector on one end, and three breadboard hookup pigtails at the other end.
That's it for this week. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another, and we'll see you next week with even more new products!