×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

Your Friday New Product Wrap-Up

This Friday, we're coming to your aid with more new products!

Favorited Favorite 0

We have a pretty good assortment of products this week. We're getting more retail products to our retailers, some new shields, LEDs (of course!), and well... I won't spoil the fun.

Yes, I really do have ESP, but only for when Dave gets hurt. I don't consider it a gift. Let's look at the products for this week.

Remember those old crystal radio kits when you were a kid (or from links on the internet)? Well, our new AM/FM receiver shield uses the Si4735 IC to turn your Arduino into a fully functional modern radio. You can receive AM and FM, as well as RDS and RBDS information. Using simple serial commands you can change volume, mute, scan radio stations, and much more! The reception is pretty impressive and if you need an extra boost, you can simply add a length of wire.

Our next product started out as a successful Kicksarter project. The Gameduino is an Arduino shield that turns your Arduino into a game console. The Gameduino features VGA output, 12-bit audio (through a 3.5mm audio jack) and enough example code to get you up and running quickly. Check out this video to see more of what it can do.

You may be asking yourself 'self, are those really RTFM bandages?'. Yes, yes they are. You see, we teach a lot of workshops and do a lot of our own projects. It doesn't always go perfectly smooth and sometimes there are some minor cuts and severed limbs. Nothing serves as a better reminder to take a little extra precaution than wrapping your wound in a SparkFun RTFM adhesive bandage. Yes, these are sterile bandages. Yes, they are real. And yes, they're awesome.

We have several products aimed at making LiPo batteries easier to use in projects. We've got the Power Cell, LiPower, and our basic chargers. But what if you just want to check how much power is left in your battery? Now we have the LiPo Fuel Gauge which can tell you how much power you have with the help of I2C. If you plan on using batteries in your next project and battery level is critical, you might want to check out the LiPo Fuel Gauge.

It seems that almost every week we have some new product relating to LEDs. This week is no exception. People seem to really like our super bright 10mm LEDs, but sometimes you don't need all that brightness, but still want a larger LED. These new diffuse 10mm LEDs aren't nearly as blindingly bright and have a softer diffuse glow to them. In addition to the red and blue seen above, we also have them in green and yellow.

We have a lot of varieties of DC barrel jacks, but didn't carry a good panel mount jack. This 2.1mm center-positive DC barrel jack has a nut and washer so you can easily mount it to a flat surface (with the aid of an 8mm hole). Use one of these to give your next project a finished look. I used one of these on the NCWP that I built for my wife.

Here at SparkFun, we never make mistakes. Oh, I kid... We make mistakes all the time just like anyone else. This time we assembled our XMega100 Breakout Boards with a bad PCB. We didn't notice it until after they were built. Personally, I think they look kinda neat. The silkscreen is mirrored on the underneath side. It looks like you're looking through the board. The board tests fine and the labels are still correct, they are just mirrored and on the wrong side. If you know what you're doing and want to save a couple of bucks, check out the XMega100 Breakout - Kriss Kross edition.

In addition to all the fine products above, we also released a few new retail products this week. That means that your local retailers might soon have new stock of some of these products. But don't worry, you can get them all here online and most of them are products we've already been carrying. This week we added the Arduino Header Kit, Clear Breadboard, TTL Laser, ITG-3200 Breakout, USB Mini Cable, USB A-B Cable, Breadboard Arduino Kit, and the Thumb Joystick Kit.

That's all I have to talk about this week. We have quite a wide range of products this week. Of course, I'll be back next week with even more new products to talk about. Thanks for reading.


Comments 33 comments

  • MikeGrusin / about 14 years ago / 4

    First aid box contents FTW!

  • jakkjakk / about 14 years ago / 4

    Thanks for showing us your screw ups because now when I screw up I don't feel so bad.

  • htimmis / about 14 years ago / 2

    thanks for another great product post

  • NetMeyer / about 13 years ago / 1

    -moved to 08.12.11

  • NetMeyer / about 13 years ago * / 1

  • SomeGuy123 / about 14 years ago / 1

    Did anyone notice that everything on his desk shifted at 2:56?

  • pchalla90 / about 14 years ago / 1

    Sorry to be "that guy", but you misspelled Kickstarter in the section regarding the Arduino video game shield.

  • Member #219969 / about 14 years ago / 1

    Am I the only one who wanted him to pull a Koolaid Man and bust through the boxes on his way to rescue Dave?

  • HP / about 14 years ago / 1

    Uhm, I think that it is up to the user (and the power supply) to decide which terminal is positive on that barrel jack connector..
    the FM radio is awesome! oh, and the bandages too!

  • J.Sweet / about 14 years ago / 1

    I can't make out what Rob says as he's running down the hall and knocks the stuff out of his hands, can anyone else?

  • Love the "Boxwall" effect and I hope it stays. It feels like something you'd see in a kid's show. "Alright, boys and girls, let's see what in today's box!"
    Seriously, I think you should pull the products from a different wallbox each time.
    Lastly, how long until you start carrying the "SFE hacker first aid kit"? 'Cause I want one. :)
    Additional: I would have thought that Dave-pain ESP would be very helpful. That way, you'd know if your prank worked without having to be there: See "The Dreadmill"!

  • Plaid / about 14 years ago / 1

    You know what I want to see? Kapton tape bandages. That way after I apply a bandage to my soldering-iron-burned fingers, they won't get burned so easily again!

  • Tenyu / about 14 years ago * / 1

    I noticed you were running around barefoot in that video, Rob. That pretty common for you guys there? Talk about relaxing work dress code :)

  • I love radios:D

  • scharkalvin / about 14 years ago / 1

    Your new "studio" for "filming" (is videoing a word?) the Friday updates seems to be lined with sparkfun boxes. Reminds me of KORN from Hee-Haw with all the egg crates glued to the walls. Or is what you have just "wall paper" and not actual boxes (though the boxes would be real cool).

    • The boxes were there last week, too. I just lost an electron that they're real boxes (I'm "positive". Hahaha!).
      BTW, think they'll ever carry something like this?

    • TeslaFan / about 14 years ago / 1

      I've taken to calling all capturing of real world events to a recording device "recording".
      Those are real boxes. He removes one from the wall! And the room is clearly smaller. I have 100 Quatloos that says they didn't even remove the normal wall decorations... just entombed them behind the wall of red.

    • they are real boxes. see how I remove one from the wall?

  • Great post! How do I email videographer Greg a question?

  • Member #218679 / about 14 years ago / 1

    It ain't all epic win, man.

Related Posts

Recent Posts

Tags


All Tags