Plasma Speaker

Check out this awesome project from a couple of Eastern Washington students.

Favorited Favorite 1

If you have ever been within earshot of SparkFun's shipping department during the workday, you have probably heard some pretty decent beats (or beatz?) coming from the area. It is a not-so-well-kept secret that SparkFun employees like to blast tunes during work hours. In fact, it has been shown to increase workplace productivity by 89%* (*in a non-scientific poll conducted by me just seconds ago).

Which brings us the project you see above - this is a plasma speaker created by Brian Hainey and Chris Lewis, engineering students at Eastern Washington University. The speaker above is not your typical sound output device, but rather features a TL494 PWM chip which provides a 45 kHz "carrier" signal onto which audio can be modulated. This transmits audio data that is detected by a microphone in Matlab (you remember Matlab right? Of course you do...), and then processed with Simulink to generate text data.

This is a very cool project that is sure to impress your friends at your next party. Check out Brian's webpage - MuskratMicros - to see more about the plasma speaker, learn about some other awesome projects, or just see a picture of Brian heaterizing a peep (hopefully he read the instructions). Great work Brian and Chris!


Comments 31 comments

  • TECH GEEK / about 14 years ago / 3

    Ha Ha "FunSparks at SparkFun" Lol :D

  • tsimop / about 14 years ago / 2

    I built this a few months ago: Instructable - Plasma Speaker - the circuit looks quite similar to the video posted here.
    See my video at the bottom of the page here
    I have since improved the circuit to use a properly driven H-bridge and a resistor in line with the transformer - now the FETs don't even warm up without a heatsink.
    Now we're working on using plasma ailerons for roll control on a UAV.

  • SomeGuy123 / about 14 years ago / 2

    Sparkfun should consider carrying the panavise shown in the beginning of the video.
    I bought on due to the interchangeable heads you can purchase for it.

  • Itai N / about 14 years ago / 2

    Please correct to title (Plama -> Plasma).

  • Vihtori / about 14 years ago / 1

    Interesting to see the plasma speaker is coming around again. I read an article in Poplular Electronics magazine back in the '70s on putting together such a play thing. Required a flame, high voltage, some salt, and other items.

  • Nicholas.Searcy / about 14 years ago / 1

    Check this out, designed at University of Louisville by Paul Faget and Seth Tucker a few months ago.
    http://www.youtube.com/watch?v=GetuOyujKvg&feature=player_embedded

    • Nicholas.Searcy / about 14 years ago / 1

      Also plasma arc speaker (tweeter) with a little different design and an adjustable arc length.

  • Dave Sears / about 14 years ago / 1

    10/10 for effort, tho if you want to see some real plasma speakers see timetec's channel on utube :

  • Ekisu / about 14 years ago / 1

    Ah, plasma speakers. Very cool stuff. I built one of these when i was in high school. They're not as complicated on the inside as they look like they would be.

  • Member #120616 / about 14 years ago / 1

    I do not know how to order a Pico Board from you

  • sephers / about 14 years ago / 1

    wait a sec, so that blue beam is creating the sound??

    • SomeGuy123 / about 14 years ago * / 1

      Correct. The speaker uses changes in the density of the plasma to create vibrations in the medium surrounding the plasma.

      • sephers / about 14 years ago / 1

        that's awesome :D what kinda voltage would be used for that

  • RoBo101 / about 14 years ago * / 1

    So how big is the leap form this to making a plasma cutter?..
    - Blasting air with an air compressor past one of the tips and connecting the other tip's lead to a sheet of mettle?

  • I was just talking about plasma sound yesterday. Any details/schematics out there?

    • I've looked into it awhile back. There's quite a bit on google if you just search around. I never got around to making one though.

      • TheBestJohn / about 13 years ago / 1

        Take a Look at My blog... I built one of these 2 or 3 years ago and have some good links. blog.thebestjohn.com

  • sultanblender / about 14 years ago / 1

    That is really cool, but is it... Dangerous?

    • SomeGuy123 / about 14 years ago / 3

      It's only dangerous if you don't handle it correctly.

    • rwizard / about 14 years ago / 1

      The most common final words uttered by Sparkfun customers: "Hey everybody, watch this!". (If it isn't dangerous, why bother?)

  • Member #150164 / about 14 years ago / 1

    For anyone who cannot afford to buy a copy of Matlab, Scilab from scilab.org is a good, free alternative. Scilab is a powerful Numerical Computation program and much of the syntax is even compatible with and can import Matlab files.

  • SlyVixsky / about 14 years ago / 1

    Plasma speaker made by a university? I've seen hobbiest plasma speakers from tv and pc/crt fly-backs since around 2005 :D awesome project in any case :D

    • rwizard / about 14 years ago / 1

      As a child I read an article on building a "flame speaker" in Popular Electronics - this would have been in the mid 1960's best I remember. As I recall it involved a gas flame and used a high voltage power supply to ionize the stream. My memory of the details are a little fuzzy after 40 to 50 years, but I sure wanted to build one back in the day - read the ink off of the pages. Anyway, it is far from a new idea, and goes much further back than 2005. I believe someone was even selling a commercial plasma speaker at one time.

    • Not really 'by a university,' but by a couple of students at a university.

Related Posts

Recent Posts

What is Quadband?

Tags


All Tags