Photoacoustic Revolution with SCD4x

We have two new environmental sensors that feature the SCD4x line from Sensirion as well as a wide-angle lens version of the RPi Camera Module 3 NoIR!

Favorited Favorite 0

Hello everyone and welcome back to another Friday Product Post here at SparkFun Electronics! We have three exciting new products to show off this week and we are going to start with the new SCD40 and SCD41 CO₂ Humidity and Temperature Qwiic Sensors. These two boards have some slight difference, so make sure you read on to learn more! Following that, we have a wide-angle version of the Raspberry Pi Camera Module 3 NoIR (in case you missed it, we released the standard lens version last week). Alright, let's jump in and take a closer look at this week's new products!

SCD40 or SCD41... Choices, choices!

SparkFun CO₂ Humidity and Temperature Sensor - SCD40 (Qwiic)

SparkFun CO₂ Humidity and Temperature Sensor - SCD40 (Qwiic)

SEN-22395
$54.95

This SparkFun CO2 Humidity and Temperature Sensor features the next-generation SCD40 photoacoustic CO2 sensor for high-accuracy environmental readings. The SCD40 uses Sensirion's PASens® photoacoustic measurement system that combines narrow-band IR light and a microphone inside the sensing package capable of detecting concentrations from 0 to 40000 ppm with high accuracy over 400-2000 ppm ±(50 ppm+5%). The SCD41 has an integrated temperature and humidity CMos® sensor to improve accuracy. For additional accuracy, the SCD40 also accepts ambient pressure readings!


SparkFun CO₂ Humidity and Temperature Sensor - SCD41 (Qwiic)

SparkFun CO₂ Humidity and Temperature Sensor - SCD41 (Qwiic)

SEN-22396
$64.95

Meanwhile, this SparkFun CO2 Humidity and Temperature Sensor features the next-generation SCD41 photoacoustic CO2 sensor for high-accuracy environmental readings. The SCD41 uses Sensirion's PASens® photoacoustic measurement system that combines narrow-band IR light and a microphone inside the sensing package capable of detecting concentrations from 0 to 40000 ppm with high accuracy over 400-5000 ppm ±(40 ppm+5%). The SCD41 has an integrated temperature and humidity CMos® sensor to improve accuracy. For additional accuracy, the SCD41 also accepts ambient pressure readings!


Raspberry Pi Camera Module 3 NoIR - Wide Angle

Raspberry Pi Camera Module 3 NoIR - Wide Angle

SEN-21735
$35.00

The Raspberry Pi Camera Module 3 NoIR (Wide Angle) features a wide-angle lens (120° field of view) and does not employ an infrared filter (thus the NoIR). Built around a 12-megapixel Sony IMX708 image sensor module, Camera Module 3 offers a few key enhancements over its predecessor. Improved low-light sensitivity makes for better photos and output in situations where there's not a lot of light. The module also features powered autofocus, making getting a sharp picture output easier.


That's it for this week. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another! We'll be back with more new products next week so make sure to check back then. Happy hacking!

Never miss a new product!


Comments 4 comments

  • Member #134773 / about 2 years ago / 1

    OFF TOPIC: I was in a JoAnn Cloth and Craft store yesterday, and they're having a sale on "Super Stackable" storage boxes through June 14. Since I've used such boxes to house small projects, I "stocked up" on them. They're clear, have latches to hold the lids on them, and are of a soft plastic that's easy to make holes for mounting things inside with something like a "hobby knife" (for example, an X-acto knife). They come in several different sizes, the smallest being designed to hold a box of crayons.

    I'm not sure how wide-spread JoAnn stores are. There are several here in the Phoenix area.

  • Member #134773 / about 2 years ago / 1

    Looks like the timing on releasing the CO2 sensors is a great coincidence what with the smoke from the Canadian wildfires coming into the north eastern part of the U.S.! I've been joking that I'm glad that I don't happen to need to order anything from Adafruit at the moment, because I wouldn't want a box full of that polluted air in my house! ;-) :-) ;-)

  • electric_insect / about 2 years ago / 1

    This is the 2nd time you posted the NoIR cameras have an IR filter. You might want to check your datasheets and update that description. From raspberrypi.com

    The Camera Module 2 NoIR gives you everything the standard Camera Module offers, with one difference: it does not employ an infrared filter. (NoIR = No Infrared filter.)

Related Posts

Recent Posts

Tags


All Tags