Our Qwiic connect system has not only taken our products by storm after being introduced by SparkX in 2017, but it's also being used across the industry as to simplify I2C for all types of applications!
by
Chowdah
October 3, 2023 12:00 pm UTC
2
Favorited
Favorite
0
It's interesting to think that there was a time, not too long ago, when Qwiic didn't exist at all at SparkFun. That 4-pin JST connector is so ubiquitous on SparkFun's boards that there's hardy a new board from us that goes to market without it. That is to say that since it's release from
SparkX in 2017, our Qwiic line of products has grown to include a popular spread of development boards, helpful shields, a vast array of sensors and much more. And it's easy to see why; the solderless, daisy chain-able, polarized connector has wide appeal ranging from electronics beginners who don't like playing with hot irons to seasoned experts who are prototyping and want to quickly try out a bunch of different configurations. It makes sense.
In stock
DEV-16400
The MicroMod Machine Learning Carrier combines the freedom to explore any processor in the MicroMod lineup without the need f…
Out of stock
DEV-18710
The MicroMod mikroBUS Carrier Board takes advantage of the MicroMod, Qwiic, and mikroBUS ecosystems making it easy to rapidly…
Out of stock
WRL-20168
The USB-C variant of ESP32 Thing Plus is a development board with WiFi, SPP, BLE, Qwiic connector, 21 I/O pins, RGB status LE…
3
In stock
SEN-22396
The SparkFun CO2 Humidity and Temperature Sensor - SCD41 (Qwiic) features the SCD40 CO2 from Sensirion©.
Side Note: One time we tried to figure out how many variations of Qwiic boards you could connect. Answer: it's a lot - like such a large number I don't even have a concept for how big the number is...
Pronounced "Quick," but with 2 "i's" and a "c," like I^2C, get it?
These are littered everywhere around HQ
As popular as this tech is internally, in true SparkFun fashion we have released the technology and use of logo open source for the public to use. We love to see other companies adoption the Qwiic-Connect standard into their products.
Did You Know: Qwiic connectors use a standardized I2C interface. This means that devices from different manufacturers that support the Qwiic system can be easily connected and used together. It promotes interoperability and allows users to mix and match components from various sources. Sweet!
Other reasons for companies to add Qwiic connectors on their boards: plug-and-play functionality, modularity, time-saving, reduced potential for wiring errors.
In stock
DEV-22632
Arduino UNO R4 is a 32-bit microprocessor offering more speed, memory, connectors and connectivity options than any version o…
9
So, in the spirit of uncountable possibilities for your infinite inspiration: here's a not-comprehensive list of some products from companies that are implementing Qwiic Connectors!
There are some scenarios where maybe you wish a board had a Qwiic Connector but it doesn't. We have a growing line of "hats" that can offer cross-brand compatibility. Check them out, or alternatively, use something simple like this.
Only 1 left!
DEV-17512
The Qwiic pHAT Extension for the RPi400 provides you with an easy way to access all GPIO, stack your favorite HAT upright or …
In stock
DEV-18346
The PoE+ HAT allows you to power your Raspberry Pi using Power over Ethernet networks with up to 25.5 Watts (PoE+) over CAT5 …
4
19 available
WRL-19956
The AHPI7292S is the world's first WiFi HaLow™ Raspberry Pi™ HAT module from ALFA Network.
2
In stock
DEV-25268
An M.2 HAT+ for the Raspberry Pi 5. Allows you to interface with devices such as M.2 SSDs.
As always, share your projects and let us know which other companies have Qwiic connectors on their boards! Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn, or check us out on Hackster. Thanks for reading y'all!
A couple of "conspicuous by their absence": First, our friends over at Adafruit have a LOT of items that have QWIIC compatible connectors, though they call it "STEMMA QT".
The other is that I had hoped that the Raspberry Pi 5 announced last week would include an on-board QWIIC connector. (Yes, I'm aware of the SparkFun Qwiic SHIM for Raspberry Pi, as well as several "hats" that have QWIIC connectors.). I'm hoping the next version of RPi will include an on-board QWIIC connector!
Ah we also wish there was a Qwiic Connector on the new Pi 5! Hopefully we can make this happen in the future!