×

SparkFun will be closed on Tuesday, December 24th, and Wednesday, December 25th, in observance of the Christmas holiday. Any orders qualifying for same day shipping placed after 2:00 p.m. (MST) on Monday, December 23rd, will be processed on Thursday, December 26th, when we return to regular business hours. Wishing you a safe and happy holiday from all of us at SparkFun!

Please note - we will not be available for Local Pick up orders from December 24th-December 27th. If you place an order for Local Pick-Up we will have those ready on Monday, December 30th.

Engineering Roundtable - Cymatics with Joel

Check out today's Roundtable project with Joel, SparkFun Product Vetter.

Favorited Favorite 0

It's that time again - we have another episode of "Engineering Roundtable!" Today's host is Joel, SparkFun product vetter and hacker extraordinaire. Joel is going to guide you through his cymatics project - check it out:


Vimeo version found here.

Just a bit of warning - if you are going to try this out at home, you might want to use some hearing protection. It's very loud! As always., please leave any questions in the comments section below. We'll see you in two weeks with our next edition of "Engineering Roundtable." Enjoy!


Comments 16 comments

  • sgrace / about 12 years ago / 3

    I wanted to point something out to those who were wondering why he was just getting circles with the circular plate. The sinusoid and the circle are closely related to each other (by Pi), by having a circular plate, all you will see is the nodal points he described in circles. The place where the salt is forming these circles is the period length. Remember, the higher the frequency the shorter 1 period. With this said, if you get up into the MHz ranges, you are dealing with mere inches/centimeters.

    Now the difference between the circle and square. Sound is sent out in a circular pattern, and on a circular plate it will not reverb/reflect the sound back to the speaker (equal and opposite). However, with a square, you don't get this since the sound wave will reach an edge before it reaches a corner, and since the square does not fit within the ratio of Pi, there will be some reverb/reflection. This will cause waves to do partial cancellation and see the complex patterns.

    I welcome people to correct me on terminology, but I hope I gave everyone new to cymatics a gist of what you could see.

  • Jeremy Sag / about 12 years ago / 2

    Nice video, thanks for sharing. Oh, and don't attempt to listen with headphones. 0_0

    (it hertz)

  • Perhaps this would be a good application for a surface transducer?

  • super cool subject

    presentation style old brained people use (talk about what you are going to talk about>show it>talk about the cool stuff)

    presentation style young brained people use (I'm a 47 year old genius) (show the cool stuff>talk about it)

    the interwebs has reduced old brain stuff, but most people are still prisoners of the medieval school system.

    thank you for making this, it may provide a fundamental insight into the nature of the universe.

  • Carlos Fernandes / about 12 years ago / 1

    is it possible to do this without any sound? maybe modifying the speaker... using something else...

    I was thinking on using this to build something beautiful for my living room.

  • Dopey / about 12 years ago / 1

    Somewhat related, Non-Newtonian fluids on speakers. http://youtu.be/3zoTKXXNQIU

  • TheRegnirps / about 12 years ago / 1

    Very cool patterns. Try an old (really old) HP 202A/B generator to get continuous frequency sweep. I'll offer some hopefully useful critique. First, I think you are not sending sound through the plate, you are shaking it with the speaker coil and the force is applied where the glue is applied. It is like shaking a big piece of sheet metal and getting all those cool sounds. So, you need the theory of vibrations, not sound. Check on Bessel Functions and the modes of vibration of a drum head for a good example - you are into a special case of the hypergeometric equation here, so take a deep breath and a nicotine patch. On the square plate I could see the circular shape faintly at the higher frequencies like 340 Hz. Was it glued to the outer circle of the speaker cone/frame? If yes, the driving force is much different than on the round plate, with pressure applied over a large circular area. Second, modeling this mathematically is a nightmare without finite element techniques and numerical methods. Closed form solutions are impossible for things much more complicated than said drum head. So you can throw out all the talk of sin waves and such. Vibration nodes, yes. Sound? Not really. Sinusoidal motion? Maybe sort of near nodes. Try the salt on an out of balance washing machine. Never heard of cymatics. From the web, it looks like there is a mix of sound and vibration effects depending on the medium and mistakenly called wave phenomena in most cases. (If Sparkfun does not have an HP202, you really should keep your eyes out. They are phenomenal. The 202B is 0.008 Hz to 1200Hz continuous.)

    • John Price / about 12 years ago / 1

      so, putting some weights on the circle, perhaps paper clips, should allow you to get varying shapes...

      • TheRegnirps / about 12 years ago / 1

        I would think so, provided there is enough mass compared to the mass of the disk and the driving force and how rigid the disk - Young's and Bulk modulus of the material. More likely, if the masses are attached by being rigidly clipped on or glued, there will be big difference. From the looks of the mechanics, it would take something like 100 gram weights. But you would have to test. It might be very sensitive to adding mass in the right spots and you could develop a new kind of measuring instrument.

  • This brings a whole new meaning to engineering roundtable.

    And just cause I can't stop myself, circleception.

  • Far_Seeker / about 12 years ago / 1

    Something that I found interesting was most of the square plate patterns resembled popular ceramic or stone tilling patterns. Just a conincidence I'm sure, but IMHO a remarkable one.

  • philfromseattle / about 12 years ago / 1

    Aren't particle collection points where the wave reflections cancel? basically, standing wave patterns? That's why the circular plate had round nodal patterns. A multi driver configuration might be a great way to create more complex patterns

  • customer207 / about 12 years ago / 1

    That was excellent! Very cool demonstration, and a nice , calm , clear delivery.

  • LJ2 / about 12 years ago / 1

    could you add links for the parts used in the video?

Related Posts

Recent Posts

Tags


All Tags