Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
If you need more ways to hold material in your Nomad, this Threaded Table provides you with plenty of connection points.
The SparkFun Current Sensor Breakout is a high accuracy board that utilizes the ACS723 for moderate AC and DC current sensing…
The low current version of the SparkFun Current Sensor Breakout is a high accuracy board that utilizes the ACS723 for low to …
This SparkFun Distance Sensor Breakout utilizes the VL53L1X next generation ToF sensor module to give you the highly accurate…
The SparkFun Inventor's Kit Bridge Pack for micro:bit was designed to provide you with an easy way to transform your m:b into…
Here is a simple, low-cost, high quality servo for all your mechatronic needs. This servo is able to take in 6 volts and deli…
Does your robot crush objects with its hulkishly strong grip? Give your robotic hand or claw a better sense of touch with the…
The Pixy2 CMUcam5 is smaller, faster and more capable than the original Pixy. The Pixy2 can learn to detect objects that you …
The WE1010 from Weller is a powerful 70 watt soldering station that is perfect for passionate hobbyists, DIYers, and anyone w…
This is a replacement soldering tip for the Weller WE1010 soldering station. It is a "screwdriver" type of soldering tip, mea…
This is a replacement soldering tip for the Weller WE1010 soldering station. Each conical-type tip measures 0.02" (0.6mm) wid…
The LilyPad Light Sensor is a sewable breakout board with an ALS-PT19 light sensor built in and ready to use right away.
This SparkFun Real Time Clock (RTC) Module is a Qwiic-enabled breakout board for the RV-1805 chipset running at only about 22…
This is a time saving large kit of 700 jumper wires - cut, stripped, and pre-bent for your prototyping pleasure.
The SparkFun ProtoShield Kit lets you customize your own Arduino shield using whatever circuit you can come up with and then …
The SparkFun Arduino ProtoShield is a bare PCB with no attached or included parts that lets you customize your own shield usi…
This sleek, red 16GB thumb drive has been emblazoned with our SparkFun Electronics logo and our moniker to Start Something!
The AH1815 is an integrated Hall-Effect non-latched sensor.
LIDAR has never looked so good! The LIDAR-Lite v3HP is *the* ideal optical ranging solution for drone, robot, or unmanned veh…
USB C is fantastic. But until we have converted all our hubs, chargers, and ports over to USB C this is the cable you're goin…
The SparkFun Grid-EYE Infrared Array Breakout board is an 8x8 thermopile array, giving you a square of 64 pixels capable of i…
The SparkFun MLX90393 Magnetometer Breakout is a 3-axis magnetic sensor, capable of sensing very small fields even under satu…
The Noisy Cricket Stereo Amplifier, uses the LM4853 which can be configured to output up to 1.5W of power in mono operation o…
This is a basic 12 button keypad that has been designed for easy user input and functionality.
With this Insulated Silicone Soldering Mat you will be provided with the means to protect your desktop, soldering station, or…
An adjustable potentiometer can open up many interesting user interfaces. With this 100k Ohm linear pot just turn the dial an…
An adjustable potentiometer can open up many interesting user interfaces. With this 100k Ohm logarithmic pot just turn the di…
This black version of the Day of the Geek soldering kit you will be able to learn the basics of soldering by being able to as…
This white version of the Day of the Geek soldering kit you will be able to learn the basics of soldering by being able to as…
The Unigeek is a soldering kit that teaches you the basics of PTH and SMD soldering while assembling a light up unicorn badge…
With this Lighthouse kit you will be able to learn the basics and intermediate skills of soldering by being able to assemble …
With the heART Surface Mount Soldering Kit you will be able to learn the basics of SMD soldering by being able to assemble a …
The Raspberry Pi 3 B+ is here to provide you with the same Pi as before, but now with gigabit and PoE capable Ethernet!
The Magnetic Imaging Tile uses an array of 64 hall effect sensors to convert magnetic fields to the visual spectrum. That's r…
These 32x32 RGB LED panels are an awesome place to start to add color to a project! You can create animations, games, or usef…
The SparkFun AST-CAN485 Dev Board is a mini Arduino possessing on-board CAN (Control Area Network) and RS485 ports enabling q…
This great GT-521F52 fingerprint module from ADH-Tech communicates over TTL Serial so you can easily embed it into your next …
This 10mL no-clean flux pen from Chip Quik is great for all of your solder, de-solder, rework, and reflow purposes!
The SparkFun Variable Load is a quick to assemble kit that has been designed to allow users to draw a specific amount of curr…
These 2-pin JST-SM pigtail connectors mate perfectly with LED strips and other applications that require only two lines and a…
These 3-pin JST-SM pigtail connectors mate perfectly with LED strips and other applications that require only two lines and a…
These 4-pin JST-SM pigtail connectors mate perfectly with LED strips and other applications that require only two lines and a…
The Walabot Starter is a small, programmable sensor tool that looks into objects using radio frequency technology sense the e…
This version of the APA102 (or “DotStar”) is an astoundingly tiny, 8-pin, 2020-sized (2x2mm) SMD LED. With an integrated …
Ready to add some good vibes to your project? Look no further than the SparkFun Haptic Motor Driver. This board breaks out Te…
It's tiny, it's handy, and it can give your normal USB-equipped device a micro-B connector! With the USB to Micro-B Adapter y…
If you need to add user input without using a button, then a capacitive touch interface might be the answer. The AT42QT1011 S…
This is a simple strip of five signal-conditioning Balun Ember Transformers from Wurth Elektronik that allows you to convert …