Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
This motor from Pololu has a long (0.365" or 9.27 mm), D-shaped metal output shaft that matches the Pololu wheel 42x19mm and …
**Replacement:** None. We don't carry a direct replacement for this supply but take a look at our others in the [power suppli…
The Pixy CMUcam5 is a remarkably fast image sensor that is able to be taught to find objects of various shapes, sizes, and co…
**Replacement:** None. We do not have a direct replacement for this board. This page is for reference only. Carrier board fo…
**Replacement:**[BOB-11040](http://www.sparkfun.com/products/11040). The new version of this board gives full RGB control for…
The SparkFun Ludus ProtoShield is a motor driver shield for your Arduino that is designed to make connecting motors, sensors …
This red EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that you w…
The Intel® Edison is an ultra small computing platform that will change the way you look at embedded electronics. Each Ediso…
The HiFive1 is a low-cost, Arduino-compatible dev board featuring the Freedom E310 making it the best way to start prototypin…
The Shapeoko 4 XXL is a 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non-ferrous metals, ha…
So it turns out that your XBee based device would work even better as a Bluetooth device... that probably means back to the d…
This 10ft Category 6 (CAT 6) Ethernet cable is the solution to your internet working needs. With a speed of up to 500MHz you …
We all know that not every Arduino shield is 3.3V, many are 5V boards. This is the voltage translator shield, an easy to use …
If you're looking for a fun input device for your project this thing is a ball... really! This trackball communicates via PS/…
**Replacement:** None. There is no direct replacement for this item. This page is for reference only. A USB powered plasma b…
**Replacement:** None. There is no direct replacement for this programmer. This page is for reference only. JTAG programmer …
ABS Filament reels from Chroma Strand Labs. ABS is favored for it's strength, resilience, and heat resistance which makes it …
The uArm is an Arduino-powered, 4-axis robot arm that has been modeled after industrial pallet packing and car building robot…
**Replacement:** None. We are not carrying this product anymore. This page is for reference only. Custom header board for MS…
**Replacement:**[DEV-09219](http://www.sparkfun.com/commerce/product_info.php?products_id=9219) and [DEV-09221](http://www.sp…
**Replacement:** None. We do not have a direct replacement for this product. This page is for reference only. Feature-filled…
The XBee-PRO 900 RF module is ideally suited for low-latency point-to-multipoint networking applications. Capable of point-to…
The Tiger Claw Clamp is a low profile, high-quality stainless steel clamp that can be used on the Nomad or the Shapeoko.
**Replacement:** None. We are no longer carrying this development board. This page is for reference only. This is the second…
**Replacement:**[SWG-08343](http://www.sparkfun.com/commerce/product_info.php?products_id=8343). This product was retired bec…
**Replacement: **None. We are not carrying this product anymore. This page is for reference only. Development board for the …
Do you find yourself wishing that you had just a few more GPIO pins? What if you only need that _one more pin_? You _could_ a…
The Moog Werkstatt-Ø1 is a patchable and compact, one oscillator analog synthesizer. What's really amazing about this kit is…
We love heat shrink! We use it for all sorts of handy projects. Use it to reinforce connections, protect devices, and electri…
The 4th edition of our popular SIK for Arduino Uno, fully reworked from the ground up for a better learning experience! Perfe…
These hub-mountable aluminum gears are ideal for transmitting motion from a motor or servo to a wheel or shaft. These gears h…
This motor mount connects to other [Actobotics](https://www.sparkfun.com/pages/Actobotics) products with a swivel mount, allo…
It's that time of year when we sell off our production scrap. These boards do not work, but they make for great practice, and…
By popular demand, this is the new SparkFun T-Shirt. Black with SparkFun parts scattered around the phrase "Let Your Geek Shi…
These 0.1" spaced female headers are perfect for building your own Raspberry Pi B add-on modules. These PTH headers are arran…
This is a simple breakout for the ADXL345 accelerometer and the ITG-3200 MEMS gyro. With this board, you get a full 6 degrees…
**Replacement:** None. We are no longer carrying these rework nozzles. For more soldering and rework tools check out the [too…
**Replacement:** None. We are no longer carrying this processor, but we are still carrying a selection of [PIC microcontrolle…
When you need POWER, SparkFun has you covered! Welcome to the future, people. It's 2015 and we may not be able to predict the…
This cubelet displays the block's value as a light-up bar graph. The value is normalized to the number of points on the bar g…
**Replacement:** None. We do not have a direct replacement for this nozzle. This page is for reference only. Hot-air rework …
nGen is a co-polyester Filament that is optimized for 3D printers and perfect for both prototyping and production. With high …
This is an eval board for the ET-312 GPS module. We developed this eval board for it, but messed up the ET312 footprint. We h…
These blue precision disk wheels have an outer diameter of 4”, a width of 0.23”, and utilize the 0.77” hub pattern. The…
This is a wall adapter with a Barrel Jack Connector that has 15.0W of power.
This gunmetal, anodised aluminium case for the Raspberry Pi 4 will give you 10-15°C of passive cooling under a full CPU load…
Bluetooth is a great addition to a variety of projects, but the interface to most Bluetooth modules is through a serial UART,…
These orange precision disk wheels have an outer diameter of 3”, a width of 0.23”, and utilize the 0.77” hub pattern. T…