Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
Do you need big logic analysis in a small package? That's exactly what the Logic16 delivers. The Logic16 is a 16-channel USB …
**Replacement:**[BOB-00199](http://www.sparkfun.com/products/199). We are no longer selling this bare IC but we do continue t…
**Replacement:** None. We are no longer carrying this bare IC on the storefront. This page is for reference only. Silicon La…
8 Darlington Arrays in 18-Pin DIP Package part # ULN2803A. Perfect for running relays and high-power devices up to 500mA and …
This XL black tee proudly displays a large "X" (that's 10 in roman numerals) on a seven-segment display all in a sharp lookin…
**Replacement:** None. We are no longer carrying this widget. This page is for reference only. The UberTracker represents …
**Please note, these machines are built to order & have an estimated lead time of 10 days before shipping** This is the Sh…
DB9 Female Header Solder Tail package.
**Replacement:** None. We are no longer carrying this crystal. This page is for reference only. Standard frequency crystals …
This simple on-off switch is rated for 20A at 12V but who cares about all that, it looks way awesome. These toggle switches c…
This pink EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that you …
DC to DC converter/regulator MC34063A. Has an input range of 3V to 40V, output switch current of up to 1.5 amp. Step up, step…
**Replacement:**[COM-00589](https://www.sparkfun.com/products/589). We still offer the SMD package for this part. This page i…
**Replacement:**[LAB-12727](https://www.sparkfun.com/products/12727). Due to restrictions with the flux pen, we were unable t…
The Accel 7 Click is a tri-axis acceleration sensing Click board™ powered by the KXTJ3-1057 14-bit tri-axis digital acceler…
Standard frequency crystals - use these crystals to provide a clock input to your microprocessor. Rated at 20pF capacitance a…
The SparkFun Roshamglo is the new and fun way to play Rock-Paper-Scissors with your friends! The board uses the ATtiny84, and…
This is a medium-sized heatsink that has been designed to dissipate heat away from your boards and ICs. Each of these black a…
The STEMTera is an innovation in breadboard history. It is the first breadboard with an Arduino-compatible hardware suite bui…
Let your geek shine with this five pack of white NFC LED nail stickers. These nifty little things power themselves when in a …
MIKROE MP3 Click is an accessory board in mikroBus™ form factor.
BLE 6 Click is a Bluetooth low energy system-on-chip application processor certified module, compliant with BT specifications…
This is the surface mount header that mates with the Lassen IQ. **Part #**: CLP-104-02-G-D [ www.samtec.com](http://www.samt…
This medium, gray, men's shirt has been designed to keep all those around you guessing at what game you are playing with a CR…
A metal caster used for omni-directional robots. Omni-what? Imagine a robot with the dual-motor gear box. The robot can piv…
Track set for tank treads. Use these treads to create your own tank setup. These work superbly with the Tamiya dual gear box.…
Let your geek shine with this five pack of pink NFC LED nail stickers. These nifty little things power themselves when in a c…
The Qwiic Distance Sensor uses the new RFD77402 Time of Flight sensor. This sensor is special in that it uses an infrared VCS…
Riding on the waves of the very popular Arduino USB board is this small prototyping shield. Originally spawned with collabora…
This is the Zombonitron 1600 MOSS Basic Kit, an incredibly fun kinematic robot construction system from Modular Robotics. The…
What is a 'laser card' you ask? It is only the coolest thing to hit Spark Fun Electronics since the Color LCD last week! Don'…
V to Hz 2 Click is a device that converts an analog voltage input signal into a pulse wave signal of a certain frequency.
**Replacement:** None. We are not carrying this product anymore. This page is for reference only. Custom header board for th…
This module uses the newest 2.4GHz transceiver from Nordic Semiconductor, the nRF24L01+. This transceiver IC operates in the …
Go from blinking an LED to virtual prototyping in seven hours and still have time to eat lunch! This class is for anyone who …
**Replacement:** None. We are no longer carrying these rework nozzles. For more soldering and rework tools check out the [too…
The pi-topPROTO is a HAT-compatible add-on board for prototyping electronics for your pi-top or pi-topCEED. With plenty of sp…
The 915MHz Serial Telemetry Radio Kit is a lightweight and inexpensive open source radio platform that can allow for ranges o…
The MyoWare LED Shield is designed to pair with the [MyoWare Muscle Sensor](https://www.sparkfun.com/products/13723). The blu…
**Replacement:** None. There is no direct replacement for this part. This page is for reference only. Hot-air rework nozzles…
**Replacement:** None. The supplier decided to move to Mars or something, so we are unable to get these from them. As of now …
DIGI POT 4 Click is a digitally controlled dual potentiometer, with the resistance of 10KΩ.
The tinyTILE, an Intel® Curie-based board, is a miniaturized adaptation Arduino/Genuino 101® board perfect for wearable and…
Let your geek shine with this five pack of green NFC LED nail stickers. These nifty little things power themselves when in a …
The SparkFun Inventor’s Kit (SIK) for micro:bit is a great way to get creative, connected and coding with the micro:bit. Th…
Dip sockets for all your prototyping needs. If you've ever had to de-solder a dip part from a circuit board, you know how val…