Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
MIKROE Tilt 3 Click is a compact add-on board used for measuring the tilt in multiple axes in relation to an absolute level p…
The SparkFun SGP40 Air Quality Sensor provides a measurement of the quality of the air in your room or house. The Sensirion m…
We designed the Fiber Duplex Board for creating simple fiber links to embedded devices. This board has the same pinout as our…
Load Cell 6 Click is a compact add-on board representing a weigh scale solution.
MIKROE CXPI Click is a compact add-on board that contains a transceiver that supports the next-generation automotive communic…
The RS485 5 Click is a Click board™ equipped with the MAX485, low-power, slew-rate-limited transceiver for RS-485 and RS-42…
The Serial Fiber Modem combines a CH340C USB-to-Serial bridge with a fiber receiver and emitter pair from Industrial Fiber Op…
This board is actually a pair of boards! We wanted to design a product that gave you the bare minimum amount of support circu…
The Loomia Single Backlit Button is a simple mechanical switch that comes with an LED inside.
MIKROE Heart Rate Click is a heart rate monitoring and pulse oximetry measuring Click board™.
LDC Touch Click is a compact add-on board optimized for inductive touch applications.
The AS7341 is an 11-channel spectral sensor from AMS that covers wavelengths between 350nm to 1000nm. It features eight chann…
The Raspberry Pi Pico represents a first look into the world of microcontrollers for some people and the world of MicroPython…
I2C Isolator 3 Click is a compact add-on board that offers completely isolated bidirectional communication.
MIKROE Magneto 9 Click is a compact add-on board that contains a low-power, accurate, and reliable magnetic sensing device.
BATT-MAN 3 Click is a compact add-on board representing an advanced battery management solution.
The Shapeoko 4 XL is a 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non-ferrous metals, har…
MIKROE Brushless 7 Click is, as its name said, a motor driver based expansion board for controlling BLDC motors with any micr…
MIKROE Proximity 12 Click is a compact add-on board that contains a high-performance light and proximity sensing solution.
ADC 6 Click is an advanced 24bit multichannel analog to digital converter (ADC).
The LPS25HB is an absolute pressure sensor which means that it has an internal vacuum as a reference. (As opposed to *differe…
Panasonic's SN-GCJA5 laser type PM sensor is an addition to its already broad range of specialty sensor solutions. It is comp…
MIKROE OPTO Click is an accessory board in mikroBUS™ form factor. It features two VO2630 dual channel, high speed optocoupl…
MIKROE 4-20mA R Click is an add-on board in mikroBUS™ form factor which serves as a receiver in a 4-20mA current loop stand…
MIKROE MRAM Click features MRAM module which contains 262,144 magnetoresistive memory cells, organized into 32,768 bytes of m…
MIKROE GSM/GNSS Click combines GPS/GLONASS location tracking with GSM module capability for mobile communication.
Common Mode Chokes are useful in a variety of noise countermeasure applications, including power supplies, home appliances, a…
BarGraph Click is a 10-segment bar graph display Click, which uses a high-quality bar graph LED display.
This 8-channel USB Logic Analyzer with support for sampling rates of up to 24MHz provides a good while economic option making…
The MightyOhm Geiger Counter Kit++ includes all components needed to build by soldering a completely open source, hackable, w…
The SparkFun O-Clock can convert your X-Y analog oscilloscope into an analog clock or terminal. In addition, it can be used a…
TouchKey 3 Click uses the AT42QT1110, an 11-key QTouch® Touch Sensor IC from Microchip.
Rotary B Click carries a 15-pulse incremental rotary encoder with detents, surrounded by a ring of 16 blue LEDs.
The Heart Rate 9 Click is a Click board™ which features PIC16F1779 8-bit MCU and SFH 7060 heart rate and pulse oximetry mon…
WiFi NINA Click is a powerful standalone WiFi module, equipped with the state-of-the-art NINA-W132 module from u-blox.
The Bar02 Ultra-High Resolution 10m Depth/Pressure Sensor is a low-pressure, high resolution, high accuracy version of our Ba…
This board has gone red! You can see the new version [here](https://www.sparkfun.com/products/18012). We added a power LED so…
This sticker sheet provides 30 plastic labels for the 30 pins on the Analog Discovery 2 flywires.
This versatile T-track system provides a flexible and reliable way to hold down a wide assortment of material to your standar…
It features a microSD card slot for microSD cards used as a mass storage media for portable devices.
The Single Cell Click allows the user to program temperatures generated from external sources to control the fan speed.
This versatile T-track system provides a flexible and reliable way to hold down a wide assortment of material to your Shapeok…
This kit provides you with a RedBoard Turbo, two sensors, a joystick, and an OLED screen as well as all the cables you need t…
The 3x3 mini pressure matrix has six leads, allowing you to map which point you are at in the 3x3 matrix.
The straight 4-wire Bus has four leads that are each 0.15in wide.
The C-Curve Bus is perfect for connecting two 0.15in buses together at a wide angle.
The single pressure sensor gives you an analog read that maps to force on the sensor.
The SparkFun English edition of Elektor magazine is loaded with up-to-date news and views, real-world lab tests and high qual…