Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement:**[LCD-09924](http://www.sparkfun.com/commerce/product_info.php?products_id=9924). The new version doesn't have…
These are very thin variable potentiometers. By pressing down on various parts of the rotary dial, the resistance linearly ch…
This is the RFduino PCB USB Shield, a small add-on board that plugs into any USB port and is used to load your sketches onto …
The littleBits Deluxe Kit contains everything you need to design and create large, powerful projects just by snapping a few m…
This hot knife fits our butane soldering iron (SolderPro 50). It works well at cutting thin plastics, styrofoam, or various b…
**Replacement: **[PRT- 09914](http://www.sparkfun.com/products/9914). We won't be ordering anymore "backwards" cables, but yo…
**Replacement:** None. We don't have a direct replacement for this product. It has been discontinued. Check out our other [Bl…
This is the connector for the Keypad Sealed Membrane Switches. Comes with 14 pins in a ZIF right angle SMD package with 1mm p…
This is a handy little Bluetooth USB mini-adapter. This adapter supports Bluetooth v2.0 class 1 and has a maximum distance of…
**Replacement:** None. We don't carry a replacement for this module. This page is for reference only. If you need a small si…
Stay warm, outdoors! This is a high quality hoodie with front pocket. Large SparkFun logo on the front, blank back. If …
The TLC5940 is a 16 channel PWM unit with 12 bit duty cycle control (0 - 4095), 6 bit current limit control (0 - 63), and a d…
These 2" long aluminum tubes have an outer diameter of 5/8", an inner diameter of 0.569", and a wall thickness of 0.028". Whe…
**Replacement:** None. There is no direct replacement for this board. This page is for reference only. A nice prototype boar…
**Replacement:**[WRL-09034](http://www.sparkfun.com/products/9034). We are no longer carrying the bare IC. This page is for r…
This is a simple five wire cable. Great for jumping from board to board or just about anything else. There is a 5-pin Molex c…
Replacement: None. Unfortunately, this module is no longer being produced so we can no longer carry it in our catalog. This p…
**Replacement:** None. We are no longer carrying this SMD connector in our catalog. This page is for reference only. This is…
This is a high-quality, easy to use 28 pin [ZIF](http://en.wikipedia.org/wiki/ZIF_socket) socket that is 0.3" wide. Makes for…
This is the same product as the [Danger Shield](https://www.sparkfun.com/products/10570). The difference is this version come…
Want to start playing with sensors, but don't know where to begin? This kit includes a variety of basic sensors for any begin…
This new revision includes a JST cable and also fixes the TX/RX swap from the last revision. Now you can use an FTDI correctl…
These 2" long stainless steel tubes have an outer diameter of 1", an inner diameter of 0.88", and a wall thickness of 0.06". …
**Replacement:**[SWG-11354](https://www.sparkfun.com/products/11354). We have new stickers!! This page is for reference only.…
**Replacement:**[WRL-12576](https://www.sparkfun.com/products/12576). The firmware on this Roving Networks product has been u…
The SparkFun SPI Shortcut allows you to control SPI pins over USB, allowing for a virtual "SPI Terminal." Using basic serial …
This is the latest evolution of our serial LCD. Included on a single board is a 16x2 LCD and an embedded circuit based around…
**Replacement:**[SWG-11063](https://www.sparkfun.com/products/11063). We're now selling these notebooks exclusively in the gr…
This is the same product as the XBee Shield with a multitude of extra parts including 2 XBee modules, the popular XBee Explor…
Through-hole 24.5 mm coin cell holder. This holder fits our rechargeable 24.5mm Lithium Ion coin cell battery. Holds battery …
The SparkFun Serial Controlled Motor Driver allows you to control up to two DC motors using a serial command interface. The s…
**Replacement:** None. We are no longer carrying the ePIR in our catalog. This page is for reference only. Zilog's ePIR is a…
**Replacement:**[WRL-10559](http://www.sparkfun.com/products/10559). The new version comes with the headers unpopulated for m…
This is a low cost USB-based JTAG programmer for ARM processors based on the OpenOCD platform.
This faceplate is a perfect fit for the Arduino USB development board and Chameleon 1 enclosure. With a Chameleon 1 enclosu…
We all know that you can never get too many LEDs. Don't worry, we've got you covered. This is a pack of 25 LEDs all convenien…
Resonators function like crystals but stick closer to their specified frequency over a full temperature range. These resonato…
30 AWG wire for wire wrapping. Blue color. Very important to color code projects. Or else at 2am: "Which ones are the power b…
**Replacement:** None. Due to slow sales, we've decided to remove this product from our catalog. This page is for reference o…
**Replacement:** None. There is no direct replacement for this board, but check out our [development tools](http://www.sparkf…
Here is the breakout board for the RFM22B which gives you access to the pins. The RFM22B is a low-cost ISM (industrial, scien…
It's your basic blue action button! This is a very useful, small, panel-mount momentary switch. It is a SPST N.O. with the th…
**Replacement:** None. We are retiring this product due to poor sales. This page is for reference only. The PSoC mixed signa…
**Replacement:**[SEN-09694](http://www.sparkfun.com/products/9694). This is not a direct replacement but is a suitable substi…
**Replacement:**[PGM-09825](http://www.sparkfun.com/products/9825). The new version uses an SMD 5x2 header instead of a throu…
**Replacement:** None. We are not carrying this product anymore. This page is for reference only. You asked for it, now here…
This pamphlet is a sales sheet for retailers to use for their retail displays. Have them for customers as informational take-…
With this cable, you to can split one 3.5mm stereo jack into two stereo jacks.