Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
The Edimax WiFi Adapter is a nano-sized USB wireless adapter that supports maximum range and speed when connected to your loc…
These 6" long stainless steel shafts have a diameter of 1/4". These shafts are solid, which makes them an ideal choice for ax…
Photoluminescent is a big word that means a simple thing: Glow in the Dark! And do they ever! These Photoluminescent stickers…
The is a wonderfully simple 5V power source from Bodhilabs. This unit uses a two AA batteries and generates 5V using a DC to …
PowerBank Click is a USB charging expansion board which can be used for creating power bank devices or adding charging option…
The PI22TAT5R5G5B-2427 is a mouthful, but it's also an addressable RGB LED in a *very* small 2.4x2.7mm package. This four pin…
The RELAYplate from Pi-Plates is the first dedicated relay board for the Raspberry Pi designed to meet the safety requirement…
Brushless 17 Click is a compact add-on board suitable for controlling brushless DC (BLDC) motors with any MCU.
Who doesn't love the soft glow of electroluminescence? This EL panel is a flexible plastic sheet which contains a phosphor la…
MIKROE Turbidity Click is an adapter Click board™, used to interface a compatible turbidity sensor with the host MCU.
MRAM 3 Click is a compact add-on board representing a magneto-resistive random-access memory solution.
Forrest M. Mims III has written more than sixty books about science, lasers, computers, and electronics. In 1993, He received…
These Wall Adapter Cables from iPixel are terminated with a standard NA plug at one end and two insulated spade terminal conn…
The FLIR® Lepton® Adapter Module allows your OpenMV Camera to interface with the FLIR Lepton 1/2/3 Thermal Imaging sensors …
Intended for connection directly to multimeter or power supply.
MIKROE Haptic Click carries DRV2605, a Haptic Driver for ERM and LRA vibration motors.
Digital logic is the foundation of every task that a computer can do, so it's no wonder that in order to fully understand how…
Even though the Tron movies have been out for a while, electroluminescence is still the coolest thing since sliced bread. The…
A universal programmer and debugger for ARM® Cortex®-M, RISC-V, PIC®, dsPIC, PIC32, and AVR over USB-C.
Pogo pins make life so much easier when you are trying to program without having to solder a single thing, and when you attac…
These tags operate in the UHF (865MHz to 928MHz) band and contains a 96-bit EPC field that is programmable by the user.
MIKROE RTC2 Click is an accessory board in mikroBus™ form factor. It features the DS1307 serial real-time clock (RTC).
Atmel's ATmega328P 8-Bit Processor in 28 pin DIP package. It's like the ATmega168, with double the flash space. 32K of progra…
UV 4 Click is a powerful Ultra Violet (UV) sensing device and Ambient Light Sensor (ALS) Click board™.
This is a 40W single output switching power supply from Mean Well that has been specifically designed to be with LED applicat…
Do you like LED matrices? We do! Now we are giving you the power to make your own with minimal soldering any beginner can per…
MIKROE WiFi PLUS Click is a compact solution for adding WiFi communication to your project.
This versatile combo breakout pairs the u-blox ZED-F9P multi-band high precision GNSS module with the NEO-D9S L-band GNSS cor…
Pressure 19 Click is a compact add-on board that contains a board-mount pressure sensor.
This is a very small FM transmitter. Designed to be the building block of wireless microphones and MP3 broadcasters, this sma…
This is the LilyPad revision of our [FTDI Basic](http://www.sparkfun.com/products/9716). It is the same as our other FTDI Bas…
The PureThermal 2 Smart I/O Board is a hackable thermal USB webcam breakout for the FLIR Lepton® thermal imaging camera core…
The Fio v3 is a new spin on the Arduino Fio hardware powered by the ATmega32U4.Not only is it small and LiPo-ready, it's a ve…
MPU IMU Click carries the MPU-6000 integrated 6-axis motion tracking device.
The step down DC-DC regulator used on this Click board™ is the MPM3632C, a 18V 3A ultra-low profile DC-to-DC power module b…
In celebration of the most popular Arduino board, the Uno, Arduino has made and Arduino Uno Mini!
The SparkFun Infrared Control Kit give you an easy and cost-effective way to control electronics from across the room and wir…
These are the same RGB LEDs that were used for the old WS2801 breakout board. They're great when you need a lot of color from…
Radar Click as its foundation uses the MM5D91-00, a presence detection sensor module with an integrated mmWave technology fro…
The SparkFun Serial Controlled Motor Driver (SCMD) is a DC motor driver that’s been designed to drive small DC motors with …
Dual gearbox from Tamiya. This is an excellent way to get started quickly with robotics! You may have read many websites abou…
The ground probe connection has a detachable quality hook and the cable fits directly on a 2.54mm (0.100”) pitch pin header…
Were you not able to make it to the Autonomous Vehicle Competition ([AVC](https://avc.sparkfun.com/)) at Maker Faire® Denver…
BATT-MON 3 Click is a compact add-on board representing an advanced battery monitoring solution.
The SparkFun RTK Facet is a fully enclosed GNSS receiver for centimeter-level positioning. Perfect for high precision geoloca…
The SparkFun 9DoF Sensor Stick is an easy-to-use 9 Degrees of Freedom IMU. The Sensor Stick deftly utilizes the LSM9DS1 motio…
This great GT-521F32 fingerprint module from ADH-Tech communicates over TTL Serial so you can easily embed it into your next …
MIKROE PULSE Click is a pulse generator with an adjustable frequency.