Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement:** None. We are no longer carrying this t-shirt in our catalog. This page is for reference only. We've hit the…
The Arcade MegaWing is an opensource add-on for the Papilio FPGA development platform that gives you all the hardware you'll …
The LogicStart is an open source MegaWing for the Papilio Pro development platform that provides you with everything you need…
The RetroCade is an open source MegaWing for the Papilio Pro that allows you to make some totally radical MIDI music straight…
This is one of the smallest servos we carry but don't let its size fool you, the HS-35HD is a durable and strong little servo…
Fingerprint scanners are awesome. Why use a key when you have one right at the tip of your finger? Unfortunately, they're usu…
The Raspberry Pi is everybody's favorite little computer, the last thing that you'd want is for something bad to happen to it…
These orange ELastoLite inverter connectors are to be used in conjunction with the INV135 electroluminescent inverter for dri…
These green ELastoLite inverter connectors are to be used in conjunction with the INV133 electroluminescent inverter for driv…
The arLCD from EarthMake is an easy and cost effective way to have a touchscreen LCD in your Arduino project. This is a smart…
The Temperature Cubelet contains a tiny thermometer (actually, a thermistor) that detects temperature. It's calibrated to out…
The Distance Cubelet detects how far it is from an object. It uses infrared light and is accurate between 10 and 80 cm. The s…
The Knob Cubelet has a potentiometer embedded in one of its faces. It outputs a 0 when turned fully counterclockwise, and a 1…
The Brightness Cubelet has an analog photocell that responds to varying light conditions and detects the amount of light hitt…
The Minimum Cubelet can accept any amount of data, but only outputs the smallest value that it receives. It can be handy for …
The Inverse Cubelet calculates a value that is the opposite of the values it receives. Specifically, the Inverse Cubelet will…
The Maximum Cubelet accepts many different inputs but only passes along the one with the greatest value. With a maximum block…
The Passive Cubelet is a basic building block. It carries power and data from its neighbors, but it basically acts like a sma…
The Blocker Cubelet is a basic building block that "blocks" data from its neighbors. It still passes power, but effectively s…
The Drive Cubelet contains a motor and roller wheels for moving on a horizontal surface and moves in one direction, slowing t…
The Rotate Cubelet allows one face to spin at a rate corresponding to the block's input values. Cubelets are magnetic block…
The Speaker Cubelet contains a small speaker and an amplifier that will chirp according to the block's data value. Cubelets…
The Flashlight Cubelet emits a focused beam of light from a powerful white LED. The light becomes brighter with higher input …
The Battery Cubelet provides energy to power a construction. It contains two rechargeable batteries and a small power switch.…
This is the BC127, a highly flexible, low power, small form factor Bluetooth Version 4.0 Certified Audio module. Each module …
**Replacement:** None. Unfortunately, this Bluetooth remote is not FCC certified so we cannot carry it in our catalog. This p…
The Bluetooth Cubelet contains a tiny Bluetooth radio that you can pair with your Android device or PC. With the Cubelets Con…
It's the end of the world, and you need a button to press. This is it. A white economy grade 100mm diameter (outside diameter…
This is a perfect choice if you are in need of a heavy duty push button! These metal push buttons are a very tough, small, pa…
The Arduino Mega 2560 R3 is a very big and powerful microcontroller,needless to say, you want to keep it protected. Why not p…
It's your basic green action button! This is a very useful, small, panel-mount momentary switch. It is a SPST N.O. with the t…
It's your basic blue action button! This is a very useful, small, panel-mount momentary switch. It is a SPST N.O. with the th…
It's your basic yellow action button! This is a very useful, small, panel-mount momentary switch. It is a SPST N.O. with the …
This is a simple USB Webcam that can be plugged into your computer or dev board and start capturing video right away. The res…
The WDS112 MetaWatch is a fantastic little smartwatch designed to compliment your smartphone. A smartwatch is essentially a c…
This motor has a 3mm D-shaped metal output shaft that matches the Pololu wheel 42x19mm and 32x7mm. The face plate has two mou…
**Replacement:** None. We are no longer carrying this mini metal gearmotor in our catalog. This page is for reference only. …
Want to make a 12 ft GPS wall clock? This is the perfect item to light it up! Even if that's not the project you are looking …