Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement:** None. We are no longer carrying this product. This page is for reference only. AVR-JTAG is the new In Circu…
**Replacement:**[DEV-10531](http://www.sparkfun.com/products/10531). The new revision uses a type-B USB jack as well as makin…
**Replacement:** None. We don't have a direct replacement for this kit. This page is for reference only. The VoiceGP DK incl…
**Replacement:** None. There is no direct replacement for this board. This page is for reference only. Header board with LCD…
**Replacement:** None. We do not have a direct replacement for this board. This page is for reference only. Prototype board …
**Replacement:** None. We are no longer carrying this part in our catalog. This page is for reference only. This is an un-so…
**Replacement:** None. We are no longer carrying this product which means it's time for this one to step back and make room f…
**Replacement:** None. We are no longer carrying this dev board but check out the rest of the [AVR development tools](https:/…
**Replacement:** None. We've eliminated the circuit overlays in the SIK in favor of larger, clearer diagrams. This page is fo…
**Replacement:** None. We are no longer carrying this parts box in our catalog. This page is for reference only. This is a n…
Common Mode Chokes are useful in a variety of noise countermeasure applications, including power supplies, home appliances, a…
**Note: **We have some of these left. Grab 'em for a limited time only! User Manuals are full of helpful information to get …
Too long have you suffered at the hem of shapeless, boxy t-shirts! Finally, we're stocking our popular SparkFun Tees in women…
Your computer science department in a box! From beginner's coding to advanced AI, bring CS learning to life.
Build rovers and robots with additional components for more complex maker projects.
Everything you need to build a robot.
Power your robotics projects with computer vision and applied AI.
This Translucent Plastic Enclosure is a multipurpose enclosure ideally suited for horizontally mounting printed circuit board…
This faceplate is a perfect fit for the ET-AVR development board and Chameleon 1 enclosure. With a Chameleon 1 enclosure, d…
If you've got the project case from SparkFun, you may have altered the insert to fit the connectors for your project. Whether…
Gyro 3 Click is a three-axis gyroscope Click board™ that can sense motion over three perpendicular axes.
MIKROE H-Bridge 8 Click is a compact add-on board that contains H-bridge current regulator.
Rubber Foot - RF-003, commonly called rubber bumpers, represents a rubber pad generally used on all forms of equipment.
0.218" tall, brass [swage](http://www.rafhdwe.com/swage.htm) attachable stand off. Non-threaded.
AudioAmp 5 Click is a stereo audio amplifier, capable of delivering up to 10W per channel with the 8Ω load.
MIC 2 Click is equipped with a small electret microphone, accompanied by a suitable pre-amplifying circuit.
AudioAmp 6 Click is a mono/subwoofer audio amplifier, capable of delivering up to 18.5W per channel with the 4Ω load.
VU Meter Click is a compact add-on board representing a volume unit meter that displays the intensity of an audio signal.
Audio Xover Click is an analog active crossover solution for two-way loudspeakers.
The MIC 3 Click is a Click board™ that features the SSM2167-1RMZ-R7, a Microphone Preamplifier, from Analog Device.
Buzz 3 Click is a compact add-on board that contains a sounder driver that produces higher volume with a lower current.
Volume 2 Click is a compact add-on board that provides the user with complete digital volume control.
BT Audio 3 Click is a compact add-on board with high-performing voice and audio post-processing capability for Bluetooth audi…
Multiplexing allows address expansion as well as addressing one of the multiple identical devices, thus resolving address con…
Analog MUX 2 Click is a compact add-on board that switches one of the eight inputs to one output.
UART MUX 2 Click is a compact add-on board that enables pseudo-multidrop RS232 transmission.
Power MUX 2 Click is a compact add-on board that contains a highly configurable power mux.
MCP16331 Click functions as a buck-boost voltage regulator.
Buck 2 Click is a powerful step down DC-DC switching regulator.
The switching regulator used on MCP16331 INV Click is the MCP16331, a step-down (buck) switching regulator from Microchip.
BUCK 6 Click is an advanced synchronous DC-DC step down (buck) converter, with a very wide input voltage range and reasonably…
Boost 3 Click is a compact add-on board that contains a boost converter with an integrated current mirror function.
USB-C Sink Click is a compact add-on board that contains a standalone autonomous USB power delivery controller.
eFuse 2 Click is a compact add-on board that contains an integrated FET hot-swap device.
eFuse 3 Click is a compact add-on board that contains an electronic eFuse.
PAC1954 Click is a compact add-on board that contains an energy monitoring solution.