Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SIK for micro:bit v2 Lab Pack includes 10 complete m:b v2 Inventor's Kits, an SIK Refill Pack and 25 AAA-sized batteries …
The SparkFun Inventor's Kit (SIK) is a great way to get started with programming and hardware interaction with the Arduino pr…
The Go Bundle is a quick and economical way to get started with the micro:bit v2. So gather up your crew, give your club a co…
The 4th edition of our popular SIK for Arduino Uno, reworked to v4.1 for a better learning experience! Perfect for internatio…
The SparkFun Inventor’s Kit (SIK) for micro:bit v2 is a great way to get creative, connected and coding with the micro:bit …
The micro:bit v2 Educator's Lab Pack includes 10 micro:bit v2 boards and everything you need to get you started with the new …
The LilyPad Sewable Electronics Kit lets you explore the wonderful world of electronic sewing (e-sewing) and e-textiles throu…
The MaKey MaKey Classic by JoyLabz is an invention kit that tricks your computer into thinking that almost anything is a keyb…
With the release of the Jetson Nanoâ„¢ Developer Kit, NVIDIA® empowers developers, researchers, students, and hobbyists to e…
The SIK Lab Pack includes 10 complete Inventor's Kits, a Refill Pack with, and AA sized batteries to get your class started i…
The SparkFun Inventor’s Kit for RedBot is a great way to get started with two motor robotics and sensor integration using t…
Combining the micro:bit with the SparkFun moto:bit carrier board creates a flexible, low-cost, Qwiic-enabled robotics platfor…
This is the latest version of our popular through-hole Simon Says Kit. We've made some changes to the board that should make …
The SparkFun Raspberry Pi 4 Hardware Starter Kit provides a solid set of parts and instruction for working with the Pi 4 in a…
The 8GB Raspberry Pi 4 Hardware Starter Kit provides a solid set of parts and instruction for working with the RPi4 in a more…
The digital multimeter (DMM) is an essential tool in every electronic enthusiasts arsenal. The SparkFun Digital Multimeter, h…
The BBC micro:bit v2 is a pocket-sized computer that has been updated with additional features that let you get creative with…
The micro:bit v2 is a pocket-sized computer and the Go Bundle provides you with everything you need to get hooked up and powe…
The Raspberry Pi 4 Basic Kit includes everything you'll need to get up and running with the new Raspberry Pi 4 8GB.
The SparkFun micro:climate kit is a full weather station kit that is built on top of the weather:bit carrier board.
This is the E-textile Basics Lab Pack, a basic wearables learning kit that can easily get you and a group of peers or student…
We all know that you can never get too many LEDs. Don't worry, we've got you covered. This is a pack of basic red, yellow, bl…
The SparkFun weather:bit is a fully loaded "carrier" board for the micro:bit that provides you with a fully functional weathe…
Alligator clips (or Crocodile clips, if you prefer) are likely to be the most useful thing on your workbench besides the work…
The SparkFun Inventor's Kit Bridge Pack for micro:bit was designed to provide you with an easy way to transform your m:b into…
Have you ever seen a [Weevil](https://en.wikipedia.org/wiki/Weevil)? It's a pretty under-appreciated beetle, so we thought it…
The SparkFun Qwiic micro:bit Breakout with Headers is a board that connects to the BBC micro:bit and expands the capabilities…
Copper tape has countless applications in electronics from creating low-profile traces for electrical components to RF-shield…
The SparkFun Paper Circuits Kit teaches the basics and fundamentals of creating an electric circuit without the need to solde…
The Raspberry Pi 4 Basic Kit includes everything you'll need to get up and running with the Raspberry Pi 4 4GB.
The SparkFun moto:bit is a fully loaded carrier board for the micro:bit that provides you with a fully functional robotics pl…
This is a simple 4-pack of momentary, multicolor buttons, great for all sorts of projects! Unlike previous iterations of mult…
The SparkFun Line Follower Array is a long board consisting of eight IR sensors that have been configured to read as digital …
The Line Follower sensor is an add-on for your RedBot that gives your robot the ability to detect lines or nearby objects. Th…
This is a 10-pack of wires that are pre-terminated with an alligator clip on one end and a male header on the other.
With the micro:arcade kit V2.0 you will be able to turn a classic controller into an arcade cabinet by connecting just a few …
This assortment of tools is great for those who need a solid set of tools to start your workbench on the right foot!
This is the Wheel Encoder Kit from DAGU, a simple add-on to any wheeled robot that can help measure the speed or distance the…
The J-Link EDU Mini is a stripped-down, budget-friendly model of the J-Link debug probe created for educational use.
The WE1010 from Weller is a powerful 70 watt soldering station that is perfect for passionate hobbyists, DIYers, and anyone w…
This is a unique two-cell AAA battery holder built specifically for the BBC micro:bit. The 6" (~150mm) cable has been termina…
The Raspberry Pi 3 B+ Starter Kit is a great way to gain a solid introduction to the small, credit-card-sized computer.
Robots are fun, and Arduinos are easy. So wouldn't it be nice if there were a kit that included everything you need to get yo…
These are a pair of right angle, hobby gearmotors from DAGU. These gearmotors are the same ones utilized in the Magician Chas…
Bare Conductive's Electric Paint Pen is just like any other water-based paint... except that it's electrically conductive!
The Mountable MI:pro is a simple and compact protective case for the micro:bit.
Our through-hole Simon Says Kit is a great beginner's kit and also a pretty fun toy. All components are through-hole, making …