Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
With the heART Surface Mount Soldering Kit you will be able to learn the basics of SMD soldering by being able to assemble a …
The Raspberry Pi 4 Basic Kit includes everything you'll need to get up and running with the Raspberry Pi 4 2GB.
Bare Conductive's Electric Paint is just like any other water-based paint... except that it's electrically conductive!
Binary Blaster is a game designed to help teach what binary numbers are and how to convert from decimal (and hexadecimal) to …
The Raspberry Pi 4 Basic Kit includes everything you'll need to get up and running with the Raspberry Pi 4 but without the bo…
The SparkFun Qwiic micro:bit Breakout is a board that connects to the BBC micro:bit and expands the capabilities of the devel…
With this Lighthouse kit you will be able to learn the basics and intermediate skills of soldering by being able to assemble …
This is your basic spool of leaded solder with a 63/37 water soluble resin core. 0.031" gauge and 100 grams. This is a good s…
The SparkFun Raspberry Pi Zero 2 W Basic Kit provides you with everything you need to get started with this successive Pi, al…
The SparkFun RedBot Mainboard is a robotic development platform that works with the Arduino IDE.
Tip tinner is a good thing to have in your arsenal of soldering supplies. Composed of a mild acid, it helps remove baked on r…
The SparkFun Raspberry Pi Zero W Camera Kit provides you with a pan/tilt camera controlled via a Raspberry Pi Zero W.
A simple looking ball-point pen that allows you to draw circuits instead of soldering or wiring them to a breadboard.
This is a brass sponge that will help clean your soldering iron tip. Use it to remove residue from your iron tip before solde…
Engineering Just Got Cool with the Arduino Engineering Kit! Bring the power of the Arduino MKR1000 to the classroom with MATL…
The MI:pro Protector is a simple and compact protective case for the micro:bit.
These are your run-of-the-mill 1/4 Watt, +/- 5% tolerance PTH resistors. Commonly used in breadboards and other prototyping a…
This black version of the Day of the Geek soldering kit you will be able to learn the basics of soldering by being able to as…
These simple switches are the Mechanical Bumper sensor for the SparkFun RedBot, giving you the ability to detect a collision …
This is a simple soldering iron stand composed of a heavy-duty metal base and a reinforced spring holder. The base and holder…
The Unigeek is a soldering kit that teaches you the basics of PTH and SMD soldering while assembling a light up unicorn badge…
This buzzer is an add-on for your RedBot that gives your robot the ability to make awesome beep-boop noises or alerts when so…
The SIK Guidebook V4.1 contains step by step instructions with circuit diagrams for building each project and circuit with th…
The Kitronik Autonomous Robotics Platform for Raspberry Pi Pico is a fun and hands-on introduction to buggy robotics.
The Arduino microcontroller makes it easy to learn about electronics, but it can be hard to know where to start. The 10 proje…
This white version of the Day of the Geek soldering kit you will be able to learn the basics of soldering by being able to as…
Thanks to the SparkFun gator:soil micro:bit Accessory Board, you can now measure the moisture level in soil without any vocal…
This is a very simple fixed temp, quick heating, 30W 110/120 VAC soldering iron. We really enjoy using the more expensive iro…
The SparkFun Wireless Motor Driver Shield is designed to make connecting motors, sensors and other components to your Arduino…
The Accelerometer sensor is an add-on for your RedBot that provides bump and motion detection. The sensor works by measuring …
The full-color LilyPad Sewable Electronics Kit Guidebook contains step-by-step instructions for creating four interactive pro…
The SparkFun gamer:bit is a fun-filled "carrier" board for the micro:bit that, when combined with the micro:bit, provides you…
Arduino AKX00015 CTC Go Kit is an educational program with several modules that can be combined to teach different STEAM subj…
Processing is a free, beginner-friendly programming language designed to help non-programmers create interactive art with cod…
The SparkFun gator:microphone is a micro:bit Accessory Board that integrates a microphone into SparkFun's gator:bit series of…
Bare Conductive's Electric Paint Pen is just like any other water-based paint... except that it's electrically conductive!
Have some fun coding your very own AI robot with TJBot, a do-it-yourself template to learn, experiment with and explore AI wi…
The SparkFun gator:bit is an all-in-one “carrier” board for your micro:bit that provides you with a fully functional deve…
The release of the Jetson Nano™ 2GB Developer Kit, NVIDIA® empowers developers, researchers, students, and hobbyists to ex…
The fourth edition of our popular SIK, fully reworked from the ground up for a better learning experience! V4.1 now has the a…