Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun Triad Spectroscopy Sensor is a powerful optical inspection sensor with three sensors combined alongside LEDs us…
The SparkFun OpenPIR is a highly customizable Passive Infrared (PIR) sensor based around the NCS36000 PIR controller. Passive…
The new PureThermal Mini Pro JST-SR with Thermal by FLIR® is a hackable thermal camera for the FLIR Lepton® thermal imaging…
With everything included in this Sensor Kit, you'll be able to sense gesture, humidity, temperature, motion, touch, sound, al…
This SparkFun Distance Sensor Breakout utilizes the VL53L1X next generation ToF sensor module to give you the highly accurate…
The SparkFun Grid-EYE Infrared Array Breakout board is an 8x8 thermopile array, giving you a square of 64 pixels capable of i…
The SparkFun AS7263 Near Infrared (NIR) Spectral Sensor Breakout brings spectroscopy to the palm of your hand, making it easi…
This SparkFun Distance Sensor Breakout utilizes the VL53L4CD next generation ToF sensor module to give you the highly accurat…
The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWI…
This version of the QRE1113 breakout board features an easy-to-use analog output, which will vary depending on the amount of …
The TFMini Plus is a ToF LiDARcapable of measuring the distance to an object as close as 10 centimeters and has been designed…
The Line Follower sensor is an add-on for your RedBot that gives your robot the ability to detect lines or nearby objects. Th…
With the FLIR Radiometric Lepton Dev Kit you will be able to bring FLIR's thermal imaging reliability and power to your desir…
The TFMini-S Micro LiDAR Module is a ToF LiDAR sensor capable of measuring the distance to an object as close as 10 centimete…
The SparkFun Essential Sensor Kit V2 includes a variety of basic sensors for any beginner or experienced programmer.
The SparkFun Line Follower Array is a long board consisting of eight IR sensors that have been configured to read as digital …
This version of the QRE1113 breakout board features a digital output, using a capacitor discharge circuit to measure the amou…
The SparkFun Qwiic Human Presence and Motion Sensor is built around the STHS34PF80 low-power, high-sensitivity IR sensor for …
The SparkFun Photoacoustic Spectroscopy CO2 Sensor features the XENSIV™ PAS CO2 sensor package from Infineon©, which provi…
The Qwiic Mini Human Presence and Motion Sensor is built around the STHS34PF80 low-power, high-sensitivity IR sensor for pres…
The SparkFun Proximity Sensor Breakout is a simple IR presence and ambient light sensor utilizing the VCNL4040.
The MLX90640 SparkFun IR Array Breakout is equipped with a 55° FOV, 32x24 array of thermopile sensors creating a low resolut…
The SST Liquid Level Sensor provides single point liquid detection via a TTL compatible push/pull output. This optical liquid…
This is a simple to use motion sensor. Power it up and wait 1-2 seconds for the sensor to get a snapshot of the still room. I…
Photo interrupter, photogate, photodiode, phototransistor, whatever you want to call it, this sensor is composed of an infrar…
Great for detecting motion in a small area and optimized for small movements to offer motion-sensing options for battery powe…
The MLX90640 SparkFun IR Array Breakout is equipped with a 110° FOV, 32x24 array of thermopile sensors creating a low resolu…
Great for detecting motion in a small area & optimized for small movements to offer motion-sensing options for continuously p…
The Raspberry Pi Camera Module 3 is the latest entry in our mainstream camera line-up, and the successor to the popular Came…
The radiometric Lepton has 80x60 active pixels to capture accurate, calibrated, and non-contact temperature data in every pi…
This is an evaluation board for the MLX90614 IR Thermometer. The sensor is connected to an ATmega328 running at 3.3V with a S…
Embrace the World of Precision Distance Measurement with the SparkFun DataLogger IoT Distance Sensing Kit.
This simple device operates at 940nm and works well for generic IR systems.
This IR proximity contactless button makes for a good replacement for typical push buttons
Melexis' MLX90614ESF-BAA is an infrared thermometer designed for non-contact temperature sensing. An internal 17-bit ADC and …
The SparkFun WiFi IR Blaster is designed to connect all of those old, legacy IR-controlled devices to a WiFi network exposing…
The FLIR Lepton Thermal Camera Breakout Board is an easy-to-interface evaluation board to quickly connect the Lepton camera m…
Use this simple IR receiver for infrared remote control of your next project. With low power consumption and an easy to use p…
A line follower sensor gives your robot the ability to detect lines or nearby objects.
Passive Infrared (PIR) sensors are great for detecting motion in a small area around the sensor.
The EX8036 Stereo Camera is a high-end imager controller and patterned IR illuminator with a global shutter capable of both c…
The SparkFun Qwiic PIR Starter Kit (1µA) comes with just the basics of what you need to get started working with passive inf…