Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The Raspberry Pi 4 Case Fan keeps your Raspberry Pi 4 at a comfortable operating temperature even under heavy load.
The Kitronik Autonomous Robotics Platform for Raspberry Pi Pico is a fun and hands-on introduction to buggy robotics.
The Raspberry Pi Global Shutter Camera is a specialized 1.6-megapixel camera from Raspberry Pi that is able to capture rapid…
The Raspberry Pi 400 is a complete Raspberry Pi 4-based personal computer, integrated into a keyboard.
The Build HAT allows you to control LEGO® Technic™ devices with your favorite Raspberry Pi.
The Compute Module 4 plugs right into the I/O Board and provides a multitude of inputs and outputs for prototyping or evaluat…
The compact Simply Servo board for Raspberry Pi Pico allows for up to 8 servos to be controlled simultaneously.
This is a basic baseplate for the Raspberry Pi 3 B+. The baseplate is designed for the RPi to remain on the attached via fric…
The Qwiic pHAT Extension for the RPi400 provides you with an easy way to access all GPIO, stack your favorite HAT upright or …
A sturdy pan-tilt mechanism for most of the cameras that are used with microcontrollers.
The Compute Module 4 packs all the best features of the Raspberry Pi Model B 4 into a more favorable form-factor for embedded…
The Kitronik Smart Air Quality Board for Pico provides a complete air monitoring and reporting solution for the Raspberry Pi …
With Single-Board Computers (SBCs) on the rise, it is a good idea to have an easy way to interface with them. Operating on a …
WizFi360-EVB-Pico is based on Raspberry Pi RP2040 and adds WiFi connectivity using WizFi360.
The Kitronik Discovery Kit for Raspberry Pi Pico (Pico not included) is a great way to learn about microcontrollers, Python c…
This is a USB Type-C Power Supply that is compatible with the Raspberry Pi 4.
The Raspberry Pi is everybody's favorite little computer, the last thing that you'd want is for something bad to happen to it…
This adaptor allows you to power your RPi 4 with a previous usb-micro B power supply.
Make the Raspberry Pi Pico the core of your new buggy project with the Kitronik Compact Motor Driver Board for Raspberry Pi P…
The Argon POLY+ Raspberry Pi 4 Case uses a three piece snap-fit plastic design to protect your Pi 4 in a cost-effective way.
The Raspberry Pi Compute Module 4 represents a huge change for the Compute Module line. The biggest change being the move fro…
This is the Antenna Kit for the Raspberry Pi 4 Compute Module wireless variants.
This module allows a designer to leverage the Raspberry Pi hardware and software stack in their own custom systems and form f…
A 200mm MIPI Cable for interfacing the Raspberry Pi Display Modules with the Raspberry Pi 5.
The SparkFun RP2040 mikroBUS™ Starter Kit is designed to give you just what you need to start using the Click, Qwiic, and R…
The Raspberry Pi Compute Module 3+ contains the guts of a Raspberry Pi 3 Model B+ with 8GB of eMMC Flash memory.
The is the official, 1m, HDMI to HDMI Cable for use with the Raspberry Pi.
The pi-topCEED is a DIY desktop computer that helps you start learning how to code, create awesome devices and take your know…
This 2x13 shrouded header has the same number and spacing of pins as the Raspberry Pi so you can easily connect via ribbon ca…
Feeling Fancy? The SparkFun Top pHAT is the fundamental machine learning add-on for Raspberry Pi or any 2x20 GPIO SBC!
This 8MP IR (Infrared) camera module is capable of 1080p video and still images and connects directly to your Raspberry Pi.
The IQaudIO Pi-DAC+ HAT Audio card for the Raspberry Pi delivers outstanding sonic performance and full-HD (24/192) audio cap…
This 8mp camera module is capable of 1080p video and still images that connect directly to your Raspberry Pi.
Have some fun coding your very own AI robot with TJBot, a do-it-yourself template to learn, experiment with and explore AI wi…
The Argon40 Fan HAT for the Raspberry Pi Model B boards is a great way to cool your board during more intensive applications.
The Raspberry Pi High Quality Camera M12 Mount is the same high quality camera as the previous model but with an M-12 lens mo…
This is a class 10, 16GB, micro SDHC card that has been pre-installed with the NOOBS operating system for the Raspberry Pi.
The Raspberry Pi Compute Module 3+ contains the guts of a Raspberry Pi 3 Model B+ with 16GB of eMMC Flash memory.
This is the official case for the Raspberry Pi 3 Model A+ (it also fits the Raspberry Pi 1 Model A+ as well).
The Raspberry Pi Compute Module 3+ contains the guts of a Raspberry Pi 3 Model B+ with 32GB of eMMC Flash memory.
The Raspberry Pi Zero is half the size of a Model A+, with twice the utility. A tiny Raspberry Pi that’s affordable enough …
The Raspberry Pi 3 A+ is here to provide you with the same Pi you know and love, just more compact and at a cheaper price!
The PiJuice is a fully uninterruptible power supply HAT that will always keep your Raspberry Pi powered.
The next iteration of the Raspberry Pi single board computer featuring a 64-bit quad-core Arm Cortex-A76 processor running at…